Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116558 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    I agree with you Shabaz. It's not so wrong to discuss - hopefully someone will read these threads - because the most dangerous thing I see is just the wrong documentation, worst than lack of documentation. I needed a day to install and see the Kivy framework working. And it is almost essential to manage small touch screen displays like the 7 inches and more the 4.2 inches for Raspberry PI. So if people don't know, IMO should put clear that what they write is "unverified" or at least it is a personal opinion. Not like it is the absolute knowledge then users go in panic. Last but not least, the documentation is one of the key factors of the marketing. Also with newbie users (maybe more with them).

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    Part of it is due to the hiding of information (perhaps for good intentions - to make things "easier"). So when an Arduino program fails, people are not really sure what could be occurring, because the knowledge of what the IDE and programming mechanism is doing is underlying and wasn't ever explained. So everything breaks down because the thin layer between 'easy' and 'hard' has been scratched. Just an opinion : ) and a major digression, so sorry about that.

    But yes, I agree, a minimal paper would be helpful. I always refer to the simple references, so I can

    clear my head of needing to remember everything : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    Shabaz,

    I give it for sure. A minimal paper is essential also for us. Especially in these things. This makes the difference of a product. The need to make a all-in-one tutorial is just because all explain how and no one seems have tried at least one time to see what. Excluding very rare cases (e.g. our Charles_Gantt that is very serious tech journalist, me - obviously - and few others) I read incredible things. It is rare the people really make tests and see what happens. And more rare that try to solve the problems. Easier to say works/don't than investigate. In my opinion this is a form of loss of respect.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    I think it is raspberrypi.org's failure, they perhaps should have shipped a bunch of displays to non-tech people before launch, who could have provided them enough feedback to put together a diagram.

    Basically early field trial.

    In the absence of a diagram or label, you or I would check flat flex orientation precisely, but

    since it is unkeyed, proabably many non-tech people would think it is reversible.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    Hi Shabaz,

     

    the documentation coming with the display is something like "search for the documentation on the Internet" image Nothing !

     

    But the usage of the cables is insidious because it is very difficult to see where the contacts are in the connectors.

     

    BTW, as you receive your display remember to rad this page image

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    Hi Enrico,

     

    Does any documentation come with the display? Sounds like there really ought to have been a 1-sheet drawing explaining how to plug everything in.

     

    I know they have like 7 or 8 steps, but who follows so many steps : ) The magic max. number is 3.

     

    Also, they could have had a paper sticker on the ribbon cable with a drawing showing how to open the connector first..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    Also, the white flat flex cable may be flipped the wrong way around - with some connectors it doesn't matter, but I don't know which specific connectors were used on the RPI and the LCD board.

    So, best to flip the entire flat flex around on both boards, so it looks _exactly_ like in the photo in the blog post (i.e. text side facing the RPI, not facing away as you have it. It might be subtle, but it is possibly important.

     

    he he he ... image Clever minds think the same

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hello Mark,

     

    about the installation, for the software side frankly I think that all seems correct. Anyway take a look to some more details on the post I have published just now in the Raspberry Accessories section: Essential Raspberry Pi Peripherals #2 (annex 2): 7" LCD touch screen display installation notes

     

    Instead about hardware: it sounds ok the settings of power it is sufficient a single power supply on the Raspberry PI with the read and black cables connected as I see in the images, I suggest to remove the second power supply image

     

    What seems wrong to me - but images are not showing it perfectly is the white flat cable. Please try to remove it and invert it. Maybe this is the problem. The cable has one white side and one with blue text. The white side should be on top respect the display board and reversed on the Raspberry PI too. Maybe this is the problem. No matter as the contacts are on one side only. The result is that you have put the cable but without connecting the two boards image

     

    Just to be clear, take a loo to the following image:

    image

    Your cable is in the opposite side, as far as I see.

     

    Let me know if this will work.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    You appear to have USB cables on both boards - this is fine, but then you shouldn't have the red and black jumpers connected (as I understand - I've not tried it, nor seen any schematics).

     

    Also, the white flat flex cable may be flipped the wrong way around - with some connectors it doesn't matter, but I don't know which specific connectors were used on the RPI and the LCD board.

    So, best to flip the entire flat flex around on both boards, so it looks _exactly_ like in the photo in the blog post (i.e. text side facing the RPI, not facing away as you have it. It might be subtle, but it is possibly important.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    imageimageimageimage

     

    Here is my setup. I just checked the cables with a multi Meter. Everything seems to be eine.

    Any Suggestionen?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>