RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs AMD Xilinx Kria KV260 Vision AI Starter Kit : Preparing the KV260
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: feiticeir0
  • Date Created: 7 Mar 2023 11:53 PM Date Created
  • Views 11450 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended
  • RoadTest
  • kv260 vision
  • Kria KV260 Vision AI Starter Kit
  • AMD XILINX
  • roadtest review
  • kv260
  • AMD Xilinx Kria KV260 Vision AI Starter Kit
  • amd

AMD Xilinx Kria KV260 Vision AI Starter Kit : Preparing the KV260

feiticeir0
feiticeir0
7 Mar 2023

image

Hi all  !Hope everyone is well.

This is the second post regarding my experience with the Xilinx Kria KV260 Vision AI Starter KIT

For more information and the first POST, read it here

AMD Xilinx Kria KV260 Vision AI Starter Kit : First Impressions

On the third post I went through training a custom object detection model to detect Car's License Plates

Software

Today was the day to learn how to install the software and prepare the KV260 for the next steps.

I'm going to try both images available for the KV260 - PetaLinux and Ubuntu.

Because I always loved to be on the bleeding edge, I've decided to download and use the latest versions. If they are available and are not beta version, let's use them.

All the documentation and tutorials that I've seen and read are all for previous versions. Because of that, strap on and let's go for a ride. This is going to be wild... Slight smile

firmware upgrade

According to the Wiki, for the latest Linux images - Ubuntu 22.04 LTS or PetaLinux, a firmware upgrade is needed. Let's first download the boot update

image

At this point, I don't know how to upgrade the firmware . I've been reading and there are some utilities that do this, but still don't know if I can use the PetaLinux latest version and upgrade the firmware from there, or if I need to download a previous version, upgrade the boot firmware and then use the latest PetaLinux .

I'll download the latest version of PetaLinux and see if it boots. If it boots, I will use the xmultil bootfw_update utility to update the boot firmware.

I had to dig a bit because when downloading the PetaLinux image, this was a format I never had seen before. But it turns out, it's just like a img and can be used with dd or any other software to write images to a SDCARD

image

I've downloaded the 2022.1 version - petalinux-sdimage_xilinx-k26-starterkit

The PetaLinux file is big,6.0GB and it's now being written to the SD CARD - a 32GB one.

image

After so, many, minutes, all was done

image

Let's put it in and power on the device

First boot and PetaLinux

At first, nothing appear on the screen. No HDMI image. Decided to try the DisplayPort. Still no image. What was going on ? I confess that the instructions for booting the PetaLinux are not clear or I didn't find any documentation on how to do it. This was my first time with it.

Decided to read about the Ubuntu installation - it's bit more complete. 

After reading the documentation, I've connected the USB port to the computer and something appeared on the logs.

image

image

So many ttyUSB...

Configuring my minicom with the recomended settings: 115200,8,n,1,N

At first, I've tried all the serial ports and nothing. No prompt, nothing. Turning it off and on again, with ttyUSB2, ttyUSB3 and ttyUSB0, nothing. just a line on the screen.

Decided to try ttyUSB1 and finally something was appearing on the terminal. A Linux booting.

But, it didn't work. A lot of errors and no prompt. I'm assuming that this is because I haven't yet upgraded the firmware to allow me to use the latest version.

So, I decided to download the previous version - Kria Starter Kit 2021.1 and see if it would boot so I could upgrade the firmware and be able to boot the lastest version available.

image

Inserted the SD Card in the KV260 and let's try it again

This time it worked and I have a full Linux ready.

Firmware upgrade

To upgrade the firmware, I just followed the instructions.

Having now a network connection and a user and password, it's easy.

Copy the downloaded firmware (insert link) to the KV260

scp BOOT_xilinx-k26-starterkit-v2022.1-09152304_update3.BIN petalinux<at>192.168.2.228:

Inside the terminal:

sudo xmutil bootfw_update -i BOOT_xilinx-k26-starterkit-v2022.1-09152304_update3.BIN

sudo reboot

After the reboot, validate the boot

sudo xmultil bootfw_update -v

And that's that.

image

After a successful reboot, having a terminal and the boot firmware upgraded, let's try the latest PetaLinux version.

Again, put the image on the SD Card. Again, wait an endless time for the copy...

image

Let's put the SD Card in the KV260 and turn it on.

This time, the terminal just went until a login screen appeared - but not here (on the debug terminal - ttyUSB1)

I had to connect a USB keyboard to be able to login. This time I had image from the HDMI display. Hurray.

PetaLinux

After the full upgrade and a reboot, let's try some of the APPS already available for the KV260.

The Kria Applications - or AA.

After a lot of reading on why I can't find the SmartCamera APP (or any other APP for that matter), finally I found some post on the Xilinx forums saying that the APPs are going to be released in a future time..

As of 2022 there's no packages available to download with xmutil .. Nothing shows when doing xmultil getpkgs. All the documentation I've seen was for previous versions.

After reading and reading, I'm guessing I need to - install Ubuntu or create a PetaLinux image with the APP already there.

After some more reading about creating a PetaLinux image, I've decided to give a go to Ubuntu. After perusing through the documentation, I'm guessing that Xilinx (AMD) is really betting on Ubuntu and on the relationship with Canonical.

Ubuntu

After downloading the Ubuntu image, let's decompress it and put it in the SD Card. Tea time

image

It's already in the SD CARD, lets try and boot it.

After a boot, I have a full Ubuntu desktop on the HDMI monitor and a remote ssh to it.

Don't tell anybody, but it's a tad slow. But, nothing that I wasn't expecting.

image

Let's try to run some examples.

According to the documentation, an upgrade is recommended and after that, install the Xilinx Development & Demonstration Environment.

sudo snap install xlnx-config --classic --channel=2.x

Now let's wait until all is done

image

Next, we need to run xlnx-config.sysinit to install some PPAs

image

Yes we do. Answer yes to all the questions .

After a while we get all the repositories installed - the ones with the applications for us to test.

And another upgrade is done.

After a reboot, let's search for the AAs

SmartCam APP

sudo apt search kv260

And, finally some results

image

Let's install the SmartCam app

sudo apt install xlnx-firmware-kv260-smartcam

And after a while, we have it installed.

Let's try and run it

First, we need to disable the desktop environment

sudo xmutil desktop_disable

Next, see the apps listed with xmutil

sudo xmutil listapps

And it's there

image

Now, we need to unload the current app loaded and load the smartcam app

sudo xmutil unloadapp

remove from slot 0 returns: 0 (Ok)

sudo xmutil loadapp kv260-smartcam

image

Now that the APP is loaded.

After a few minutes trying to find the application binary, nothing.

Since this was a full Linux with Ubuntu apps, installed a small utility - mlocate - that creates a database with all the files and the location, making it really easy and fast to search for something. The downside is that from time to time you need to update the database. But I've decided to give it a go.

After creating the database, decided to search for the app or files and/or directories with the name

locate smartcam

Nothing relevant. What was going on ? Was the documentation wrong ?

After a lot more reading and reading and reading, it turns out that as of Ubuntu 22.04 for the KV260, applications are deployed as Docker containers.

I'm starting to think that the bleeding edge is not wort it ! Slight smile

Let's install docker, shall we ?

Docker

These are instructions from the Docker website for Ubuntu and these are the instructions recommended from the documentation.

sudo apt-get update
sudo apt-get install ca-certificates curl gnupg lsb-release
sudo mkdir -m 0755 -p /etc/apt/keyrings
curl -fsSL https://download.docker.com/linux/ubuntu/gpg | sudo gpg --dearmor -o /etc/apt/keyrings/docker.gpg
echo "deb [arch=$(dpkg --print-architecture) signed-by=/etc/apt/keyrings/docker.gpg] https://download.docker.com/linux/ubuntu \ $(lsb_release -cs) stable" | sudo tee /etc/apt/sources.list.d/docker.list > /dev/null

Update apt

sudo apt-get update

Install docker

sudo apt-get install docker-ce docker-ce-cli containerd.io docker-buildx-plugin docker-compose-plugin

Run the hello-world

sudo docker run hello-world

Now that we have docker, let's add our user to the group

sudo usermod -a -G docker ubuntu

Let's continue with the Smartcam. Pull the latest version

docker pull xilinx/smartcam:2022.1

image

After a moment, the image is downloaded and extracted.

Let's launch the docker image

docker run \
--env="DISPLAY" \
-h "xlnx-docker" \
--env="XDG_SESSION_TYPE" \
--net=host \
--privileged \
--volume="$HOME/.Xauthority:/root/.Xauthority:rw" \
-v /tmp:/tmp \
-v /dev:/dev \
-v /sys:/sys \
-v /etc/vart.conf:/etc/vart.conf \
-v /lib/firmware/xilinx:/lib/firmware/xilinx \
-v /run:/run \
-it xilinx/smartcam:2022.1 bash

and you get this:

image

So far, so good, I'm guessing

Let's run the application in the command line. You can also run a jupyter notebook. View the documention.

I'm going to use the IAS camera and output to the HDMI monitor

smartcam --mipi -W 1920 -H 1080 --target=dp

image

And now with the USB camera (Raspberry PI camera v2)

smartcam --usb 1 -W 1920 -H 1080 --target=dp

image

Clearly there's a difference between the two cameras.

Well, for Ubuntu it's all done. For now.

PetaLinux - second Go

I like Ubuntu, but is way to heavy for this.

I knew that I could use PetaLinux - Ubuntu is great, but I've always been a CLI person. After a lot of reading and almost desperation, I found a page on the Xilinx github.io that explains how to build PetaLinux with the Application Packages - because all the videos I've seen and pages that read, mostly on Hackster.io mention building the PetaLinux and using bsp files.

NOTE: The documentation is for the 2021.1 version. Still, let's give it a shot.

The getting started videos from the Xilinx website are all in the 2021 version and the apps are all there... But for this PetaLinux version - 2022.1 - they are not.

So, let's get started

First, we need to install the PetaLinux tools, latest version from here. This an installer and will do everything.

image

We also need to download the Kria K26 Starter Kit Board Support Package - the BSP file for the KV260

image

Let's install everything needed (I'm using Arch Linux). The installer complains about xterm and netstat .

sudo pacman -S xterm net-tools

and now we can start

./petalinux-v2022.2-10141622-installer.run -d <your directory of choice for the instalation>

After a while, it says its done.

image

This is the contents of the directory

image

Now, activate the environment by running settings.sh (you may have to give it execution permissions first)

source settings.sh

image

I don't have a tftp server, but let's continue.

Now, we need to create a project using the bsp file we downloaded before (copy it to installation directory of PetaLinux)

petalinux-create -t project -s xilinx-kv260-starterkit-v2022.2-10141622.bsp

and in a moment:

INFO: Create project:
INFO: Projects:
INFO:     * xilinx-kv260-starterkit-2022.2
INFO: Has been successfully installed to /home/feiticeir0/petaLinux/
INFO: New project successfully created in /home/feiticeir0/petaLinux/

Let's go into the project directory

cd xilinx-kv260-starterkit-2022.2/

Before we build the image, we want to add the AAs just for testing

Let's add some strings and variables

echo 'BOARD_VARIANT = "kv"' >>  project-spec/meta-user/conf/petalinuxbsp.conf

Now, let's add the application groups that we want into the rootfs config file so that the menuconfig gets populated with these entries.

echo 'CONFIG_packagegroup-kv260-smartcam' >> project-spec/meta-user/conf/user-rootfsconfig

echo 'CONFIG_packagegroup-kv260-aibox-reid' >> project-spec/meta-user/conf/user-rootfsconfig

echo 'CONFIG_packagegroup-kv260-defect-detect' >> project-spec/meta-user/conf/user-rootfsconfig

echo 'CONFIG_packagegroup-kv260-nlp-smartvision' >> project-spec/meta-user/conf/user-rootfsconfig

Let's run the petalinux rootfs config

petalinux-config -c rootfs

If you get an error about libtinfo.so.5, just go into /usr/lib and create a symlink from libtinfo.so.6 to libtinfo.so.5 and it will work . Slight smile

image

Now, go into user packages and select all the AAs

image

Exit and save the configuration

Let's create the image

The following commands build the image and package it.

petalinux-build

Building the Petalinux image get's all my CPUs almost at 100%

image

But my temperature is well ! Water cooling for the win !

But it didn't work...

image

Lets see the log...

And the errors are:

image

I've posted a question to Xilinx forum. Let's wait.

Well, this where I'm at right now.

If there's any update, I'll post it here.

But, there's not stopping now.

I still have to learn how to develop applications and deploy them here. What are my options about the software. Next posts.

Last notes

I have some weird behavior with the KV260. Every time I connect and, for example, disable the desktop to try the SmartCam APP, it changes the IP address. Like you see in the picture, I've already went through all those IP addresses.

image

And sometimes Ubuntu doesn't boot. I have to turn it off and on again to have some picture... Weird stuff that I'm going to try to solve.

Oh, this has been a roller coaster.

Until the next post.

References

https://community.nxp.com/t5/i-MX-Processors/Yocto-i-MX28-How-to-use-wic-for-make-sd-card/m-p/758764

https://highlevel-synthesis.com/2022/06/12/kria-kv260-and-petalinux-2022-1-part-01-getting-started/

https://xilinx.github.io/kria-apps-docs/kv260/2021.1/build/html/docs/build_petalinux.html

https://xilinx.github.io/kria-apps-docs/kv260/2022.1/build/html/docs/kria_starterkit_linux_boot.html

  • Sign in to reply

Top Comments

  • feiticeir0
    feiticeir0 over 2 years ago in reply to pingran +1
    Hi pingran ! No, I haven't . I've installed the Smartcam APP using docker, on Ubuntu. The problem you're having doesn't surprise me. Despite they "are the same". Try to compile it directly on Ubuntu…
  • pingran
    pingran over 2 years ago

    Thank you for sharing. Have you compiled the source code of smartcam and run it on Ubuntu? If so, what cross-compilation tools did you use for compilation? I tried compiling the smartcam source code using the SDK generated by petalinux2023.2, along with the vitis AI library and vvas. The compilation was successful, but the executable cannot run on Ubuntu. The cross-compilation chain I obtained has been updated to the official Ubuntu version. Additionally, the .so file required by the smartcam executable is newer than the version available on Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago in reply to amahpour

    Are you sure is not your SD CARD? Have you tried with a new one ?

    Have you tried to see what's happening on the debug console ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amahpour
    amahpour over 3 years ago in reply to feiticeir0

    Thanks for the quick response. The longest portion was the part after the kernel fully loaded but right before GNOME desktop booted. It sits with a blank screen for ~10 minutes. Wondering if maybe there's a problem with my board (even though it's brand new).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago in reply to amahpour

    Hi !

    Ubuntu booting was not slow - it is a tad slow when in the desktop - I'm guessing because of the graphics card.

    Are you sure your SD Card is in good condition ?  It can be because of the SD Card.

    Can you monitor the debug console while the system is booting ? Maybe there's something there - an error message or a message that can explain why your system is taking that long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amahpour
    amahpour over 3 years ago

    Thanks for the bring up notes. Just curious, how long did it take you to boot up Ubuntu 22.04 for the first time? A tad slow is a bit of an understatement. I've run through the process several times already (including Ubuntu 20.04 as well) and it usually takes 15-20 minutes to get to the log in screen.

    After restart it can still take close to 10 minutes for a restart. Am I doing something wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>