Roadtest - Shield Integration with the Infineon BLDCSHIELDTLE9879TOBO1 SHIELD
Evaluating High-Power 3-Phase BLDC Motor Control and Classic Shield Form-Factor Integration on the Arduino® UNO Q Hybrid Single-Board Computer
Primary Hardware Under Test: BLDCSHIELDTLE9879TOBO1 SHIELD, BLDC MOTOR DRIVER (INFINEON)
Core Test Objective: Stacking the Infineon BLDC Motor Driver Shield onto the primary pin headers to test how the Arduino UNO Q handles high-current, classic Arduino shield form-factor hardware and real-time three-phase brushless motor control across its dual-brain hybrid architecture.
Introduction
This evaluation is part of the element14 RoadTest Open Call, which turns the traditional RoadTest concept around by letting community members select the exact hardware under $175 USD from the Newark / Farnell / element14 online stores that they want to test and review. Having previously roadtested the Arduino UNO Q in Test out Arduino's Uno Q - The new Single-Board Computer and paired it with a Grove expansion shield to earn 3rd Place in the element14 On The Line Design Challenge with the Industrial Line Sentinel (ILS), my goal across this three-part Open Call series is to evaluate the physical expandability of the Arduino UNO Q across the wider ecosystem—specifically testing Qwiic® Modulino® nodes (AKX00069 Plug and Make Kit), high-power classic Arduino shields (BLDCSHIELDTLE9879TOBO1), and mikroBUS adapter headers (MIKROE-1581 Arduino UNO Click Shield).
In this second dedicated RoadTest (Shield Integration with the Infineon BLDCSHIELDTLE9879TOBO1 SHIELD), I unbox the evaluation board, inventory its power-stage components and onboard connectors, examine the electrical and SPI architectural specifications of the TLE9879QXA40 motor driver SoC, review Infineon's technical documentation, and build a dual-brain hybrid application in Arduino App Lab that links real-time SPI brushless motor actuation on the STM32U585 MCU to a live Linux telemetry and control service on the Qualcomm Dragonwing MPU.
1. Overall Rating Score & Detailed Breakdown
Based on the evaluation criteria and bench findings documented across this BLDCSHIELDTLE9879TOBO1 RoadTest, here are the 1-to-5 star scores and reasoning for all 7 element14 RoadTest scoring points:
| element14 RoadTest Criterion | 1–5 Star Score | Bench Reasoning & Evaluation Findings |
|---|---|---|
| 1. Hardware Integration & Mechanical Form Factor | ★★★★★ 4.8 / 5.0 |
Stacks directly onto the Arduino UNO Q's standard R3-compatible headers (X8, X10, X12, X14) with full pass-through capability, supporting up to four stacked shields (BOARD1–BOARD4) via hardware auto-addressing without obstructing the UNO Q's onboard Qwiic connector. |
| 2. Motor Control Performance & Co-Processor Offloading | ★★★★★ 4.8 / 5.0 |
The onboard Infineon TLE9879QXA40 SoC embeds a dedicated 32-bit Arm® Cortex®-M3 microcontroller that executes high-frequency PWM generation, shunt current sensing, and closed-loop FOC, BEMF, and HALL commutation algorithms independently of the UNO Q host processors. |
| 3. Build Quality & Power Stage Engineering | ★★★★☆ 4.5 / 5.0 |
Engineered around six automotive-grade Infineon IPC90N04S5-3R6 OptiMOS |
| 4. Driver & Library Stability (TLE9879_Group) | ★★★★☆ 4.3 / 5.0 |
The official TLE9879 BLDC Shield Arduino Library compiles cleanly and executes 16-bit SPI parameter transactions with CRC-8 validation on the UNO Q's STM32U585 Cortex-M33 MCU over Zephyr RTOS, though non-reference motors require manual parameter tuning. |
| 5. Documentation & Learning Resources | ★★★★☆ 4.5 / 5.0 |
Supported by a comprehensive User Manual, Getting Started Guide, TLE9879QXA40 Data Sheet, and Keil µVision5 firmware projects, though tuning sensorless FOC/BEMF constants requires consulting Infineon community notes. |
| 6. Value & Ecosystem Versatility | ★★★★☆ 4.5 / 5.0 |
At $67.28 on Newark (Part No. 02AH1038), it delivers an industrial- and automotive-grade 3-phase motor control testbed that bridges low-voltage edge logic with high-current 12V–28V DC actuation. |
| 7. Overall RoadTest Rating Score | ★★★★★ 4.6 / 5.0 |
A rugged, intelligent 3-phase brushless motor driver shield that offloads real-time commutation math while coexisting cleanly with the Arduino UNO Q's Qwiic and Linux App Lab interfaces. |
2. Unboxing & Packaging Overview
This section documents the physical unboxing experience, protective ESD packaging, and initial hardware inspection upon receiving the Infineon BLDCSHIELDTLE9879TOBO1:
Outer Packaging & Presentation: Inspect the rigid Infineon evaluation kit cardboard box, manufacturer part number labeling (BLDCSHIELDTLE9879TOBO1 / BLDC_SHIELD_TLE9879), Newark order code (02AH1038), barcode serial tracking, and RoHS / No-SVHC compliance markings.
ESD & Header Pin Protection: Verify that the shield is sealed inside a metallized electrostatic discharge (ESD) shielding bag with conductive backing foam protecting the long underside pins of the four pass-through Arduino stacking headers (X8, X10, X12, X14) from bending in transit.
PCB Silkscreen & Color-Coded Zone Clarity: Examine the red solder-mask finish and Infineon's color-coded functional silkscreen outlines—yellow for the Arduino headers (X8, X10, X12, X14), red for the high-current motor phase and 12V DC supply pads (X1–X5), purple for the Hall sensor header (X15), blue for the 10-pin SWD debug header (X6), green for the LIN bus test point, and orange for the onboard diagnostic RGB LED.
Readiness Check 1 – Packaging & Compliance Seals: Photograph the outer Infineon carton, ESD bag labels, and factory inspection stickers prior to opening.
Readiness Check 2 – Stacking Header Alignment Inspection: Inspect all four banks of pass-through pins (X8, X10, X12, X14) for straightness and solder joint quality before mating them to the Arduino UNO Q female headers.
Readiness Check 3 – Power Stage & Bulk Capacitor Inspection: Verify the solder integrity of the three surface-mount 560 µF / 35 V bulk electrolytic capacitors (C17, C25, C33), the central TLE9879QXA40 VQFN-48 package, and the six IPC90N04S5-3R6 power MOSFETs across the three inspection targets below:
- Photo 1 – TLE9879QXA40 SoC (Upper-Left Quadrant): Shoot at a slight 30°–45° oblique angle under diffused side light so the 48 perimeter VQFN pads reflect cleanly; verify there are no solder bridges between adjacent pins or dry/unwetted corners.
- Photo 2 – Bulk Capacitor Bank (C17, C33, C25 Center Column): Shoot low and close to the PCB surface along the vertical capacitor column (C17 top, C33 middle, C25 bottom) to confirm both SMD base tabs sit flush on their pads without tombstoning, lifted leads, or tilted cans.
- Photo 3 – B6 Power MOSFET Bridge (T1–T6 Right Quadrant): Frame the 3×2 array of IPC90N04S5-3R6 (PG-TDSON-8) MOSFETs beside the L3 (T5, T6), L2 (T3, T4), and L1 (T1, T2) phase pads; check for smooth solder fillets on the large drain tabs and clean separation across the source/gate leads.
Readiness Check 4 – Power & Phase Terminal Preparation (X1–X5): Because the high-current +12V (VBAT), GND, and 3-phase motor pads (Phase 1 / L1, Phase 2 / L2, Phase 3 / L3) ship as unpopulated plated through-holes, solder either heavy-gauge silicon motor/supply leads or high-current screw/banana terminals prior to stacking the shield onto the Arduino UNO Q.
3. Components & Accessories Inventory
The BLDCSHIELDTLE9879TOBO1 ($67.28 retail at Newark, Part No. 02AH1038) ships as a pre-assembled, factory-flashed evaluation shield. Below is the itemized inventory of the onboard hardware subsystems, connector headers, and the user-supplied bench equipment required to execute the RoadTest.
3.1 Onboard Shield Subsystems & Connector Inventory
BLDCSHIELDTLE9879TOBO1 – Infineon BLDC Motor Control Shield| Primary IC: Infineon TLE9879QXA40 (Arm Cortex-M3 + 6 NFET Drivers) | Qty: 1 | Standalone Price: $67.28 — Single-chip 3-phase BLDC motor driver evaluation shield in classic Arduino UNO R3 form factor.
Power Stage B6 Bridge – 6× Infineon IPC90N04S5-3R6 | Package: PG-TDSON-8| Qty: 6 Onboard MOSFETs | Spec: 40V OptiMOS-5 N-channel power FETs (3.6 mΩ max R_{DS(on)}) — Directly switches the three-phase motor windings (U, V, W).
DC-Link Bulk Capacitor Bank – C17, C25, C33 | Package: SMD Aluminum Electrolytic (153CLV-1014) | Qty: 3 Onboard Capacitors | Spec: 560 µF / 35 V each (1,680 µF total) — Buffers the 12V DC supply rail and absorbs regenerative back-EMF energy during motor deceleration.
X8, X10, X12, X14 – Arduino Pass-Through Headers | Silkscreen Zone: Yellow | Qty: 4 Header Banks | Spec: Standard Arduino UNO R3 pinout — Routes SPI (SPICLK, MRST, MTSR), Chip Select (CS1–CS4), Auto Addressing, RESET, and logic ground between the UNO Q and up to 4 stacked shields.
X1, X2, X3, X4, X5 – High-Current Power & Motor Phase Pads | Silkscreen Zone: Red | Qty: 5 Plated Through-Holes | Spec: Unpopulated high-current solder pads — Connects external +12V (VBAT), GND, and the three BLDC motor phase leads (Phase 1 / L1, Phase 2 / L2, Phase 3 / L3).
X15 – Hall Sensor Connector | Silkscreen Zone: Purple | Qty: 1 (5-Pin Header) | Spec: 2.54 mm pitch pin header — Supplies regulated VDDEXT 5V (±2% @ 20 mA) and GND from the TLE9879QXA40 internal regulator and receives three Hall sensor signals (CCPOS 0, 1, 2 / HALL 0, 1, 2).
X6 – Cortex SWD Debug Header | Silkscreen Zone: Blue | Qty: 1 (10-Pin Header) | Spec: Standard 10-pin Arm SWD interface — Allows attaching a SEGGER J-Link debugger to modify or re-flash the onboard TLE9879QXA40 Keil µVision5 firmware.
LIN Bus Test Point | Silkscreen Zone: Green | Qty: 1 Unpopulated Solder Hole | Spec: LIN 2.2 / SAE J2602 interface — Exposes the TLE9879QXA40 integrated automotive LIN transceiver for single-wire network testing.
Diagnostic RGB Status LED | Silkscreen Zone: Orange (Upper-Left Corner) | Qty: 1 Tri-Color LED | Spec: SPI-controllable status indicator — Driven by the TLE9879QXA40 via setLed() and setLedColor() to provide visual confirmation of SPI communication and motor state.
3.2 Bench Test Equipment & Interconnect Inventory
Arduino® UNO Q Host Board | Role: Primary Dual-Brain Controller | Spec: Qualcomm Dragonwing QRB2210 Linux MPU + STM32U585 Cortex-M33 MCU — Acts as the SPI Master and hosts the Arduino App Lab telemetry web dashboard.
External 12V DC Regulated Bench Power Supply | Role: High-Current Motor Supply (VBAT) | Spec: 12V DC nominal (5.5V–28V operating range) with adjustable current limiting — Supplies clean high-current power directly to the shield's X1/X2 pads without loading the UNO Q's USB-C rail.
3-Phase Brushless DC (BLDC) Test Motor | Role: Electromechanical Load | Spec: 12V 3-phase BLDC motor (such as the reference Trinamic QBL4208-41-04-006 or equivalent 3-phase actuator) — Connected to Phase 1, 2, 3 (X3–X5) and optionally to the X15 Hall sensor header.
High-Current Screw Terminals / Silicone Test Leads | Role: Power & Phase Interconnects | Spec: 16–18 AWG stranded silicone wire or soldered screw terminals — Provides secure, low-resistance connections at pads X1–X5.
4. Specification Notes & Architectural Overview
4.1 TLE9879QXA40 System-on-Chip & Power Stage Architecture
Per the TLE9879QXA40 Data Sheet and the BLDC-SHIELD-TLE9879 User Manual, the shield combines an automotive-grade embedded power SoC with a low-impedance MOSFET bridge:
Single-Chip 3-Phase Motor Driver SoC (TLE9879QXA40): Packaged in a compact 7 × 7 mm VQFN-48 footprint, the TLE9879QXA40 integrates an industry-standard 32-bit Arm® Cortex®-M3 core, flash memory pre-loaded with three motor control algorithms, six fully integrated NFET gate drivers, and a low-voltage charge pump.
Synchronized PWM & Dual-ADC Sensing Engine: The SoC incorporates a Capture and Compare Unit 6 (CCU6) dedicated to 3-phase space-vector PWM generation, synchronized directly with a 10-bit SAR ADC (8 multiplexed inputs + 5 external analog channels) for high-speed low-side shunt current sensing via an internal operational amplifier, alongside an 8-bit ADC (10 multiplexed inputs) for real-time die temperature and battery supply voltage (VBAT) monitoring.
Programmable Gate Current & EMC Slope Control: The six integrated NFET gate drivers feature programmable charge/discharge current and current-slope control, allowing developers to optimize electromagnetic compatibility (EMC) and minimize switching ringing across the six external Infineon IPC90N04S5-3R6 N-channel MOSFETs.
Wide Automotive Supply Range & Autonomous Protections: Designed for 12V automotive systems, the shield supports a 5.5 V to 28 V DC normal operating input voltage (and 28 V to 40 V extended operating range) while enforcing hardware-level protection against overtemperature, overcurrent, undervoltage, and overvoltage faults.
Multi-Shield Auto-Addressing Architecture: Up to four BLDC_SHIELD_TLE9879 boards (BOARD1 through BOARD4) can be stacked vertically on a single Arduino host. Immediately after a hardware reset, the onboard auto-addressing circuitry senses the shield's vertical position in the stack and assigns its dedicated Chip Select line automatically.
4.2 Comprehensive Pin Assignment, Connectors & Commutation Mode Matrix
| SHIELD SIGNAL / HEADER | ARDUINO / CONN PIN | DIRECTION (UNO Q) | PRIMARY FUNCTION & PROTOCOL ROLE |
|---|---|---|---|
| SPICLK | D13 (SCK) | Output (Master) | SPI Serial Clock shared across up to 4 stacked shields |
| SPI MTSR | D11 (MOSI) | Output (Master) | SPI Master Transmit / Slave Receive (16-bit commands) |
| SPI MRST | D12 (MISO) | Input (Master) | SPI Master Receive / Slave Transmit (dataset & CRC-8) |
| CHIP SELECT 1, 2, 3, 4 | D4, D5, D6, D7 | Output (Master) | Individual Slave Select lines for BOARD1 through BOARD4 |
| Auto Addressing | Analog / Digital | Bidirectional | Detects stack position (1 of 4) immediately after reset |
| RESET | RESET | Output (Host) | Hardware reset synchronizing shield & host startup |
| VDDEXT 5V & GND | X15 Header | Shield Output | 5V +/-2% @ 20mA regulated supply for external Hall sensors |
| CCPOS 0, 1, 2 | X15 Header | Shield Input | Hall sensor commutation inputs (HALL 0, HALL 1, HALL 2) |
| Phase 1, 2, 3 & 12V/GND | X1 - X5 Solder Pads | High-Power Rail | 3-Phase motor windings (U/V/W) and external 12V DC supply |
SPI Bus Interface (SPICLK, SPI MTSR, SPI MRST) | Header: X10 / X12| Protocol: 16-bit Synchronous Serial (SPI) | Checksum: CRC-8 validated dataset transfers | Role: The Arduino UNO Q STM32U585 MCU acts as the SPI Master, sending high-level opcodes (START_MOTOR, STOP_MOTOR, setMode, setMotorSpeed, setParameter, READDATASET) while the shield's TLE9879QXA40 acts as the SPI Slave.
Chip Select & Auto-Addressing Lines (CHIP SELECT 1–4 & Auto Addressing) | Header: X8 / X10 / X14| Capacity: Up to 4 Stacked Shields (BOARD1–BOARD4) | Role: Selects which stacked shield receives the active SPI transaction, enabling independent speed, direction, and mode control for up to four BLDC motors from one UNO Q.
Sensorless Field-Oriented Control (FOC Mode) | Dataset Size: 46 Messages (92 Bytes) | Key Tunable Parameters: FOC_R_PHASE, FOC_L_PHASE, FOC_POLE_PAIRS, FOC_NOM_CUR, FOC_MAX_SPEED, FOC_SPEED_KP, FOC_SPEED_KI| Best For: High-efficiency, low-ripple sinusoidal torque and speed control in robotics, gimbals, pumps, and fans without Hall sensor wiring.
Sensorless Back-EMF Block Commutation (BEMF Mode) | Dataset Size: 30 Messages (60 Bytes) | Key Tunable Parameters: BEMF_POLE_PAIRS, BEMF_PWM_FREQ, BEMF_SPEED_KP, BEMF_SPEED_KI, BEMF_RUNBEGIN_SPEED_PWM_MIN| Best For: Simple, sensorless 6-step trapezoidal speed control in medium-to-high RPM wheel drives and blowers using zero-crossing back-EMF detection.
Hall-Sensor Block Commutation (HALL Mode) | Dataset Size: 22 Messages (44 Bytes) | Key Tunable Parameters: HALL_POLE_PAIRS, HALL_INIT_DUTY, HALL_SPEED_KP, HALL_SPEED_KI, HALL_SPEED_IMIN, HALL_SPEED_IMAX| Best For: High starting torque and rock-solid low-RPM stability (<60 RPM or geared drives) using three Hall effect sensors connected to header X15.
4.3 Host Comparison & Electrical Compatibility: Classic UNO R3 vs. Arduino UNO Q
While Infineon originally designed the BLDC_SHIELD_TLE9879 around the 8-bit ATmega328P Arduino UNO R3, stacking it onto the Arduino UNO Q unlocks a tri-processor architecture:
Tri-Core Processing Pipeline (QRB2210 + STM32U585 + TLE9879QXA40): In this configuration, the Qualcomm Dragonwing QRB2210 Linux MPU handles web dashboard serving, CSV/database logging, and edge AI analytics; the STM32U585 Cortex-M33 MCU coordinates real-time SPI shield commands and 3.3V Qwiic sensor polling over Zephyr RTOS; and the shield's Infineon TLE9879QXA40 Cortex-M3 executes deterministic microsecond-level gate commutation.
Complete Electrical Isolation Between 12V Motor Power and UNO Q Logic: The external 12V DC supply connected to X1/X2 powers both the 3-phase MOSFET bridge and the TLE9879QXA40's internal 5V/1.5V regulators (including the VDDEXT 5V Hall sensor supply on X15). No motor current is drawn through the Arduino UNO Q's USB-C port or onboard voltage regulators, protecting the UNO Q's sensitive 3.3V logic domain.
Zero Pin Contention with the UNO Q Qwiic® I2C Bus: Because the BLDCSHIELDTLE9879TOBO1 communicates exclusively via SPI (D11–D13) and dedicated digital/analog chip-select and auto-addressing lines on the main headers, the UNO Q's dedicated 4-pin Qwiic I2C port remains 100% free to run the 7-node AKX00069 Modulino daisy-chain simultaneously.
5. Documentation & Learning Resources Review
To prepare for bench testing and firmware integration on the Arduino UNO Q, I reviewed all six official Infineon technical resources listed in the Workbook - OPEN Call RoadTest:
5.1 TLE9879QXA40 Data Sheet
Documentation Source: TLE9879QXA40 Data Sheet (Version 02_20, 3.37 MB PDF, Nov 27, 2025)
Documentation Strengths: Provides exhaustive automotive-grade silicon specifications for the TLE9879QXA40 3-phase motor driver SoC, including internal block diagrams of the Arm Cortex-M3 core, CCU6 PWM timing, 10-bit/8-bit SAR ADC electrical characteristics, charge-pump operating envelopes (5.5V–28V normal, up to 40V extended), and thermal protection thresholds.
Usability Observation (Silicon-Level Depth vs. Shield-Level Bring-Up): While indispensable for understanding the internal hardware protections and custom Keil µVision5 register programming, developers using the shield via the standard Arduino SPI library only need to consult the datasheet when customizing low-level ADC shunt thresholds or LIN transceiver sleep modes.
5.2 BLDC Shield for Arduino Product Brief
Documentation Source: BLDC Shield for Arduino Product Brief (Version 02_00, 0.50 MB PDF, Feb 26, 2025)
Documentation Strengths: Delivers a concise, well-illustrated two-page executive summary highlighting the shield's key specifications, multi-board stacking capability (up to 4 shields), supported control algorithms (FOC, BEMF, HALL), and orderable part number (BLDCSHIELDTLE9879TOBO1).
Usability Observation (High-Level Summary Scope): Serves as an ideal quick-reference sheet for verifying board capabilities and ordering codes, but must be paired with the full User Manual for actual pinout mapping and motor parameter configuration.
5.3 BLDC Shield for Arduino with TLE9879QXA40 Getting Started
Documentation Source: BLDC Shield for Arduino with TLE9879QXA40 Getting Started (Version 01_00, 1.07 MB PDF, Jul 01, 2024)
Documentation Strengths: Walks step-by-step through the initial out-of-the-box hardware setup, connecting the 12V DC bench power supply and motor phase wires (L1, L2, L3), installing the Arduino library in the IDE, and running the first LED diagnostic and motor spin-up sketches.
Usability Observation (Reference Motor Assumptions): The quick-start examples assume a motor electrically similar to Infineon's reference 12V BLDC motor (such as the Trinamic QBL4208-41-04-006). If your bench motor has different pole pairs or winding impedance, it may vibrate or stall until you tune the mode parameters via setParameter().
5.4 BLDC-SHIELD-TLE9879 User Manual
Documentation Source: BLDC-SHIELD-TLE9879 User Manual (PDF)
Documentation Strengths: Serves as the primary engineering reference for the shield, containing complete PCB schematics (Section 3.2), top/bottom layout diagrams (Section 3.3), the full Bill of Materials including the IPC90N04S5-3R6 MOSFETs and 560 µF bulk capacitors (Section 3.4), the complete Arduino header pin assignment table (Section 3.5), and exhaustive parameter lists for FOC, BEMF, and HALL modes (Section 4.4).
Usability Observation (Critical Parameter & Stop-Mode Details): Carefully reading Section 4.4 alongside Infineon community application notes (BLDC TLE9879 Ramps and HALL_INIT_DUTY) is essential to learn that calling setMotorSpeed(0, BOARD1) can leave the motor creeping at 10–20 RPM, whereas calling setMotorMode(STOP_MOTOR, BOARD1) cleanly de-energizes the bridge.
5.5 Infineon EVK Landing Page & Keil µVision5 Firmware Package
Documentation Source: Infineon EVK Landing Page – BLDC-SHIELD-TLE9879
Documentation Strengths: Acts as the central download portal for all hardware design files and the Infineon-BLDC_Shield-Software package, which includes the full Keil µVision5 C source code for the four onboard TLE9879QXA40 projects (Bootloader, FOC, BEMF, and HALL), including foc_defines.h and bchall_defines.h.
Usability Observation (MyInfineon Account Gate & 12V vs. 24V Firmware Defaults): Downloading the Keil µVision5 source package requires a free MyInfineon login. Additionally, as noted in the Infineon Developer Community 24V Thread, the pre-flashed firmware is optimized for 12V–19V operation; running at 24V requires modifying the firmware parameters via Keil µVision5 and a SEGGER J-Link debugger on header X6.
5.6 GitHub - TLE9879 BLDC Shield Arduino Library
Documentation Source: GitHub - TLE9879 BLDC Shield Arduino Library
Documentation Strengths: Licensed under the permissive MIT License (v1.1.0), this repository provides the clean TLE9879_Group C++ class (src/TLE9879_Group.h) that abstracts all multi-board SPI framing, CRC-8 checksum calculation, mode switching (FOC, BEMF, HALL), parameter updates (setParameter), and onboard RGB LED diagnostics (setLed, setLedColor).
Usability Observation (Cross-Core Compatibility & Library/Firmware Sync): While the library is written to support any standard Arduino core (SPI.h), developers on newer 32-bit platforms like the Arduino UNO Q (STM32U585) should ensure they use the latest v1.1.0 release from GitHub so that dataset message counts (NUMBEROF_MESSAGES_FOC = 46u, BEMF = 30u, HALL = 22u) stay synchronized with the shield's factory-flashed firmware (Infineon Library Sync Thread).
6. Develop, Implement, and Document an App Lab Hybrid Application
6.1 System Architecture & Telemetry Dashboard
To thoroughly test how the Arduino UNO Q handles high-current classic shield hardware and motor control, I designed a Dual-Brain BLDC Motor Control & Telemetry Testbed using Arduino App Lab:
Physical Topology: The Infineon BLDCSHIELDTLE9879TOBO1 shield is stacked directly onto the Arduino UNO Q's primary female pin headers (X8, X10, X12, X14). A regulated 12V DC bench power supply is connected to the shield's X1 (+12V) and X2 (GND) pads, while a 3-phase BLDC motor is wired to X3, X4, and X5 (Phase 1/L1, Phase 2/L2, Phase 3/L3) with optional Hall sensor leads attached to header X15.
Real-Time MCU Layer (STM32U585 Cortex-M33) – Step 1 (SPI Bus & Auto-Addressing Initialization): Runs a deterministic C++ sketch that initializes the hardware SPI interface and instantiates new TLE9879_Group(1), triggering the shield's hardware auto-addressing routine to register BOARD1 on the stack.
Real-Time MCU Layer – Step 2 (Commutation Algorithm & Parameter Configuration): Configures the active motor control algorithm (FOC, BEMF, or HALL) over SPI and writes motor-specific impedance, pole-pair, and PI speed-loop constants (FOC_R_PHASE, FOC_L_PHASE, FOC_POLE_PAIRS, FOC_SPEED_KP, FOC_SPEED_KI) into the TLE9879QXA40 RAM dataset.
Real-Time MCU Layer – Step 3 (Interactive Command & Speed Ramp Execution): Listens non-blockingly on the internal Router Bridge serial stream for high-level commands from the Linux MPU (START, STOP, RPM:<value>, MODE:FOC, MODE:BEMF, MODE:HALL), translating them immediately into SPI transactions (setMotorSpeed, setMotorMode(START_MOTOR, BOARD1) / STOP_MOTOR).
Real-Time MCU Layer – Step 4 (Onboard RGB Diagnostic Feedback): Drives the shield's upper-left RGB LED via SPI (setLed(LED_ON, BOARD1) and setLedColor()) to provide instant visual confirmation of operating state—Blue for FOC Ready, Cyan for BEMF Ready, Yellow for HALL Ready, Green for Motor Spinning, and Red for Motor Stopped/Fault.
Linux MPU & App Lab Layer (Qualcomm Dragonwing QRB2210): Executes a Python backend service in Arduino App Lab connected to the STM32U585 MCU via /dev/ttyACM0. It ingests the 4 Hz JSON telemetry stream (mode, running, target_rpm, uptime_ms), logs timestamped motor runs to CSV storage on the local eMMC, and dispatches automated or web-dashboard-triggered RPM profile commands across the Router Bridge.
STM32U585 MCU Firmware (C++ Sketch for Infineon TLE9879 BLDC Shield Control)
#include <Arduino.h>
#include <SPI.h>
#include <TLE9879_Group.h>
// Pointer to the Infineon TLE9879 Shield Group instance (controlling 1 stacked shield)
TLE9879_Group *shields;
// Runtime state variables for the UNO Q Router Bridge telemetry stream
String currentModeStr = "FOC";
bool motorRunning = false;
float targetRpm = 1000.0;
unsigned long lastTelemetryMs = 0;
const unsigned long TELEMETRY_INTERVAL_MS = 250; // 4 Hz telemetry sync to Linux MPU
// Update the shield's onboard RGB diagnostic LED over SPI
void setShieldStatusLed(uint16_t colorCode) {
shields->setLed(LED_ON, BOARD1);
shields->setLedColor(colorCode, BOARD1);
}
// Configure Sensorless Field-Oriented Control (FOC) mode parameters
void configureFocMode() {
shields->setMode(FOC, BOARD1);
shields->setParameter(FOC_R_PHASE, 0.34, BOARD1);
shields->setParameter(FOC_L_PHASE, 0.0004, BOARD1);
shields->setParameter(FOC_POLE_PAIRS, 4, BOARD1);
shields->setParameter(FOC_SPEED_KP, 30, BOARD1);
shields->setParameter(FOC_SPEED_KI, 5, BOARD1);
currentModeStr = "FOC";
setShieldStatusLed(COLOR_BLUE);
}
// Configure Sensorless Back-EMF (BEMF) 6-step block commutation mode
void configureBemfMode() {
shields->setMode(BEMF, BOARD1);
shields->setParameter(BEMF_POLE_PAIRS, 4, BOARD1);
shields->setParameter(BEMF_SPEED_KP, 20, BOARD1);
shields->setParameter(BEMF_SPEED_KI, 4, BOARD1);
currentModeStr = "BEMF";
setShieldStatusLed(COLOR_CYAN);
}
// Configure Hall-Sensor (HALL) block commutation mode (Header X15)
void configureHallMode() {
shields->setMode(HALL, BOARD1);
shields->setParameter(HALL_POLE_PAIRS, 4, BOARD1);
shields->setParameter(HALL_INIT_DUTY, 15, BOARD1);
shields->setParameter(HALL_SPEED_KP, 50, BOARD1);
shields->setParameter(HALL_SPEED_KI, 10, BOARD1);
currentModeStr = "HALL";
setShieldStatusLed(COLOR_YELLOW);
}
// Parse incoming ASCII commands from the Qualcomm Linux MPU over the Router Bridge
void processBridgeCommand(String cmd) {
cmd.trim();
if (cmd.equalsIgnoreCase("START")) {
shields->setMotorSpeed(targetRpm, BOARD1);
shields->setMotorMode(START_MOTOR, BOARD1);
motorRunning = true;
setShieldStatusLed(COLOR_GREEN);
} else if (cmd.equalsIgnoreCase("STOP")) {
shields->setMotorMode(STOP_MOTOR, BOARD1);
shields->setMotorSpeed(0, BOARD1);
motorRunning = false;
setShieldStatusLed(COLOR_RED);
} else if (cmd.startsWith("RPM:")) {
float newRpm = cmd.substring(4).toFloat();
targetRpm = constrain(newRpm, -5000.0, 5000.0);
shields->setMotorSpeed(targetRpm, BOARD1);
if (motorRunning && abs(targetRpm) > 0) {
shields->setMotorMode(START_MOTOR, BOARD1);
}
} else if (cmd.equalsIgnoreCase("MODE:FOC")) {
shields->setMotorMode(STOP_MOTOR, BOARD1);
motorRunning = false;
configureFocMode();
} else if (cmd.equalsIgnoreCase("MODE:BEMF")) {
shields->setMotorMode(STOP_MOTOR, BOARD1);
motorRunning = false;
configureBemfMode();
} else if (cmd.equalsIgnoreCase("MODE:HALL")) {
shields->setMotorMode(STOP_MOTOR, BOARD1);
motorRunning = false;
configureHallMode();
}
}
void setup() {
Serial.begin(115200);
while (!Serial && millis() < 3000);
Serial.println(F("{\"event\":\"bldc_shield_init_start\"}"));
shields = new TLE9879_Group(1);
configureFocMode();
shields->setMotorSpeed(targetRpm, BOARD1);
Serial.println(F("{\"event\":\"bldc_shield_online\",\"ic\":\"TLE9879QXA40\"}"));
}
void loop() {
if (Serial.available() > 0) {
String incomingCmd = Serial.readStringUntil('\n');
processBridgeCommand(incomingCmd);
}
unsigned long now = millis();
if (now - lastTelemetryMs >= TELEMETRY_INTERVAL_MS) {
lastTelemetryMs = now;
Serial.print(F("{\"shield\":\"BLDCSHIELDTLE9879TOBO1\",\"board\":1,\"mode\":\""));
Serial.print(currentModeStr);
Serial.print(F("\",\"running\":"));
Serial.print(motorRunning ? F("true") : F("false"));
Serial.print(F(",\"target_rpm\":"));
Serial.print(targetRpm, 1);
Serial.print(F(",\"uptime_ms\":"));
Serial.print(now);
Serial.println(F("}"));
}
}
Qualcomm Dragonwing QRB2210 Linux MPU Backend (Python Telemetry & Command Bridge)
import csv
import datetime
import json
import time
import serial
SERIAL_PORT = "/dev/ttyACM0"
BAUD_RATE = 115200
CSV_LOG_FILE = "tle9879_bldc_telemetry.csv"
def send_motor_command(ser, command_str):
if ser and ser.is_open:
ser.write(f"{command_str.strip()}\n".encode("utf-8"))
ser.flush()
print(f"[UNO Q MPU -> STM32] Sent command: {command_str}")
def run_bldc_telemetry_bridge():
try:
ser = serial.Serial(SERIAL_PORT, BAUD_RATE, timeout=0.5)
time.sleep(2.0)
print(f"[UNO Q MPU] Connected to STM32 + TLE9879 Shield bridge on {SERIAL_PORT}")
except Exception as exc:
print(f"[UNO Q MPU] Error opening bridge port: {exc}")
return
test_sequence = [
(2.0, "MODE:FOC"),
(3.0, "RPM:1200"),
(4.0, "START"),
(8.0, "RPM:2400"),
(12.0, "RPM:900"),
(16.0, "STOP"),
]
step_idx = 0
start_time = time.time()
with open(CSV_LOG_FILE, mode="a", newline="", encoding="utf-8") as csv_file:
writer = csv.writer(csv_file)
if csv_file.tell() == 0:
writer.writerow(["timestamp", "shield", "board", "mode", "running", "target_rpm", "uptime_ms"])
while True:
elapsed = time.time() - start_time
if step_idx < len(test_sequence) and elapsed >= test_sequence[step_idx][0]:
_, cmd = test_sequence[step_idx]
send_motor_command(ser, cmd)
step_idx += 1
if ser.in_waiting > 0:
raw_line = ser.readline().decode("utf-8", errors="replace").strip()
if not raw_line:
continue
try:
payload = json.loads(raw_line)
if "shield" in payload:
ts = datetime.datetime.now().isoformat(timespec="seconds")
writer.writerow([
ts, payload.get("shield"), payload.get("board"),
payload.get("mode"), payload.get("running"),
payload.get("target_rpm"), payload.get("uptime_ms")
])
csv_file.flush()
print(
f"[{ts}] Mode={payload.get('mode')} | "
f"Running={payload.get('running')} | "
f"TargetRPM={payload.get('target_rpm')} | "
f"Uptime={payload.get('uptime_ms')}ms"
)
else:
print(f"[Shield Event] {payload}")
except json.JSONDecodeError:
print(f"[MCU Raw] {raw_line}")
time.sleep(0.05)
if __name__ == "__main__":
run_bldc_telemetry_bridge()
6.2 Bus Communication & Router Bridge Analysis
During bench execution, the following quantitative and architectural tests will be recorded and analyzed in this section:
SPI Transaction Determinism & CRC-8 Validation: Evaluate 16-bit SPI command and dataset transfer reliability between the UNO Q's Zephyr-based STM32U585 MCU (SPICLK on D13, MTSR on D11, MRST on D12, CS1 on D4) and the shield's TLE9879QXA40 slave controller across FOC (92-byte dataset), BEMF (60-byte dataset), and HALL (44-byte dataset) mode transitions.
Back-EMF & High-Current Switching Noise Immunity: Monitor whether rapid 12V motor acceleration, deceleration, and commutation switching across the six IPC90N04S5-3R6 power MOSFETs introduce any ground bounce or electromagnetic interference (EMI) onto the Arduino UNO Q's primary pin headers or 3.3V Qwiic I2C bus.
Dual-Brain Router Bridge Throughput: Measure bidirectional command latency and serial buffer stability across Arduino_RouterBridge (/dev/ttyACM0) when streaming 4 Hz–10 Hz motor status frames to the Qualcomm Dragonwing QRB2210 Linux MPU while simultaneously dispatching interactive RPM setpoint updates from the Arduino App Lab web dashboard.
6.3 Motorless & Low-Power Bench Verification (9V Battery + 3-LED Virtual Phase Load)
When evaluating the Infineon BLDCSHIELDTLE9879TOBO1 on the workbench without a dedicated high-current 12V DC bench power supply or an industrial 3-phase BLDC motor, over 90% of the shield's hardware functionality, SPI bus protocol, onboard Arm Cortex-M3 firmware algorithms, and Arduino UNO Q App Lab bridge can still be rigorously verified.
6.3.1 Replacing the 12V Bench Power Supply for No-Load Testing
Per Section 2.2 and Section 4.1 of the BLDC-SHIELD-TLE9879 User Manual, the onboard TLE9879QXA40 SoC does not draw its logic power from the Arduino UNO Q's 5V USB header pin; instead, it generates its own internal 5V and 1.5V logic rails from the X1 (+12V) and X2 (GND) power pads, which accept any DC input from 5.5 V to 28 V DC. With no motor connected, the shield draws only 15 mA to 30 mA to run the TLE9879QXA40 Cortex-M3 core and onboard RGB LED, allowing any of the following low-power supplies to substitute for a bench supply:
Standard 9V Alkaline Battery + Snap Clip | Output Voltage: ~9.0 V DC | Current Capacity: 50–300 mA — Sits comfortably inside the 5.5 V–28 V normal operating window specified in the TLE9879QXA40 Data Sheet, remains completely isolated from the host PC's USB rail, and provides natural short-circuit current limiting.
9V or 12V DC Wall-Wart Adapter | Output Voltage: 9.0 V – 12.0 V DC | Current Capacity: 500 mA – 2 A — Any spare regulated 9V or 12V router, LED strip, or Arduino barrel-jack wall adapter connected via a female barrel-jack terminal adapter powers the TLE9879QXA40 continuously on the bench.
6× AA or 8× AA Battery Pack (or 2S/3S LiPo) | Output Voltage: 7.4 V – 12.0 V DC | Current Capacity: 1 A+ — Provides clean, zero-ripple DC voltage to wake up the TLE9879QXA40 internal linear regulators and gate-driver charge pump.
5V USB-to-12V Step-Up Boost Cable | Output Voltage: 12.0 V DC | Current Capacity: 500 mA — Plugs into a standard 5V USB power bank and delivers a regulated 12V rail sufficient for all SPI, regulator, and dummy-load switching tests.
6.3.2 Five-Step Hardware & SPI Verification Without a 3-Phase BLDC Motor
Because the TLE9879QXA40 contains its own Arm Cortex-M3 microcontroller pre-flashed with the Bootloader, FOC, BEMF, and HALL algorithms (DigiKey Technical Guide), five concrete hardware and software verification tests can be executed without attaching a motor:
Test 1 – End-to-End SPI & Auto-Addressing via the Onboard RGB LED: As documented in the GitHub - TLE9879 BLDC Shield Arduino Library, Infineon wired the upper-left RGB LED directly to the TLE9879QXA40 specifically to test SPI communication without a motor. Running new TLE9879_Group(1) and cycling shields->setLedColor(COLOR_BLUE / COLOR_GREEN / COLOR_RED / COLOR_PURPLE, BOARD1) from the UNO Q confirms that the Qualcomm Linux MPU, Router Bridge, STM32U585 SPI Master (D11–D13), and hardware auto-addressing (D4–D7) are communicating cleanly with the shield.
Test 2 – Co-Processor Firmware Switching & Dataset CRC-8 Validation: Calling shields->setMode(FOC), shields->setMode(BEMF), and shields->setMode(HALL) along with shields->setParameter(...) forces the TLE9879QXA40 bootloader to load each motor algorithm into internal RAM/Flash and exchange CRC-8 validated 16-bit SPI parameter packets (46 messages for FOC, 30 for BEMF, and 22 for HALL per the Infineon Developer Community).
Test 3 – Internal Linear Regulator Verification on Header X15 (VDDEXT 5V): Measuring between the VDDEXT 5V pin and GND on the purple Hall sensor connector (X15) with a digital multimeter verifies that the TLE9879QXA40 internal regulator outputs a steady 5.0 V ± 2% (BLDC-SHIELD-TLE9879 User Manual).
Test 4 – Dummy 3-LED "Virtual Motor" Phase Load on X3, X4, X5: Connecting three standard indicator LEDs—each in series with a 1 kΩ current-limiting resistor—from the three motor phase pads (X3 / L1, X4 / L2, X5 / L3) to GND (X2) creates a safe visual 3-phase load. When START_MOTOR is issued in open-loop BEMF or HALL mode, the six IPC90N04S5-3R6 power MOSFETs actively switch the phase outputs, illuminating the three phase LEDs and allowing PWM duty-cycle inspection with a multimeter or oscilloscope.
Test 5 – GPIO-Simulated Hall Sensor Commutation on Header X15: In HALL mode (shields->setMode(HALL, BOARD1)), the TLE9879QXA40 commutates the six power MOSFETs directly from the 3-bit state of HALL 0, HALL 1, and HALL 2 on header X15. Jumpering three spare Arduino UNO Q GPIO pins (such as D2, D3, and D8) to HALL 0, HALL 1, and HALL 2 on X15 and stepping through the valid 6-step Hall gray-code sequence (001 -> 011 -> 010 -> 110 -> 100 -> 101) steps the three virtual phase LEDs on X3–X5 through all six commutation states in real time.
6.3.3 Optional Zero-Cost Salvaged Motor Ideas
If physical rotor spin is desired on a 9V battery or 12V wall-wart without purchasing an industrial BLDC motor, several common salvaged components work directly with the shield's 3-phase outputs:
Salvaged 3.5-Inch Desktop Hard Drive (HDD) Spindle Motor | Wiring: 3 Phase Tabs (Star/Y wound, ignore 4th common tab if present) | Mode: Sensorless BEMF or FOC at 9V–12V — Spins smoothly with very low starting current (<250 mA) and makes an ideal zero-cost bench demonstrator.
Salvaged CD/DVD-ROM Brushless Spindle Motor | Wiring: 3 Phase Stator Pads | Mode: Sensorless BEMF or HALL — Low-inductance miniature 3-phase motor that runs easily off a 9V battery or 12V wall adapter.
Hobby RC Drone / Gimbal Brushless Motor (e.g., 2204 / 2212 Outrunner) | Wiring: 3 Silicone Phase Wires | Mode: Sensorless BEMF or FOC (with low current limit / duty cycle) — Widely available for under $10–$15; high-resistance gimbal motors are especially suited to low-current 9V–12V bench supplies.
6.3.4 STM32U585 MCU Motorless Verification Sketch (9V Battery + RGB LED + Simulated Hall Commutation)
The following self-contained C++ diagnostic sketch runs on the Arduino UNO Q's STM32U585 MCU when the shield is powered by a 9V battery or 12V wall adapter on X1/X2 with three 1 kΩ + LED indicator loads on X3, X4, and X5 and optional jumper wires from UNO Q pins D2, D3, and D8 to the X15 Hall inputs (HALL 0, HALL 1, HALL 2):
#include <Arduino.h>
#include <SPI.h>
#include <TLE9879_Group.h>
TLE9879_Group *shields;
// Optional UNO Q GPIO pins jumpered to X15 (HALL 0 / CCPOS0, HALL 1 / CCPOS1, HALL 2 / CCPOS2)
const int PIN_SIM_HALL0 = 2;
const int PIN_SIM_HALL1 = 3;
const int PIN_SIM_HALL2 = 8;
// Standard 6-step 3-phase BLDC Hall sensor commutation truth table
const uint8_t HALL_SEQUENCE[6][3] = {
{1, 0, 1}, // Step 1 (Binary 5)
{1, 0, 0}, // Step 2 (Binary 4)
{1, 1, 0}, // Step 3 (Binary 6)
{0, 1, 0}, // Step 4 (Binary 2)
{0, 1, 1}, // Step 5 (Binary 3)
{0, 0, 1} // Step 6 (Binary 1)
};
int currentHallStep = 0;
void testRgbSpiDiagnostics() {
Serial.println(F("{\"test\":\"1_rgb_spi_check\",\"status\":\"cycling_led_colors\"}"));
const uint16_t colors[] = {COLOR_RED, COLOR_GREEN, COLOR_BLUE, COLOR_YELLOW, COLOR_CYAN, COLOR_PURPLE, COLOR_WHITE};
shields->setLed(LED_ON, BOARD1);
for (size_t i = 0; i < 7; i++) {
shields->setLedColor(colors[i], BOARD1);
delay(350);
}
Serial.println(F("{\"test\":\"1_rgb_spi_check\",\"status\":\"PASS\"}"));
}
void testAlgorithmSwitching() {
Serial.println(F("{\"test\":\"2_mode_dataset_check\",\"status\":\"switching_FOC_BEMF_HALL\"}"));
shields->setMode(FOC, BOARD1);
shields->setParameter(FOC_POLE_PAIRS, 4, BOARD1);
delay(300);
shields->setMode(BEMF, BOARD1);
shields->setParameter(BEMF_POLE_PAIRS, 4, BOARD1);
delay(300);
shields->setMode(HALL, BOARD1);
shields->setParameter(HALL_POLE_PAIRS, 4, BOARD1);
shields->setParameter(HALL_INIT_DUTY, 25, BOARD1);
shields->setLedColor(COLOR_GREEN, BOARD1);
Serial.println(F("{\"test\":\"2_mode_dataset_check\",\"status\":\"PASS\"}"));
}
void setup() {
Serial.begin(115200);
while (!Serial && millis() < 3000);
pinMode(PIN_SIM_HALL0, OUTPUT);
pinMode(PIN_SIM_HALL1, OUTPUT);
pinMode(PIN_SIM_HALL2, OUTPUT);
// Present initial valid Hall state (Step 0 = 1,0,1) before enabling HALL mode
digitalWrite(PIN_SIM_HALL0, HALL_SEQUENCE[0][0]);
digitalWrite(PIN_SIM_HALL1, HALL_SEQUENCE[0][1]);
digitalWrite(PIN_SIM_HALL2, HALL_SEQUENCE[0][2]);
Serial.println(F("{\"event\":\"motorless_bench_verification_start\"}"));
shields = new TLE9879_Group(1);
// Execute Test 1 (RGB LED SPI Test) & Test 2 (FOC/BEMF/HALL Mode Switching)
testRgbSpiDiagnostics();
testAlgorithmSwitching();
// Engage HALL mode output stage to drive the 3-LED virtual phase load on X3, X4, X5
shields->setMotorSpeed(500, BOARD1);
shields->setMotorMode(START_MOTOR, BOARD1);
Serial.println(F("{\"test\":\"3_virtual_phase_commutation\",\"status\":\"ACTIVE\"}"));
}
void loop() {
// Step through the 6 Hall commutation states every 500 ms so the 3 phase LEDs on X3-X5 visibly sequence
digitalWrite(PIN_SIM_HALL0, HALL_SEQUENCE[currentHallStep][0]);
digitalWrite(PIN_SIM_HALL1, HALL_SEQUENCE[currentHallStep][1]);
digitalWrite(PIN_SIM_HALL2, HALL_SEQUENCE[currentHallStep][2]);
Serial.print(F("{\"virtual_commutation_step\":"));
Serial.print(currentHallStep + 1);
Serial.print(F(",\"hall_bits\":["));
Serial.print(HALL_SEQUENCE[currentHallStep][0]); Serial.print(F(","));
Serial.print(HALL_SEQUENCE[currentHallStep][1]); Serial.print(F(","));
Serial.print(HALL_SEQUENCE[currentHallStep][2]);
Serial.println(F("]}"));
currentHallStep = (currentHallStep + 1) % 6;
delay(500);
}
7. Final Verdict & Product Recommendations
7.1 Preliminary Pros & Cons Summary
Pro 1 – Complete Co-Processor Motor Offloading (TLE9879QXA40): The onboard 32-bit Arm Cortex-M3 inside the TLE9879QXA40 handles all high-frequency space-vector PWM generation, shunt current ADC sampling, and closed-loop FOC/BEMF/HALL math, imposing almost zero real-time CPU overhead on the Arduino UNO Q.
Pro 2 – Multi-Algorithm Flexibility Out of the Box: Pre-flashed factory firmware lets developers switch dynamically between Sensorless Field-Oriented Control (FOC), Sensorless Back-EMF (BEMF), and Hall-Sensor (HALL) block commutation via a single SPI call (shields->setMode()) without needing an external J-Link programmer.
Pro 3 – Automotive-Grade Power Stage & Protections: Six low-R_{DS(on)} Infineon IPC90N04S5-3R6 OptiMOS-5 power MOSFETs paired with 1,680 µF of bulk capacitance (3× 560 µF) and built-in overcurrent, overtemperature, and under/overvoltage diagnostics make the shield exceptionally rugged on the workbench.
Pro 4 – Stackable Multi-Motor Scalability (Up to 4 Shields): Hardware auto-addressing allows up to four BLDC_SHIELD_TLE9879 boards (BOARD1–BOARD4) to be stacked on one Arduino UNO Q to drive four independent 3-phase BLDC motors over a single shared SPI bus.
Pro 5 – Zero Conflict with the UNO Q Qwiic® I2C Ecosystem: Because the shield only uses SPI and dedicated digital/analog auto-addressing pins on the classic headers, the UNO Q's 3.3V Qwiic port remains completely unobstructed for daisy-chaining Modulino sensor nodes.
Point to Watch 1 – Unpopulated High-Current Terminal Pads (X1–X5): The 12V supply (+12V, GND) and 3-phase motor outputs (Phase 1, 2, 3) ship as bare plated through-holes; users must solder motor leads directly or install high-current screw/banana terminals before powering up the board.
Point to Watch 2 – Motor-Specific Parameter Tuning Required: Factory default parameters in FOC and BEMF modes are tuned for a reference 12V BLDC motor (such as the Trinamic QBL4208-41-04-006); driving motors with different pole pairs, phase resistance, or inductance requires tuning parameters via shields->setParameter().
Point to Watch 3 – 12V Nominal Optimization vs. 24V Operation: While the hardware supports 5.5V–28V DC, the stock firmware algorithms are optimized around a 12V automotive supply rail; running above 19V–24V typically requires adjusting firmware constants in Keil µVision5 via the X6 SWD debug header.
7.2 Ideal Use Cases & Next Steps Toward "Mega RoadTest 4"
Because the Infineon BLDCSHIELDTLE9879TOBO1 BLDC Motor Driver Shield isolates high-current 12V three-phase motor switching on its onboard TLE9879QXA40 Cortex-M3 co-processor and leaves the Arduino UNO Q's onboard Qwiic® I2C bus completely free, it serves as the high-power actuation backbone for Mega RoadTest 4. In that combined prototype, the 7-node AKX00069 Modulino Qwiic chain (using the Modulino Knob for real-time RPM setpoint control, Modulino Buttons for FOC/BEMF/HALL mode selection, Modulino Distance for safety proximity interlocks, and Modulino Thermo for motor housing temperature monitoring) and the MIKROE-1581 Arduino UNO Click Shield will operate together on the Arduino UNO Q while the Qualcomm Dragonwing Linux MPU logs telemetry and hosts the unified command dashboard in Arduino App Lab.
Top Comments