RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs POST 8 A case in point...Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: colporteur
  • Date Created: 11 Oct 2026 8:12 PM Date Created
  • Views 50 views
  • Likes 8 likes
  • Comments 7 comments
Related
Recommended
  • RoadTest
  • test equipment
  • red pitaya

POST 8 A case in point...Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit

colporteur
colporteur
11 Oct 2026

Recall from an earlier post, that I had ordered and then reordered a case for the Red Pitaya. The first case ordered from a local supplier, wasn’t compatible with the RoadTest unit. It would have been nice if compatibility was mentioned during ordering. It seems the Red Pitaya STEMlab 125-14 PRO Gen 2 needs its own unique case. It took a member from the E14 community to find and identify the case. My search skills are not up to par. I looked and couldn’t find the unit.

In Canadian dollar it was $148 to purchase. Duties and tariffs added another $25. Returning the wrong case cost me $29 in restocking charges. All in, a little over $200 for the case.

What rubs me the wrong way is that, Red Pitaya recommends using a case in their documentation but didn’t provide one as part of the RoadTest.

No case concerned me from the beginning. The Red Pitaya PCB exposed to my test bench had a high probability of being shorted out coming in touch with something metal.

image

After the unit was dragged off the bench due to the weight of cables, I used the pinout card to isolate and expand the surface area of the PCB using a piece of wire.

Adding the cable drag option didn’t relieve my concern of the unit being to hot to touch during operation. The metal case is designed to be heat sink as well.

image

Without the case the temperature at the heat sink was 53.1C. With the Red Pitaya wrapped in a case the temperature is down close to ten degrees at 44.5C.

I'm happy with the case. Well reasonably happy. The connectors are labeled on the PCB. You lose the labeling when enclosed in the case.

image

It seems the Red Pitaya STEMlab 125-14 PRO Gen 2 case doesn't need labels. The case on left wasn't physically compatible but it did include labels.

I'm not sure I want to test plugging the power cable the far right USB-C into the Serial console USB-C connector under the RJ45 jack. I think I'm going to break out the label maker for my new case.

  • Sign in to reply
  • obones
    obones 1 day ago in reply to shabaz

    Apart from the visual aspect that some may find pleasing, there is one advantage that I can see:

    When using the oscilloscope probe adapter, it would be impossible to place your fingers properly to connect the probe if the connectors were all parallel to each other.
    The current arrangement gives more room to manipulate those things by hand.

    But I agree that it makes life more difficult when designing mating boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 2 days ago

    I don't like the curvy edge where the RF connectors are. Makes no sense to me (just makes it harder to mate circuitry onto it, when they are at an angle. Difficult enough to screw things on right when they are properly at 90 degrees, and for this sort of board I can imagine some users would want to fit a PCB directly without cables in-between. Other high-speed hardware manages straight connectors, they could have too. Plus makes the enclosure need to also be an annoying shape, so it's a knock-on effect all round. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<