RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Roadtest Part 2 Keithley DMM6500 --Measure low current of Solar Panel
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 26 Feb 2019 7:23 PM Date Created
  • Views 2072 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended
  • 6.5 digit dmm
  • dmm
  • keithley
  • keithley dmm6500

Roadtest Part 2 Keithley DMM6500 --Measure low current of Solar Panel

snidhi
snidhi
26 Feb 2019

This blog is a continuation from Keithley Bench Digital Multimeter - Review

 

This is an experiment to measure the low current of the solar panels. I have a single solar panel of 5V and roughly 500 mA current output capability. I want to test them under different minimum light conditions to see the lower currents in the solar panel. This is to analyze the current output of the solar panels in milliamps range. As I have not put the solar panels in the sunlight I have not used any protection diode or current limiting resistor at the measurement output.

 

image

The initial test setup

 

image

Fig: Here I have tested the changing current of the solar panel with a yellow light bulb source

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Conclusion: As one can see low current measurements with high accuracy is an important feature of benchtop multimeters. I plan to use the Keithley DMM6500 extensively in my future solar panel based projects

  • Sign in to reply

Top Comments

  • geralds
    geralds over 7 years ago +1
    It's a fine feature! - dual display, numeric and graphic diagram Best Regards Gerald --
  • snidhi
    snidhi over 7 years ago in reply to geralds

    yes, it is a wonderful device. A heavenly device for low current measurements

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 7 years ago

    It's a fine feature! - dual display, numeric and graphic diagram

     

    Best Regards

    Gerald

    --