RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs TI SWIFT™︎ Power Module EVM Review: Part 3 Analog tests of the Power Module
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 2 Apr 2018 11:26 AM Date Created
  • Views 3094 views
  • Likes 3 likes
  • Comments 19 comments
Related
Recommended
  • low noise regulator
  • high-current
  • dcdc converters
  • dcdc buck regulator
  • switching frequency
  • power efficiency

TI SWIFT™︎ Power Module EVM Review: Part 3 Analog tests of the Power Module

snidhi
snidhi
2 Apr 2018

Part 2: Test the analog features of the TPSM84A21 EVM

 

To be Tested Features of TPSM84A21:

  1. Output voltage ripple measurements (with and without external capacitors)
  2. Tests at high output current with external load
  3. The Vin, Vout and PGOOD start up waveforms
  4. The Vin, Vout and PGOOD shutdown waveforms

 

Features of TPSM84A21 IC:

  1. Ultra-Fast Load Step Response
  2. Efficiencies up to 88%
  3. 1% Output Voltage Accuracy
  4. 4 MHz Switching Frequency
  5. Synchronizes to an External Clock
  6. Power Good Output
  7. Pre-Bias Output Start-Up
  8. Programmable Under-Voltage Lockout (UVLO)

 

Output voltage ripple measurements (without external capacitors)

 

Using the reference below Understanding, Measuring, and Reducing Output Voltage Ripple

Probe Sensitivity – Using 10X vs 1X Probes: When trying to measure signals in the sub ~10mV range, using a 10x probe is not appropriate. The sensitivity of the probe is not high enough to have a clean signal reading. A simple 1x probe should be used for measurements under 10mV.

 

Measurement Conditions in the oscilloscope:  1x probe settings, Noise Reject ON, LPF ON, No o/p load, BW limit set 20MHz, MEMDepth 70Mpoints, AC Coupling, 1Mohm input impedance. Ch1: Vin Yellow Ch2: Vout Blue, Measurement cable from the EVM to the scope is a RF cable 1x with BNC.

 

The Vout ripple is also load dependent but here the measurements where done without external load

 

image

Data-sheet Preview

image

Without Filtering Capacitors at the input and output For Vin = 7.969V

image

Without Filtering Capacitors at the input and output For Vin = 10V

image

Without Filtering Capacitors at the input and output For Vin = 14V

 

One can conclude from these results that there is a slow rise in the output ripple from 5 mVpp to 8mVpp. But still it is low in comparison to other fast switching DC/DC converter.

 

Output voltage ripple measurements (with external capacitors)

 

Measurement Conditions in the oscilloscope: Noise Reject ON, LPF ON, No o/p load, BW limit set 20MHz, MEMDepth 70Mpoints, AC Coupling, 1Mohm input impedance. Ch1: Vout Yellow After filtering capacitors  Ch2: Vout Blue measured before filtering capacitors.

 

image

 

Tests at High output current with external load: Very short cables were use to connect from Rload to the DMM.

The measurements were also verified using shunt resistance of 0.01 ohm at the oscilloscope.

 

 

image

 

 

VinVout Measured

RLoad

cement Resistor +

Burden resistance of Fluke 179

Output Load current

calculated

Output Load current

Measured

@8V,10V,14V1.2V0.5ohm +0.037ohm = 0.537 ohm2.234 Amp2.263 Amp
@8V,10V,14V1.1V0.5ohm +0.037ohm = 0.537 ohm2.0484 Amp2.055 Amp
@8V,10V,14V1V0.5ohm +0.037ohm = 0.537 ohm1.862 Amp1.891 Amp
@8V,10V,14V0.8V0.5ohm +0.037ohm = 0.537 ohm1.489 Amp1.502 Amp
@8V,10V,14V0.6V0.5ohm +0.037ohm = 0.537 ohm1.1173 Amp1.128 Amp
@8V,10V,14V0.500V0.5ohm +0.037ohm = 0.537 ohm0.9310 Amp0.955 Amp

 

The device closely delivers the required output current although one can see a decline as the current requirement increases. The measured output current remains stable for Vin voltages from 8V to 14V.

 

Rload = 0.1 Ohm

image

 

 

 

Vin

Vout +

Burden voltage 37mV/A

RLoad

21W Resistor + 0.037ohm

Output Load current

calculated

Output Load current

Measured

@8V,10V,14V1.2V0.1 ohm + 0.037 ohm = 0.137ohm
8.759 Amp8.351 Amp
@8V,10V,14V1.1V0.1 ohm + 0.037 ohm = 0.137ohm8.029 Amp7.61 Amp
@8V,10V,14V1.0V0.1 ohm + 0.037 ohm = 0.137ohm7.299 Amp7.1 Amp
@8V,10V,14V0.8V0.1 ohm + 0.037 ohm = 0.137ohm5.8394 Amp5.584 Amp
@8V,10V,14V0.6V0.1 ohm + 0.037 ohm = 0.137ohm4.379 Amp4.211 Amp
@8V,10V,14V0.5V0.1 ohm + 0.037 ohm = 0.137ohm3.649 Amp3.565 Amp

 

 

In both the tests, the resistor became very hot very quickly. I had to turn off the setup after sometime to avoid any melting situation. Even with the 21Watt 0.1 ohm the device turns quite hot. At high current and for low Vout the efficiency of the converter is as mentioned in the datasheet. The measured output current remains very stable for Vin voltages from 8V to 14V.

 

Another important conclusion can be derived here that the difference between the calculated load current and actual measured load current also increases drastically to around 300 mA when loads start drawing current higher than 7.5Amp.

Although the deviation of  Measured current@load from Calculated current value@load for 1Amp to 7Amp was only in the order of 20mA which can be understood as drawn by additional cable resistance.

 

The Vin, Vout and PGOOD Start up waveforms

Setup: Vin = 10V, Vout = 500mv Iout = 1A, Rload = 0.5ohm

image

The Vin and Vout rise times are comparable to those in the datahseet. Vin@6ms; Vout@4ms; PGood has a steep slope. One can see here that the PGOOD signal in ON only when the Vout reaches its stable output voltage~99%. Whereas Vout start rising when reached around 7V. And Vout has a faster rise time.

 

The Vin, Vout and PGOOD shutdown waveforms

Setup: Vin = 10V, Vout = 500mv Iout = 1A, Rload = 0.5ohm

image

The shutdown waveforms were rather difficult to catch as they should be measured in the 200ms/div window and not in 200us/div(as in the datasheet)

Vout and Pgood have a sharp falling edge but the Vin signal takes around 2 sec to fully get to the base level.

 

Short Conclusion: The TPSM84A21 is good device with fast output rising voltages. It is able to drive higher currents consistently even with as low as 8Vin and 1.2Vout without any issues. But it falls short in achieving a higher efficiency at high load currents at low input voltage. The voltage output ripple is well under control (less than 20mV) even in high current range which is pretty good. 

 

 

References:

Power Tips: Measuring Vout Ripple in DC/DC Converters

Power Tips: Simply estimate load transient response

Understanding, Measuring, and Reducing Output Voltage Ripple

Line and Load Transient Testing for Power Supplies

 

 

TI SWIFTTm Power Module EVM Review: Part 2 Test Setup Description

TI SWIFTTmPower Module EVM Review:  Part 4 Dynamically adjust the output voltage using external DAC

Go Back To: Road Test Review of TPSM84A21 Power Module

  • Sign in to reply

Top Comments

  • hlipka
    hlipka over 8 years ago in reply to fmilburn +2
    The measured effect here is that the multimeter used for current measurement has a burden voltage due to its internal shunt. For the Fluke 179, this is (in the 10A range) 37mV/A - that is, 370mV for 10A…
  • snidhi
    snidhi over 8 years ago in reply to hlipka

    Hi, ahh now I understand why I was not able to match the voltage result what I saw across my 0.01 ohm shunt in the oscilloscope didn't match closely to the value in the Fluke DMM. I forgot to add the burden voltage to the DMM measurement.

     

    I will also share results from the scope measurements although I wasn't able to minimize the cable length any further hence not able to control the wire resistance.

    How to deal with the extraordinary levels of heating of the 21Watt resistor? I am already way above the Pwatt= 1.2x10A = 13Watt range (almost double to it) in my choice of the resistor? Any ideas on that?

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago in reply to hlipka

    Thanks, clear explanation and I see the arrangement in the photogragh now Which I previously missed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 8 years ago in reply to fmilburn

    The measured effect here is that the multimeter used for current measurement has a burden voltage due to its internal shunt. For the Fluke 179, this is (in the 10A range) 37mV/A - that is, 370mV for 10A - which would be nearly 1/3rd of the output voltage.

    When you take into account that the actual load resistance is not 100mOhm, but 137mOhm, you will find that the expected output current is indeed 8.76A at 1.2V, and 3.65A at 0.5V - which is quite close to the measured value. The remaining difference is easily explained by all the additional resistance in the current path (such as the wires themselves, and the banana jacks.

    The conclusion that the device cannot deliver its rated output current is wrong. When you want to measure correctly measure the voltage across your load resistor (using a kelvin connection), and calculate the current from there (provided that you measured its resistance precisely beforehand).

    When you do the math, you will find that just connecting the Fluke179 in 10A mode to the output should deliver about 13.5A, when taking into account the additional resistance probably a little bit less than that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago

    Even with the 21Watt 0.1 ohm it can concluded that the device struggles to deliver the output current hence once can say that at high currents the efficiency of the device is low.

    Hi,

     

    Regarding above, is the efficiency less than that given in the datasheet?  My measurements up to 8 amps were equal to or better than the datasheet.  Or, does it mean the device cannot deliver rated current?  Also, do you suspect any change in resistance in the load due to heating which would impact observed Vs expected values.

     

    Regards,

    Frank

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<