RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs What Would You do with this MicroPython Single Board Computer and What Would You Need to Do it?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: rscasny
  • Date Created: 15 Feb 2021 5:55 PM Date Created
  • Views 3474 views
  • Likes 7 likes
  • Comments 10 comments
Related
Recommended
  • scasny

What Would You do with this MicroPython Single Board Computer and What Would You Need to Do it?

rscasny
rscasny
15 Feb 2021

I plan on roadtesting thw Trinamic TMCM-0960-MotionPy Single Board Computer at the end of February. Before I launched the roadtest page, I have asked for some community feedback ( Top Members  Top Members ) and I also wanted to get a conversation going with members who would be interested in roadtesting this board.

 

So, what do you think of this board? What are your thoughts about roadtesting it? Besides the board, what other things do you think would be helpful to roadtest or build something with this board?

 

As always, I appreciate the time and input you provide me to make the RoadTest program a success.

 

Here are the high points about the board:

 

The TMCM-0960-MotionPy board is an open-source single board computer running MicroPython. It comes with several communication interface options like CAN, RS485, UART, and separate GPIO headers. With a wide supply voltage range of +6...+50V and industrial Fieldbus interfaces it is the engineers’ swiss army knife for small automation applications. Plugging directly into the application for logging data on an SD card or updating subsystems without the need for additional tools, the module offers a total of 13 functions in Python programming language for ease of use.

ximage

I've attached the hardware manual.

 

Additional Information

  • TMCL Firmware V1.0
  • ECAD Files V1.6
  • 3D Model V1.6
  • PyTrinamic Python Library (GitHub)
Attachments:
imageTMCM-0960-MotionPy_HW_Manual_V10 (1) (1).pdf
  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 5 years ago +3
    Great idea RS rscasny ,on polls for possible reviews. I find the community members that make posts, provide details I may not have thought about. It also encourages me to contribute by posting something…
  • colporteur
    colporteur over 5 years ago +2
    I like to see a RoadTest that exercised the card options. How many of the interfaces are out of the box usable or would require something else to work. "Plugging directly into the application for logging…
  • Gough Lui
    Gough Lui over 5 years ago +2
    I normally associate Trinamic with motor control stuff, which is why I was a bit confused with this board (where does the motor go?) since it's actually more of a MicroPython-enabled STM32F405RGT6 microcontroller…
  • mayermakes
    mayermakes over 5 years ago

    I immediately jumped on this page when I read Single board computer..but that is a bit misleading in my opinion, it is an STM32 microcontroller board .

    Being able to run micropython or circuitpython does not make it a single board computer. From the term I expected it tu run an OS like linux on which I could implement python programms.
    or any RTOS more specific to trinamic typical applications.

    If this board would qualifiy as an SBC than my EI.O.T Episode 485: How To Make A Custom PCB From Design To Assembly

    would also be an SBC and it clearly is not.

     

    I like the products features in general but the wording is misleading. EDIT: it even Says MCU in the block diagram. so I think the marketing department made that goof.

     

    On first glance its a MCU plattform with the interfaces broken out that trinamic drivers and other products use. I'm a bit inclined to build upon it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago

    Great idea RS rscasny ,on polls for possible reviews.

     

    I find the community members that make posts, provide details I may not have thought about. It also encourages me to contribute by posting something I have discovered or question I might have.

     

    It could be suggested this information could be done on the RoadTest review posting. On the RoadTest review page, I find I'm more focused on the application and not on the finer details of research.

     

    Polls are the think tank of ideas.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • parasquid
    parasquid over 5 years ago in reply to parasquid

    dougw image  Feb 16, 2021 1:32 PM (in response to Gough Lui)

    Trinamic has a bunch of motor controllers that use CANBUS, RS485 and USB. Presumably this would add some smarts to those products.

    Perhaps one of those would be a better pairing than an arduino shield.

    Just saw this, yeah I would agree that any of these would be great in an actual roadtest as this seems to be the product intention.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • parasquid
    parasquid over 5 years ago in reply to parasquid

    I'm also not sure why they call it a single board computer, as that gives some connotation that it's on a similar platform as the raspberry pi or nvidia jetson.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • parasquid
    parasquid over 5 years ago in reply to parasquid

    That said, there seems to be only three gpio available (PA4, PC0 and PC1) so it's kinda limited in that regard. Then again, this doesn't seem to be a dev or eval board, so I guess it's meant for applications with a max requirement of 3 gpio ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>