RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Which would you get Rasberry PI 2 or Gizmo 2 and why?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 2668 subscribers
  • Views 1942 views
  • Users 0 members are here
Related

Which would you get Rasberry PI 2 or Gizmo 2 and why?

libernullmal
libernullmal over 11 years ago

Just curious between the two and I wanted to know what the pros and cons between the two?

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 11 years ago in reply to shabaz +2
    Even mSATA might require some soldering, if the device is "non-compliant" http://www.element14.com/community/community/designcenter/single-board-computers/gizmo2/blog/2015/01/30/gizmo2-installing-ssd-and…
  • dtsartsanis
    dtsartsanis over 11 years ago +1
    Gizmo 2 is using a x86 processor which means that u can install windows.So if u are not familliar with Linux software and u can spend $199 go for it. Raspberry Pi 2 now is a complete pc in a compact size…
  • najath
    najath over 11 years ago in reply to clem57 +1
    I tried Chromium on another ARM board - SABRE Lite which I had obtained thanks to element14 . The ARM board is good enough for most use cases. But unfortunately pepper-flash was not available packaged…
  • clem57
    clem57 over 11 years ago

    To start, it really depends on what you want to do, With that said, I would go with Raspberry Pi 2 because it only uses 5 watts while the Gizmo’s  10 watts. The Pi can handle video streaming very well hitting 30 fps at 1080p. Now with more memory things get even more flexible. Check out this blog What are you doing for Pi day? 3.14.15 (US) which shows different boards calculating Pi. Sorry no Gizmo and only one processor is tested, but you can get a feel for changing to newer ARM7 instead of older ARM6/

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dtsartsanis
    dtsartsanis over 11 years ago

    Gizmo 2 is using a x86 processor which means that u can install windows.So if u are not familliar with Linux software and u can spend $199 go for it.

    Raspberry Pi 2 now is a complete pc in a compact size, with a lot documentation and tutorials from the community and it costs almost nothing.

    I choose Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to dtsartsanis

    dtsartsanis I beg to differ. Linux software knowledge is not a prerequisite for Raspberry Pi. He could download and install Openelec. Start it and be in full screen without typing any Linux command. Openelec  turns the Raspberry Pi into a media center playing movies on USB or off the internet.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dtsartsanis
    dtsartsanis over 11 years ago in reply to clem57

    Yes i agree, but if u want to use it as a pc u have to install software through the command line or install Synaptic.And is not always easy for windows users to use the command line.

    For me Raspi is a great tool to learn and explore Linux and other great projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • najath
    najath over 11 years ago

    As others have mentioned, the big advantage of Raspberry Pi over gizmo2 is the low power consumption.

     

    But still I would prefer a Gizmo2 for use as a PC because of the x86 architecture. Accessing internet would be one of the main use cases as a PC. Like it or not, many websites still have flash content. The support for flash on ARM architecture has been stopped for quite some time. Flash plugin taken from chromebook can be found online, but those could be big security risk. The only secure and supported flash plugin seems to be the pepper-flash plugin developed for chrome/chromium, and they are AFAIK available only for x86

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to najath

    Google Chrome cannot be installed on Raspberry Pi, because Google does not have support for Linux/ARM.

    But Chromium, the open-source version of Google Chrome can be installed on a Raspberry Pi box, for both Arch Linux and Debian:

     

    I got this quote from a good source najath. So you are kinda of right, unless you consider Chromium. I plan on trying soon and will let you know how flash works.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • najath
    najath over 11 years ago in reply to clem57

    I tried Chromium on another ARM board - SABRE Lite which I had obtained thanks to element14. The ARM board is good enough for most use cases. But unfortunately pepper-flash was not available packaged for ARM devices. I used one that I got after an online search, and which was extracted from a chromebook. It worked reasonably well too. But for each update, I had to search the web for finding the latest version.

     

    Later I got an Intel NUC with Atom processor. So now I'm experimenting with it and have set it up as my home cloud and entertainment platform.

     

    If you find a simple and secure way of getting flash work on ARM devices, do let me know. I can then make some use of the SABRE Lite board

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to najath

    Ok! I will play for a few days and let you know.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • libernullmal
    libernullmal over 11 years ago

    I'm not really worried about the low powered consumption. the thing that really interest me is the Linux and Window on the Gizmo. However I've so far liked the Rasberry Pi and have yet to try out the Gizmo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to libernullmal

    As I understand, the Gizmo supports Windows CE which is not a full Windows.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>