RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2742 subscribers
  • Views 4513 views
  • Users 0 members are here
  • roadtest survey
  • beaglebone play
Related

ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?

rscasny
rscasny over 3 years ago

imageI have a couple of new BeagleBone SBCs that I'd like the community to roadtest.

This poll is to gauge the level of interest.

About the product:

BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line. With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image, BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positive development experience for users.

Features

  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • WiFi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC

Documentation

Datasheet 
Getting Started 
For More Information

Polls

  • Sign in to reply
  • Cancel
Parents
  • RobPaige
    RobPaige over 3 years ago

    I'd be interested, if you'd have me. Would likely be testing integration with 3d printers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RobPaige
    RobPaige over 3 years ago

    I'd be interested, if you'd have me. Would likely be testing integration with 3d printers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • misaz
    misaz over 3 years ago in reply to RobPaige

    Feel free to apply here: /products/roadtest/rt/roadtests/624/sign_up_to_review_th#pifragment-4106=9&pifragment-4100=4