RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2742 subscribers
  • Views 4513 views
  • Users 0 members are here
  • roadtest survey
  • beaglebone play
Related

ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?

rscasny
rscasny over 3 years ago

imageI have a couple of new BeagleBone SBCs that I'd like the community to roadtest.

This poll is to gauge the level of interest.

About the product:

BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line. With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image, BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positive development experience for users.

Features

  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • WiFi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC

Documentation

Datasheet 
Getting Started 
For More Information

Polls

  • Sign in to reply
  • Cancel
Parents
  • Amethyst
    Amethyst over 3 years ago

    Some of these are tough to answer.

    I'm currently working on  a Samus costume with many bells and whistles. For some applications such as mine, you may want to give an estimated battery draw for portable applications.

    I'm considering that this board may be overkill for my project, but I'm still testing many ideas to add, and having more resources available is a nice thing, battery depending. If you wanted me to try and it's not heavy power consumption, I'm interested.

    How I describe myself is vague for how I should answer. I'm IPC certified and do make props for people using electronics, but probably not enough for anything but "hobbyist"?

    But if you update with battery life, please lmk. I'm off to make another forum post for ideas for my project lol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Amethyst
    Amethyst over 3 years ago

    Some of these are tough to answer.

    I'm currently working on  a Samus costume with many bells and whistles. For some applications such as mine, you may want to give an estimated battery draw for portable applications.

    I'm considering that this board may be overkill for my project, but I'm still testing many ideas to add, and having more resources available is a nice thing, battery depending. If you wanted me to try and it's not heavy power consumption, I'm interested.

    How I describe myself is vague for how I should answer. I'm IPC certified and do make props for people using electronics, but probably not enough for anything but "hobbyist"?

    But if you update with battery life, please lmk. I'm off to make another forum post for ideas for my project lol.