RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2748 subscribers
  • Views 5974 views
  • Users 0 members are here
  • roadtest survey
Related

How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption

rscasny
rscasny over 3 years ago

imageI am planning on roadtesting this product in the near future. It's a simple device, but with WiFi and Bluetooth connectivity and an energy consumption sensor, the product stands out from others.

I primarily wanted to get some ideas on how you would roadtest it. Do you only need the product or is there anything else that should be included in the kit?

Let me give you a few basic facts about the product:

  • The product can be operated with the following load: 85-305VAC @47-63Hz.

  • Standalone device with WiFi and Bluetooth connectivity

  • Measurement of energy data and integrated relay switch to generate additional value on the power input

  • Easy integration of smart IoT functionality into existing devices

  • Connected to the Internet via WiFi 802.11b/g/n and has an integrated energy meter senso

  • Data analysis and processing via SCHURTER Dashboard or SCHURTER App

  • Relay switchable via WiFi (Cloud)

  • Integrated energy live measurement with update rate up to 60 sec.

  • Low standby Energy consumption (<0.5W)

Here are links to the documentation for you to review:

Datasheet 
Web Page 
White Paper 

While I am interested to see how you would set up the product for a product, I have been hashing out some ideas with others. These ideas include:

1. Power a load via the DT31
2. Verify Energy Measurement
3. Ease of use of the Phone App
4. Identify use cases for devices and measurements.

imageHow would you test this unit? I'd appreciate your thoughts in the comments below.

Prospective RoadTester Polls





  • Sign in to reply
  • Cancel
  • obones
    obones over 3 years ago in reply to rscasny

    That's a bit of a set back for me, having yet another cloud based solution is a show stopper as in my IOT setup is meant to work "offline"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago

    Concerning the API. The sponsor clarified with me that testing the API is something that would not be ready to do for this roadtest.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to shabaz

    Schurter just told me this: 

    The product can be operated with the following load: 85-305VAC @47-63Hz.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to kmikemoo

    Just to clarify: 

    The product can be operated with the following load: 85-305VAC @47-63Hz.  So,you should be able to use it. 

    Randall

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    I was told this: 

    The product can be operated with the following load: 85-305VAC @47-63Hz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 3 years ago

    I built one like that using one of these meters about 10 years ago and it still serves me well.

    image

    When we take equipment out for field experiments it's nice to know startup currents/watts vs running currents/watts for solar power and other limited power supplies. My version doesn't have WiFi or Bluetooth however.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to robogary

    These are universal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to rscasny

    I saw the spec said 250V, but the plugs & sockets look like 115VAC. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to shabaz

    Hi shabaz .  I wondered if that might not be the case - Marketing working with the data they had.  But I also wondered if they sensing electronics might not be frequency specific (timing circuits, et al).  Another interesting thought would be to power it from a generator and see how it likes imperfect frequency.  It wouldn't be the first time I ran a generator just to make coffee. Laughing

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • aaryan2134
    aaryan2134 over 3 years ago

    This is pretty interesting! I think testing should be easy enough directly itself. We can plug into the wall and then plug appliances on to this. We can also test if multiple appliances are connected using a powers strip or multi plug to see how it reacts to that. I also have a Wipro Smart Plug which measures energy consumption so we could also test it against other products for accuracy and features. Definitely one of the coolest roadtests to have!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>