RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 2748 subscribers
  • Views 5972 views
  • Users 0 members are here
  • roadtest survey
Related

How You Would RoadTest a Power Entry Device with Wi-Fi/Bluetooth Connectivity to Report on Energy Consumption

rscasny
rscasny over 3 years ago

imageI am planning on roadtesting this product in the near future. It's a simple device, but with WiFi and Bluetooth connectivity and an energy consumption sensor, the product stands out from others.

I primarily wanted to get some ideas on how you would roadtest it. Do you only need the product or is there anything else that should be included in the kit?

Let me give you a few basic facts about the product:

  • The product can be operated with the following load: 85-305VAC @47-63Hz.

  • Standalone device with WiFi and Bluetooth connectivity

  • Measurement of energy data and integrated relay switch to generate additional value on the power input

  • Easy integration of smart IoT functionality into existing devices

  • Connected to the Internet via WiFi 802.11b/g/n and has an integrated energy meter senso

  • Data analysis and processing via SCHURTER Dashboard or SCHURTER App

  • Relay switchable via WiFi (Cloud)

  • Integrated energy live measurement with update rate up to 60 sec.

  • Low standby Energy consumption (<0.5W)

Here are links to the documentation for you to review:

Datasheet 
Web Page 
White Paper 

While I am interested to see how you would set up the product for a product, I have been hashing out some ideas with others. These ideas include:

1. Power a load via the DT31
2. Verify Energy Measurement
3. Ease of use of the Phone App
4. Identify use cases for devices and measurements.

imageHow would you test this unit? I'd appreciate your thoughts in the comments below.

Prospective RoadTester Polls





  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago in reply to kmikemoo

    Hi Mike,

    I'm not sure, but I think it's likely a webpage mistake, because the "250V 10A" text may just mean the relay and the IEC cable rating, because there's nowhere in Europe that has such a voltage system either (nominal is 230V, not 250V). The 50 Hz doesn't make any sense alongside that. Or they might have meant 10A/230V 50Hz. Either way there's a mistake, but I don't know which they meant.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to rscasny

    I would test individually. I would like to know the consumption of each device in its typical use case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    240v, 50Hz. Frowning2  That rules me out.  To demonstrate the operation, I'd put it on the Keurig.  That little beast cycles on and off during normal business hours - just in case we need caffine.  "Just in case..."  Who am I kidding?  WHEN we need caffine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    I'd certainly look at the security of the device - how is it provisioned, how does it speak to the cloud, how does the API work, is there any local access?

    I'd also look at the functionality in terms of whether it memorises state on power outage - as I can see this being a box targeted at remotely power cycling a computer/IT equipment/rack in case of trouble.

    It would be interesting to verify accuracy of energy measurement - a resistive load, variac and power analyser could do the job for a ~PF 1.0 load, but distorting loads could be interesting as well, using a phase-angle control dimmer (leading/trailing edge).

    I don't think a load test is entirely necessary - it's probably got a relay inside rated at the right rating for the job. But if one wishes to cycle it to check for welding of contacts due to inrush, the results are likely very dependent on the load.

    Instead, I'd rather check it for operating power consumption - this is something that's going to be switched on 24/7 and contributing to the power bill, so understanding its consumption would help you avoid silly ideas (i.e. plugging a mobile charger into one, as its standby consumption would be less).

    The outlet IEC C13 (plug) is no big issue - if you're like me, you'd probably lop it off and wire in a mains socket for a bit more versatility. For those who don't want the trouble, commercially available C14 (socket) adapter cables are available especially as some UPSes use the same scheme - e.g.

    • for the UK: https://au.element14.com/pro-elec/pel01253/power-cord-iec-60320-c14-mains/dp/3052547
    • for the US: https://au.element14.com/tripp-lite/p002-001-10a/power-cord-iec-c14-nema-5-15r/dp/2578461
    • for the EU (via third party): https://www.amazon.com/Eonvic-IEC-C14-Europe-adapter/dp/B015T1LM92
    • for AU (via third party): https://www.lindy.com.au/150mm-power-cable-10a-iec-c14-plug-to-3-pin-socket

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Jan Cumps

    It looks like it is sold as an internal version as well, designed to replace the appliance IEC input. I guess this could be useful for portable equipment being moved around a site.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to beacon_dave

    I think that this is the business case for this device. Easy to deploy in unorganized circumstances.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to ntewinkel

    I noticed that myself. The datasheet only says 250V 50hz 10a. I'll have to ask about the input voltage. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ntewinkel

    I checked. It's made by a Holland company, and seems to target the Europe standard.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago

    The ratings appear to indicate it’s not for North America.

    rscasny said:
    rated at 250VAC 50 Hz 10A

    Is that correct, or does it have a 120v version too?

    Either way,  It looks like it might be a good idea to include a power cord (to the unit), and an adapter that plugs onto the C13 outlet to provide a standard socket to plug any appliance into.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ntewinkel

    110 V 60 Hz peoples beware - I believe this one runs 240 V 50 Hz. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>