RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest In RoadTesting Ethernet or SMA Eval Kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 17 replies
  • Subscribers 2749 subscribers
  • Views 3364 views
  • Users 0 members are here
  • roadtester survey
Related

Seeking Your Interest In RoadTesting Ethernet or SMA Eval Kits

rscasny
rscasny over 2 years ago

Link to the second discussion. Click here

Hi All.

We've been talking with Broadcom about roadtesting one of their evaluation kits. Right now, two are being considered. I wanted to get your feedback and/or interest in roadtesting these peroducts. I also would like to know what are parts or equipment you would need to roadtest any of these products.

Let me briefly go through them. I have a poll at the bottom of this discussion.

imageEthernet Evaluation Kit

(AFBR-FSEK50B00E Gigabit Ethernet Evaluation Kit for the AFBR-FS50B00 Optical Wireless Transceiver)

The evaluation kit  for AFBR-FSEK50B00E gives the system designer a convenient means to evaluate the performance of the Optical Wireless Transceiver AFBR-FS50B00.

The evaluation kit includes:

  • Two PCBs with RJ-45 connector and IC BCM54210, which implements the functionality of a Media Converter
  • Two PCBs with Optical Wireless Transceiver AFBRFS50B00
  • One USB memory stick containing technical documentation.

The evaluation kit does not include:

  • CAT5 cables required for GbE communications between the evaluation kit and the user’s application.
  • Micro USB cables required for power supply.

Documentation

  • Datasheet

For More Information

SMA Evaluation Kit

imageBROADCOM AFBR-FSEK50B00S SMA Evaluation Kit, AFBR-FS50B00, Optical Wireless Transceiver, Wireless Communication
SMA Evaluation Kit for the AFBR-FS50B00 - 5 Gb/s

The Broadcom® AFBR-FSEK50B00S is an evaluation platform for the Optical Wireless Transceiver AFBR-FS50B00. The AFBR-FSEK50B00S evaluation kit provides the system designer a convenient means to evaluate the performance of the AFBR-FS50B00 optical wireless transceiver.

The evaluation kit includes:

  • Two PCBs with SMA connectors and AFBR-FS50B00 optical wireless transceiver
  • Two jumpers

The evaluation kit does not include:

  • Coaxial cables required for communication through the AFBR-FS50B00 optical wireless transceiver
  • Cables required to supply power to the boards included in the evaluation kit

Documentation

  • Datasheet

For More Information


About the Broadcom® AFBR-FS50B00 Transceiver

The Broadcom® AFBR-FS50B00 is a transceiver that communicates data over free space and thereby allows connector-less/cable-less
communication in a variety of applications. Full-duplex bidirectional communication, together with a small form factor, allows a compact system design. The device keeps full functionality over a 360° rotation around the optical axis, which reduces the complexity of alignment on the system level and allows the use in rotating systems. The component is designed to operate over a wide temperature range and with a potential data rate up to 5 Gb/s and a variable distance from 20 mm up to 100 mm. The AFBR-FS50B00, a Laser Class 1 product, is RoHS-compliant and is designed for SMT solderability standard processes

image

RoadTester Poll



  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    0 kmikemoo over 2 years ago

    While I'm interested, I don't have the skill set to do what I'm thinking - so I picked "not interested".  HOWEVER, for someone that does have the skill... 

    My scenario is the USB control connection between a HF radio and laptop computer.  The setup uses a SDRUno and the laptop runs SDRPlay software.  The radio is a Kenwood TS-590.  The laptop screen is projected onto a larger screen so more people (ideally visitors) can see what is going on.  If we use a cheap USB cable to connect the radio to the laptop, the software crashes when we key the microphone.  The USB cable that works is higher quality and has ferrite chokes on each end.  With optical isolation, would the quality of the USB cable matter?
    Just thinking out loud. Relaxed

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    Hi Mike,

    Isolation would definitely help. I'm wondering, if the root cause could be absence of a balun on the antenna end of the SDRuno. It could be worth upgrading the balun (or string a load of ferrites on that antenna cable). Otherwise, ferrites on the USB cable at a minimum would be needed (might be worth adding a couple more, just to be on the safe side).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    Hi shabaz .  I agree that my problem has to be something like common mode current.  I tried using it today with the same setup that worked back in January and it's not working.

    The SDRUno actually gets its input from an output on the Kenwood.  I've got a 6" RCA to SMA cable from the radio to the SDRUno.  Maybe I need a longer jumper to move the whole system away from the radios.  There IS a chance that the last time it worked, I did not have the VHF radio turned on.  That could be my nemesis today.  Our State is having their QSO Party today so I just let the two guys that wanted to use the station go crazy.

    I'll take a crack at troubleshooting it a bit later in the contest.  I do have an RCA to something homemade cable that I can ferrite the dickens out of and adapt to SMA.  My only 1:1 balun is SO-239 to wire.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    I've had that same experience.. trying a high-value attenuation and getting nowhere near it! 

    I was wondering how to seal each stage, in the easiest-to-assemble way I could think of. I sketched the following, it still needs work, and might not be the best way.

    If (say) it was a 4-stage (where each stage shouldn't be more than about 25 dB) then that's 100dB of attenuation if desired.

    image

    The idea being that each section could be boxed with a screening can. The resistors (or at least some of them) would be large (e.g. 1210 sized) SMD, so that they could dissipate some power.

    image

    Once the cans are soldered (with a high-power iron), the adjacent cans joining each stage would need to be bridged with solder too, to prevent RF finding a way to the outside world between the stages.

    The cans are cheap in quantities of 10. Slightly taller versions would be better, but this is all I could find and might be OK:

    image

    The SMA connectors could be soldered on the other side, and then solder used to fillet all the way around the edges of each connector. Also every via hole could be soldered over if required!

    image

    Don't know if it's worth building though, because it would be hard work to solder the cans without a high-power iron. Also it would only work up to a few hundred MHz.

    Regarding a coupling loop near an attenuator (if it isn't fully shielded), or close to coax braid, it would work, but would be hard to know what the attenuation would be (and it might vary over frequency). But might be good enough! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    Hi shabaz .  The box is just a lazy man's way of terminating a SO-239 connector.  The bolt on the side is because I gave up trying to land the shield on the aluminum.  It's just a ring ternimal, bolt and nut.  I bought a number of the bodies thinking to build attenuators but they turned out rather poor.  Right now, I only use attenuators for radio direction finding - so I purchased a few and made one out of strip board that attenuates 46dB.  The calculator says 116dB but the coupling says... "I don't think so." Laughing

    I've been experimenting on and off with trying to attenuate 500mW to 750mW signals.  I have intentionally bought and made inefficient antennas.  You would be surprised how effective a 3-stack of 30dB attenuators works as an antenna.  Wouldn't a coupling loop near the dummy load act like a potential transformer?  It would be hard to get accurate level readings without plotting a bunch of known values.  I may have to try that out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    Hi Mike, 

    Interesting! Glad you're finding what works. Also, just curious, is the box an attenuator?

    image

    Depends how it's built of course, if it's super-high attenuation in there (e.g. 30dB or more) the RF might be coupling unexpectedly despite the attenuation.

    I found that out when trying to attenuate by 100dB or something (I wanted to do a similar thing, feed a transmitter into a radio receiver), and ended up using separate 20dB and 10dB attenuators (each with their individual metal cylinders) all chained up, and it was totally impractical admittedly! Partitioning inside the enclosure (e.g. walls of copper-clad PCB) could be another idea.

    Recently I found this nice thing on eBay (but it's not high power, so would still need a higher-power attenuator to front it):

    image

    I've not tried it out yet! Hoping it works. 

    EDIT: This would be another way to do it; using a coupler to get less of the signal (and pass the rest into a large dummy load), but this one only offers 15dB reduction, and only supports 4W. Maybe there are higher-power DIY versions suitable for HF use, but I've never checked to see.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to kmikemoo

    The problem wound up being in the USB providing rig control.  This cable already has a large ferrite with the USB looping through it 5 times.  Additional ferrites did not solve the problem BUT moving the USB from the 3.0 plug on the radio side to the USB 3.0 plug on the opposite side allowed it to work.  Better shielding on that side?  I still have some RF shielding I bought a while back.  Maybe I'll give that a try..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    Joy     7mm, but I've got a few.  Great fit for RG8X.  Unfortunately, this is RG59/U - but it will have to do for now.

    image   image

    I'll know in a couple of hours.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    Joy     7mm, but I've got a few.  Great fit for RG8X.  Unfortunately, this is RG59/U - but it will have to do for now.

    image   image

    I'll know in a couple of hours.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    I've had that same experience.. trying a high-value attenuation and getting nowhere near it! 

    I was wondering how to seal each stage, in the easiest-to-assemble way I could think of. I sketched the following, it still needs work, and might not be the best way.

    If (say) it was a 4-stage (where each stage shouldn't be more than about 25 dB) then that's 100dB of attenuation if desired.

    image

    The idea being that each section could be boxed with a screening can. The resistors (or at least some of them) would be large (e.g. 1210 sized) SMD, so that they could dissipate some power.

    image

    Once the cans are soldered (with a high-power iron), the adjacent cans joining each stage would need to be bridged with solder too, to prevent RF finding a way to the outside world between the stages.

    The cans are cheap in quantities of 10. Slightly taller versions would be better, but this is all I could find and might be OK:

    image

    The SMA connectors could be soldered on the other side, and then solder used to fillet all the way around the edges of each connector. Also every via hole could be soldered over if required!

    image

    Don't know if it's worth building though, because it would be hard work to solder the cans without a high-power iron. Also it would only work up to a few hundred MHz.

    Regarding a coupling loop near an attenuator (if it isn't fully shielded), or close to coax braid, it would work, but would be hard to know what the attenuation would be (and it might vary over frequency). But might be good enough! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    Hi shabaz .  The box is just a lazy man's way of terminating a SO-239 connector.  The bolt on the side is because I gave up trying to land the shield on the aluminum.  It's just a ring ternimal, bolt and nut.  I bought a number of the bodies thinking to build attenuators but they turned out rather poor.  Right now, I only use attenuators for radio direction finding - so I purchased a few and made one out of strip board that attenuates 46dB.  The calculator says 116dB but the coupling says... "I don't think so." Laughing

    I've been experimenting on and off with trying to attenuate 500mW to 750mW signals.  I have intentionally bought and made inefficient antennas.  You would be surprised how effective a 3-stack of 30dB attenuators works as an antenna.  Wouldn't a coupling loop near the dummy load act like a potential transformer?  It would be hard to get accurate level readings without plotting a bunch of known values.  I may have to try that out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    Hi Mike, 

    Interesting! Glad you're finding what works. Also, just curious, is the box an attenuator?

    image

    Depends how it's built of course, if it's super-high attenuation in there (e.g. 30dB or more) the RF might be coupling unexpectedly despite the attenuation.

    I found that out when trying to attenuate by 100dB or something (I wanted to do a similar thing, feed a transmitter into a radio receiver), and ended up using separate 20dB and 10dB attenuators (each with their individual metal cylinders) all chained up, and it was totally impractical admittedly! Partitioning inside the enclosure (e.g. walls of copper-clad PCB) could be another idea.

    Recently I found this nice thing on eBay (but it's not high power, so would still need a higher-power attenuator to front it):

    image

    I've not tried it out yet! Hoping it works. 

    EDIT: This would be another way to do it; using a coupler to get less of the signal (and pass the rest into a large dummy load), but this one only offers 15dB reduction, and only supports 4W. Maybe there are higher-power DIY versions suitable for HF use, but I've never checked to see.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to kmikemoo

    The problem wound up being in the USB providing rig control.  This cable already has a large ferrite with the USB looping through it 5 times.  Additional ferrites did not solve the problem BUT moving the USB from the 3.0 plug on the radio side to the USB 3.0 plug on the opposite side allowed it to work.  Better shielding on that side?  I still have some RF shielding I bought a while back.  Maybe I'll give that a try..