RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Weller Micro Soldering Kit and Filtration Unit - first test of desoldering tweezers
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 2745 subscribers
  • Views 1227 views
  • Users 0 members are here
  • weller
Related

Weller Micro Soldering Kit and Filtration Unit - first test of desoldering tweezers

Jan Cumps
Jan Cumps 9 months ago

Testing the desoldering tweezers. I removed a set of SMD components from a multi-layer board:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps 9 months ago

    I just did a new rework test. Remove 3 0402 resistors from a multilayer board, and replace them.

    The video above was done right after unpacking the kit. This time, I have a week of experience. You may notice that I'm more comfortable with the tweezers and iron than in video 1. They now feel natural.

    what was used from the kit:

    • the station, at 380° C. Both for tweezers and iron.
    • conical bent tip solder tweezers (RTWMS 004 C X)
    • bevel micro solder tip 0.4 mm (RTM 004 B MS)
    • micro solder iron
    • tweezers
    • auto tip cleaner (not in view)
    • fume extractor (partly in view)

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett 9 months ago in reply to Jan Cumps

    I've found that using smaller de-solder braid on smaller pads is worth the trouble of having several different sizes. The tiny bits you need for 0402 parts have trouble getting enough heat into the thicker braid.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 9 months ago in reply to michaelkellett

     michaelkellett , the largest iron of this kit (the micro solder one) comes with tips that are at the small side of its range. (except for the gull wing - that's hefty, put specialised).

    I ordered one of the larger chisel tips of this line. One that I think has enough mass for some thermal buffer. 
    image

    I didn't buy the largest one. Once I'm into the larger SMD and through-hole realm, I have better suited options than Weller's WT line. But I expect that the tip I ordered will allow me to work on small size surface mount boards with the odd through hole pin. Or with FETs and ICs that have a ground plane area

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to Jan Cumps
    Jan Cumps said:
    I ordered one of the larger chisel tips of this line. One that I think has enough mass for some thermal buffer.

    It arrived today - this would not be the daily runner for this setup. But it 'll come handy when I'm working on an SMD design with large pads or through-hole component.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps 8 months ago in reply to Jan Cumps
    Jan Cumps said:
    I ordered one of the larger chisel tips of this line. One that I think has enough mass for some thermal buffer.

    It arrived today - this would not be the daily runner for this setup. But it 'll come handy when I'm working on an SMD design with large pads or through-hole component.