RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Are you interested in Reviewing Red Pitaya's Hardware? We have the STEMlab 125-14 PRO Gen 2
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 2744 subscribers
  • Views 2335 views
  • Users 0 members are here
  • e14-redpitaya
  • stemlab 125-14 pro gen 2 starter kit
  • izd0055
  • red pitaya
Related

Are you interested in Reviewing Red Pitaya's Hardware? We have the STEMlab 125-14 PRO Gen 2

OwainM
OwainM 8 months ago

We have the opportunity to offer up the STEMlab 125-14 PRO Gen 2 Starter Kit - which is available on our online store .

image

Here's a little bit about the hardware:

What do you think?

  • Sign in to reply
  • Cancel
  • zano22
    zano22 7 months ago

    Very  interesting  piece  of  hardware, a  multi  software  platform  makes it  so  helpfull  .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Abouda_007
    Abouda_007 7 months ago

    I think it would be very useful in teaching and in research as well.

    Very intersted Module that you can program it with Python, Matlab, Labview, C, etc....

    With the FPGA on the STEMlab 125-14 PRO Gen 2 (Zynq-7010), you’re essentially sitting on a real-time, deterministic signal-processing fabric that can ingest the 2× 125 MS/s ADC streams, process them with sub-µs latency, and drive the 2× 125 MS/s DACs—while the ARM cores handle UI/networking/logging.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • OwainM
    OwainM 7 months ago in reply to DAB

    The STEMlab 125-14 PRO Gen 2 appears to use a web-based interface for different applications, explained in more detail here. 

    The linked page is also the landing page for the other control methods available. There is the option available to control it using MATLAB, LabVIEW, and Python, or to program your own applications making use of provided APIs to run C code and Python (using Jupyter notebook) or create and run your own FPGA Logic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • OwainM
    OwainM 7 months ago in reply to veluv01

    I'm not too sure currently, we're initially trying to ascertain what might be needed to give members the best chance to RoadTest this to its full potential and get the most out of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz 7 months ago

    I would be happy to roadtest this! I would use it to experiment with logic tester results for my embedded projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett 8 months ago in reply to scottiebabe

    Thanks for the reference community.element14.com/.../scottiebabe

    An interesting project but the Red Pitaya involvement was not very significant and their hype is a bit irksome.

    Full kudos to the student for the real RF work  - but it was done at 2.4GHz and the RP was only operating at much lower frequencies.

    They said:

    Red Pitaya bridges the gap between theoretical RF engineering and practical hardware design. With its 125 Msps ADC, FPGA, and built-in ARM processor, it lets students digitize high-frequency signals, run real-time processing, and control the entire radar system — all on a single board.

    But then they say:

    Here’s what made David’s DIY FMCW radar project possible with Red Pitaya:

    • Operating Frequency: 2.4–2.5 GHz

    • Sweep Rate: 1 kHz

    • Transmit Power: 26 dBm (400 mW)

    • ADC Sampling Rate: 125 Msps (14-bit resolution)

    • Core Capabilities: Simultaneous distance and velocity measurement

    The RP can't do anything useful at 2.4GHz, and it has no influence at all on transmit power.

    So the RF design would have required the usual RF gear and software.

    It would be nice to know what software was used to design the mixer and other RF stuff and how it was tested.

    In this design the RP generates a 1kHz ramp to modulate the VCO and measures the beat frequency of the RF return signal with the local oscillator (actual frequencies not disclosed).

    It doesn't look as if the RP is doing anything a £25 ST Nucleo board couldn't do.

    The Red Pitaya is an interesting and potentially useful product but over-hyping the way they do does no one any favours.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • drkirkby
    drkirkby 8 months ago

    If one is provided free of charge, I would be interested in reviewing one, and providing a report. My project would be a Q-meter for measuring inductors, which would also give inductance. This would not use the technique used in your LCR meter application, which has a few fixed frequencies. A standard LCR meter, even the latest models from Keysight, are not accurate on Q measurements of inductors of even a modest Q (>20). We have for comparison purposes 

    * Agilent 4284A Precision LCR meter 20 Hz to 1 MHz (basic accuracy 0.05%) www.keysight.com/.../5963-5390.pdf

    * HP 4285A Precision LCR meter 75 kHz to 30 MHz (basic accuracy 0.1%) www.keysight.com/.../5963-5395.pdf

    * A very old Boonton Q-meter, which has lower uncertainty than the more modern HP:Agilent//Keysight instruments. 

    * VNAs covering the frequency range 300 kHz to 20 GHz. 

    * Boonton inductors of various values, with accurate measurements of both inductance and Q. 

    The proposed Q-meter would rely on a measurement of 3 dB bandwidth of a resonant circuit, where a low-loss manually tuned variable capacitor is adjusted to provide resonance at the frequency required. 

    There is an example in the 4285A manual and datasheet showing the calculation of uncertainty for an inductor. At a frequency of 25.2 MHz, inductance of 220 nH, and measured Q of 30, the uncertainty in inductance is ±2.6%, but for Q it is −13 /+105. Thus, the Q could lie anywhere from 17 to 135. The instrument’s basic accuracy of 0.1% therefore does not translate into an accurate measurement of Q. I think this illustrates the point that even a high-end professional LCR meter is not suitable for precise Q measurements.

    Agilent did manufacture a precision Q adapter (42851A) for the 4285A. We do not have one of these, and they are around $2,500 on the used market. However, I have a good understanding of how it operates and believe a Red Pitaya could form the basis of a meter able to measure Q much more accurately than any affordable modern instrument. Comparisons with VNA measurements would yield interesting results. What is the most accurate method? Under what conditions? 

    Being provided the LCR meter add-on would be useful for comparison purposes, but ultimately the LCR meter functionality will be poor compared to other instruments we have. But if a Q-meter was built, it could be sold as an ad-on as Agilent did with the 4285A+42851A. 

    Dr. David Kirkby BSc, MSc, PhD. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe 8 months ago in reply to robogary

    Looks farm more exciting than the current modules...

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx 8 months ago in reply to robogary

    typical sport exhaust...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary 8 months ago in reply to scottiebabe

    I'd like to strap one of those on my bumper and watch the cops go nuts. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>