RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 3629 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago

    Having spent time in a previous life doing RF work for the NZ Post Office (later Telecom) I've seen a vaste array of antennas, and antenna designs.

    Each has a specific purpose, and some are designed for the environment, so they have special charateristics or materials.

     

    As awneil said the radiation pattern and gain are the key differences between antenna.

     

    The examples above are all omni-directional, (but for different bands) so the gain is the final figure as to how well it will perform.

    Therefore the 2.7-6GHz version should have a longer range with the same power.

     

    To test these you need a transmitter with adjustable gain, and a receiver that can provide the RSSI (Received signal strength).

    They need to be tested in an open environment, clear from reflections.

     

    While this provides the optimal conditions, in reality they are used in an urban environment, placed to suit the box or mounting.

    This means the real world result is varied and not able to be duplicated easily.

     

     

    What I think might be useful is to see if the testers can increase the range of the middle example by directing it, to provide a cheap link between two points.

     

    I've aluded to some antenna theory here BT_Sentry : Zero Emission Detection

    I have to build something that will allow my modifications to be tested, which is likely to involve a servo and stand in the middle of a paddock.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gecoz
    gecoz over 8 years ago in reply to mcb1

    Hi Mark,

     

    While the gain is indeed a measure of how well the antenna performs, to calculate the range you need to take into account also the frequency of the signal (assuming all the other parameters are identical).

     

    The Omni-directional SMD Antenna and the OMNI ANTENNA, 2.7-6GHZ, 5DBI, ADHESIVE both work on similar frequency bands, so looking at their datasheets, we can already infer the OMNI antenna performs better (higher gain).

     

    To establish which has a better range between the OMNI ANTENNA, 2.7-6GHZ, 5DBI, ADHESIVE and the OMNI ANTENNA, LINEAR, 433MHZ, 0.7DBI, we can use the Friis Equation - (aka Friis Transmission Formula). The distance R can be calculated as:

     

    R=√(Pt·Gt·Gr)·c√Pr·4πƒ

     

    where:

       c is the speed of light

       f is the frequency of the signal transmitted

       Pt is the power transmitted

       Pr is the power received

       Gt is the gain of the transmitting antenna

       Gr is the gain of the receiveing antenna

     

    To simplify,  lets assume the power transmitted, the power received and the receiving antenna's gain are the same for both antennas. Lets call R1 the range for the 5dBi antenna, and R2 the range for the 0.7dBi. If we calculate the ratio R1/R2, we get:

     

    R1R2 =√Gt1Gt2 ·ƒ 2ƒ 1

     

    where:

        Gt1 = 5dBi = 3.16 ,    f1=2.7GHz  (lets use the lower end of the band)

        Gt2 = 0.7dBi = 1.17 , f2=0.433GHz

     

    Calculating, we get:

     

    R1R2 ≈0.26   

     

    Therefore, under the assumptions above, the 0.7dBi antenna should give a range about 4 times longer than the 5dBi one.

     

    Fabio

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gecoz
    gecoz over 8 years ago in reply to mcb1

    Hi Mark,

     

    While the gain is indeed a measure of how well the antenna performs, to calculate the range you need to take into account also the frequency of the signal (assuming all the other parameters are identical).

     

    The Omni-directional SMD Antenna and the OMNI ANTENNA, 2.7-6GHZ, 5DBI, ADHESIVE both work on similar frequency bands, so looking at their datasheets, we can already infer the OMNI antenna performs better (higher gain).

     

    To establish which has a better range between the OMNI ANTENNA, 2.7-6GHZ, 5DBI, ADHESIVE and the OMNI ANTENNA, LINEAR, 433MHZ, 0.7DBI, we can use the Friis Equation - (aka Friis Transmission Formula). The distance R can be calculated as:

     

    R=√(Pt·Gt·Gr)·c√Pr·4πƒ

     

    where:

       c is the speed of light

       f is the frequency of the signal transmitted

       Pt is the power transmitted

       Pr is the power received

       Gt is the gain of the transmitting antenna

       Gr is the gain of the receiveing antenna

     

    To simplify,  lets assume the power transmitted, the power received and the receiving antenna's gain are the same for both antennas. Lets call R1 the range for the 5dBi antenna, and R2 the range for the 0.7dBi. If we calculate the ratio R1/R2, we get:

     

    R1R2 =√Gt1Gt2 ·ƒ 2ƒ 1

     

    where:

        Gt1 = 5dBi = 3.16 ,    f1=2.7GHz  (lets use the lower end of the band)

        Gt2 = 0.7dBi = 1.17 , f2=0.433GHz

     

    Calculating, we get:

     

    R1R2 ≈0.26   

     

    Therefore, under the assumptions above, the 0.7dBi antenna should give a range about 4 times longer than the 5dBi one.

     

    Fabio

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to mcb1
    To establish which has a better range

    It may be interesting to some ... we had much better signal to noise ratios not by increasing the power, but reducing the bandwidth of the receivers.

     

    Many of our receivers were capable of being used across the band they were designed for, but in reality they stayed on a fixed frequency, for varying reasons.

    Careful tuning reduced that to a narrow frequency, and thereby reducing the noise floor.

     

    Many of these receivers have no filtering on the front end, and therefore wide bandwidth antennas can provide higher background noise.

    Trying to extract the signal you're after in amongst the noise, can be a struggle, but is dependant on the hardware and techniques used.

     

    Mark

     

     

     

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to gecoz

    to calculate the range you need to take into account also the frequency of the signal

    of course ... and yes you're quite right that the losses increase with frequency.

     

     

    I mistaken assummed that the testing would be on antennas in the same band image

    Mark