RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 103 replies
  • Subscribers 2752 subscribers
  • Views 14784 views
  • Users 0 members are here
  • scasny
Related

Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield

rscasny
rscasny over 8 years ago

I was contacted by a supplier who is interested in giving hardware for free to someone who could do a project for them featuring  Cypress's PSoc6 BLE kit +  Honeywell Pressure Sensor Shield.

 

They would like the person to do the following:

 

Interface the pressure sensors of the Honeywell Sensor Shield with the PSoC 6 analog/digital peripherals and then transmit data via BLE or showcasing it on the E-ink display of the PSoC 6 BLE Kit. The project should have some kind of medical application. For example, measuring pressure in some kind of health/medical application.

 

Just to refresh your mind, here are the parts involved:

 

image

Click here for more information or review the roadtest we did on this product: https://www.element14.com/community/roadTests/1862/l/cypress-psoc-6-ble-pioneer-kit-cy8ckit-062-ble#comment-117223

 

image

Click here for more information on this Honeywell Sensor Shield. I have not roadtested this product.

 

I would like to do this sometime in October. I'd like to get it accomplished in a month--the shorter time period is why I am not offering it as a roadtest.

 

If you are interested, feel free to comment below.

 

thanks.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 8 years ago

    To the 5 project builders.....

     

    jomoenginer

    balearicdynamics

    BigG

    dougw

    geralds

     

    I wanted to post an update to this.

     

    First off: anyone who needs a PSoC 6 Pioneer kit, they are on their way to me. I got the tracking number so I should get them shortly. In addition, I have ordered 5 Honeywell Sensor Shields (SEK002) for all of you. Before looking at the datasheet, I casually assumed that the sensors were placed on the shield, as they are on other shields/expansion boards. After looking at the datasheet, I assumed incorrectly. I believe Enrico mentioned that too. So, I need to get some information regarding the sensors, etc. This is what is happening:

     

    I will order everyone a micropressure sensor (MRP) series. But you have to tell me which one. So go here, and select the one that you need. If you don't need one, tell me that too:

    https://uk.farnell.com/w/c/sensors-transducers/sensors/pressure-sensors-transducers/pressure-transducers?product-range=m…

     

    ABP Series

    Tell me which one you need from the ABP series: https://uk.farnell.com/search?st=honeywell%20abp

     

    Humidicon Series

    Tell me which one you need from this series: https://uk.farnell.com/search?st=honeywell%20humidicon

     

    I'm not including the particle count sensors because I don't expect they are need for the medical application.

     

     

    So look over these links and tell me which ones you need and I'll order them.

     

    Randall

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to rscasny

    Hi Randal

     

    I have a couple of queries.

     

    Please could you check with Honeywell which pin is used as the select pin for the SPI sensors on the SEK002 kit. Documentation not clear. Images in documentation show an SS0 (Arduino pin 10) and an SS1 (Arduino pin 9). Reason being is that the PSoC 6 EPD Display Shield uses Arduino pin 10 as its SSEL pin.

     

    Then wanted to check product codes and descriptions before ordering. Farnell order number 2773682 is listed as a differential sensor (ABPLANT015PD2A5) even though it is described as a single axial barbed sensor, which matches image. I always assumed that differential sensors require two ports.

     

    Also, order number 2490463 is listed as a gauge sensor (ABPDRRT005PG2A5) and has two ports.

     

    Thanks

     

    Colin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to BigG

    Hi Colin,

    The sensor ABPLANT015PD2A5 (2773682) look like this one:

     

    https://sensing.honeywell.com/ABPLANT015PD2A5-amplified-board-mount-pressure-sensors

     

    The pinouts on the SEK002:

    image

    I think, its not so a big problem.

    image

     

    The device name code includes which interface the device has.

    So for the both of your selected sensors ABPLANT015PD2A5 and  ABPDRRT005PG2A5ABPDRRT005PG2A5 they has an I2C interface with the address at 0x28

    image

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to BigG

    Hi Colin BigG ,

    Now I have received the circuit diagram, which I would like to post here as well.
    Now you can set the jumper settings correctly.

    I am already curious about the reviews.

    Best regards
    Gerald
    ---

    Attachments:
    imageSchematic SEK002.pdf
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to BigG

    Yes, I read this last week and have had thinking the same about this….

    hm....

    Now I wrote to Honeywell an email to order the schematics about the SEK001 and SEK002, got now a ticket number.

    Well I look forward hopefully to get one. I made the image to negative color so you can better see the wires.

    May be this helps a little bit.

    If don't get the schematics then I rework back, from PCB to schematic.

    image

     

    Best Regards

    Gerald

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to geralds

    I assumed that the gage reference hole (as shown on pg 11) was used to measure atmospheric pressure which is needed to provide a gage pressure measurement.

     

    My earlier comments were based on the definitions given on page 2:

     

    image

     

    As such, I see a differential sensor as having two ports where you can apply pressures to. This allows you to measure the difference.

     

    And so, sensors only having a single port can only ever be gage, or absolute, as your application can only apply pressure to this one port.

     

    I see there also have a "no port" sensor option... hmmm. I assume that must be atmospheric only.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to BigG

    Hi Colin,

     

    the sensor has a hole, on the bottom side. This is the gage reference hole to the input port.

    The sensor measures the difference pressure. Please look to image above. There are drawings of the devices it shows this hole.

    So if you builds you own PCB you have to know this, you need to make this hole also into the PCB.

    Please read page 11:

    https://sensing.honeywell.com/honeywell-sensing-basic-board-mount-pressure-abp-series-installation-instructions-32305127…

     

    Rgds

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to geralds

    Hi Gerald

     

    I was reading the Product Features list as per the html link you sent me. The first feature stated is "Measure gage and differential pressures".

     

    Oh boy, now even more confused. Still cannot figure out how it can measure differential just within the one sensor port shown.

     

    Rgds

     

    Colin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to BigG

    Just found T1!

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 7 years ago in reply to BigG

    Just found T1!