RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Evaluating Waveform and Pattern Generator ---R&S RTM3K Oscilloscope Road-Test Review
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 28 Jul 2018 8:28 PM Date Created
  • Views 1346 views
  • Likes 6 likes
  • Comments 4 comments
Related
Recommended
  • rtm3004
  • digital signal
  • function_generator
  • rhode & schwartz oscilloscope
  • pattern generator
  • mid-range oscilloscope
  • waveform_generator

Evaluating Waveform and Pattern Generator ---R&S RTM3K Oscilloscope Road-Test Review

snidhi
snidhi
28 Jul 2018

  • Evaluating the Waveform and Pattern Generator Feature
    • Specifications of the Waveform/function Generator in RTM3004
    • Testing the Waveform Generator in RTM 3004
    • Experiments with the Pattern Generator

Evaluating the Waveform and Pattern Generator Feature

This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review

 

Specifications of the Waveform/function Generator in RTM3004

image

Fig: Specifications of the RTM Waveform Generator

Testing the Waveform Generator in RTM 3004

 

As it is clear from the specifications, this is a decent but basic 14 bit waveform generator with a low sampling rate of 250 Msamples/sec and has 3% amplitude accuracy. It can generate sine, pulse, rectangle, ramp, triangle, sinc and exponential waveforms with maximum 10 MHz or a lower 1 MHz frequency.

 

The waveforms were tested by inputing the waveform patterns from RTM 3004 waveform generator into Tektronix MSO 5204 oscilloscope of 2 GHz BW (Ref higher BW with 10GSa/s sampling rate). Both the devices were powered separately using a GND loop isolating power supply Ref. The isolation was done to avoid forming GNDing loop connection between the DUT (RTM 3004) and  Tek MSO 5204.

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Fig: Setting up the Function Generator Settings in RTM 3004

 

image

Fig: Sine Signal from the RTM 3004 waveform generator

 

image

Fig: SinC Signal from the RTM 3004 waveform generator

 

image

Fig: Pulse Signal from the RTM 3004 waveform generator

 

image

Fig: Triangle Signal from the RTM 3004 waveform generator

 

image

Fig: Ramp Output Signal from the RTM 3004 waveform generator

 

image

Fig: Arbitrary Output Signal from the RTM 3004 waveform generator

 

Experiments with the Pattern Generator

 

In the RTM-3004 oscilloscope; the pattern generator is embedded in the oscilloscope itself. Normally, I have worked with stand-alone pattern generator devices. This functionality adds a uniqueness to the oscilloscope as it is very useful tool for digital engineers. The RTM-3004 has a 4 bit programmable pattern generator using which one can generate square wave, pulse patterns or any user defined patterns. Each channel can be programmed individually and used for digital testing. It can produce a repetitive signals or single shot pulse for triggering purposes. The voltage levels generated by the pattern generator are normally complaint with the digital I/O electronics standards such as TTL, LVDS, LVCMOS, LVTTL and others.

image

Fig: Specifications of the RTM 3004 Pattern Generator

 

I leave the experimental test with the Pattern Generator to future.

  • Sign in to reply

Top Comments

  • snidhi
    snidhi over 7 years ago in reply to three-phase +1
    Hi Donald, Not really much. yes this test I did was pretty basic I ran out of time but I intend to put it up in the near future. Cheers
  • snidhi
    snidhi over 7 years ago in reply to three-phase +1
    Hopefully in future. I have a number of tests lined up to go on with the RTM 3004.
  • snidhi
    snidhi over 7 years ago in reply to three-phase

    Hopefully in future. I have a number of tests lined up to go on with the RTM 3004.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to snidhi

    That's a shame, to was one of the aspects of the scope I was interested in taking a look at. I don't remember either of the other reviews looking at it either.

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 7 years ago in reply to three-phase

    Hi Donald,

    Not really much. yes this test I did was pretty basic

     

    I ran out of time but I intend to put it up in the near future.

     

    Cheers image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago

    This does look to be quite basic, did you experiment with the arbitrary generator function at all?

     

    Kind regards