GIZMO 2GIZMO 2 is the second generation open source x86 development board presented by GizmoSphere. Gizmo 2 provides the power of a high performance computer and the I/O capabilities of a microcontroller through the use of an AMD Embedded G-Series System-on-Chip (SOC). The board includes the AMD GX-210HA dual-core processor, combined on a single die with AMD Radeon HD 8210E discrete-class graphics, providing 85 GFLOPS performance while drawing only 9 watts TDP.
Gizmo 2 is among the highest performing Open Source x86 development boards available, providing a wealth of leading features and capabilities including an HDMI dedicated port, an mSATA port for connecting SSDs and a microSD card slot.
Key Applications: Gizmo 2 can be used in do-it-yourself (DIY) designs, embedded development, PC replacement, microcontroller applications, parallel processing, multi-core engineering, industrial control and automation, digital signage, electronic gaming systems, SMB storage, IP-TV, medical and network appliances, set-top boxes and more. Any type of application that would require high processing power, high graphics performance, and the ability to control external objects (relays, motors, lights, etc) as well as take inputs from many types of sources (sensors, keyboard, Internet)
Key Features
AMD G-Series SOC
1GB DDR3-1600 SDRAM
HDMI Video/Audio Output
85 GFLOPS performance
HD Audio In/Out
mSATA/mini PCIe Connector
microSD Card Slot
Onboard Gigabit Ethernet
USB 3(2) and 2(2) Connectors
AMD Debug Header
High-speed and Low-speed Special Features Card Edge Connectors
4" x 4" Form Factor
Support for DirectX® 11.1, OpenGL 4.2x and OpenCL™ 1.2, enabling parallel processing and high-performance graphics processing
Supported operating systems include Windows Embedded 8 and Linux
Product Video
You don't have permission to edit metadata of this video.
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future RoadTests.
I'm so looking forward to using the Gizmo2 for a retro games console project; Along the way, there'll be regular blog posts detailing how the project is progressing and hopefully will be complete by the time the review is due.
The blog's and additional content should be linked to from here in due course and also in the final review which will be created once I've had chance to fully evaluate the Gizmo2 and everything it has to offer.
It's great to have the opportunity to work with the latest generation of small board computers utilising modern system on chip technologies (which I am sure will be the direction that present and future computing will progress) and thank Element14, Christian ( doctorcdf), Gizmosphere and everyone involved in the selection process.
Many thanks to all who applied for this RoadTest: with 523 applications, this has been one of the most popular RoadTests we've ever had. It is a shame that we can't reward all the great applications with units: it has been a difficult decision, but we've selected the following testers:
Christever del Rosario
Andrew Peng
Lucie Tozer
Thanks once again to all who applied: those who weren't successful this time, I encourage to apply for our other exciting RoadTests.
Top Comments
Yay!!!
I'm so looking forward to using the Gizmo2 for a retro games console project; Along the way, there'll be regular blog posts detailing how the project is progressing and hopefully will be complete…
Looking forward for this retro gaming console.
Btw, I got my board and started playing with it. Will give an update soon...