Review of AMD Xilinx Kria KV260 Vision AI Starter Kit

View table of contents ...  

RoadTest: AMD Xilinx Kria KV260 Vision AI Starter Kit

Author: work14

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: (1) Stemedu ESP32-CAM Development Board with Flash Ai Thinker Camera Module OV2640 for Arduino. (2) BEAGLEBOARD SBC BeagleBone, AI-64, TDA4VM. (3) Huskylens Kendryte K21 (AI Chip FPGA module, High-end Allwinner V3 system on with 64bit RISC-V (4) OpenMV Cam H7 (5) Arduino Nicla Vision (5) iVS-AWV3-AR0521 (6) TBD

What were the biggest problems encountered?: On-Board development tools are difficult to setup properly. Some on-board update links do not work.

Detailed Review:

Review of AMD Xilinx Kria KV260 Vision AI Starter Kit

the KV260 Vision AI Starter Kit is an out-ofthe-box platform for advanced vision application development. Some links to key information regarding this RoadTest follow.

What is in the box?

Summary of Experience with the AMD Xilinx Kria KV260 Vision AI Starter Kit

The Kria KV260 Vision AI Starter Kit is an affordable advanced vision application development without requiring complex hardware design knowledge. 

Kria KV260 Vision AI Starter Kit

The results and take away of the Kria KV260 Vision AI Starter Kit Applications for this RoadTest are itemized below:

  1. Out of the box experience of the is positive. All the hardware and software along with the various AI applications worked as expected.
  2. The KV260 hardware integration with the various existing AI applications works well.
  3. Building AI Applications with currently available online support from AMD/Xilinx is possible, but requires some effort.
  4. The KV260 AI vision kit hardware and software integration is good, but development tools integration for on-target development could be more polished.
  5. This board is a highly capable hardware on its own. The available AI vision applications add to make for a powerful combination of hardware/software.
  6. The KV260 hardware and available AI application software provide a solution that works on-target out of the box.
  7. On-Board Development was successfully done and demonstrated that it is possible to generate new AI vision applications with on-board tools.
  8. Documentation for the kit was tested and reviewed. The available documentation is ample, readily available, and nearly comprehensive.
  9. We found that most of the information needed was available in one form or another within the available online documentation. 
  10. We recommend the AMD Xilinx Kria KV260 Vision AI Starter Kit  and available, on-target ready to use AI vision applications as a powerful starting platform for AI vision solutions. 


Pro

  • No hardware design knowledge required to utilize and develop software for AI vision applications.
  • Documentation is readily available for the various Linux flavors.
  • On-line training and tutorials are available for learning and experimenting Using Accelerated Applications for the KV260.
  • All on-target readily available AI vision applications work well.
  • Easy use of AI neural network models.
  • AI vision applications can be accessed and will interface from remote locations
  • Boot firmware is robust and easy to update.
  • Linux integration works well.
  • Once the board has been properly updated, then applications can be up and running in a short time with no FPGA experience needed. 
  • Customization is possible via preferred design environments from application software to AI model to FPGA design.
  • Successful On-Board Development is possible: see section Experimenting and Developing with VitisTm AI Libraries and PetaLinux 2022.2 Boot FW


Con

  • Software needed to build on-target AI applications with the KV260 is not easily found.
  • On-target missing software development tools are hard to integrate when found.
  • In some instances it is not clear which development tools match which Linux flavor. 
  • On-target development tools generate errors that are difficult to decipher and troubleshoot.
  • When on-target software development tools are found and are integrated, the tools may still not work nor generate an executable application. 
  • Initial effort needed to update the board firmware . 
  • Somewhat easy to make mistakes with the firmware and Linux setup. Sometimes is necessary to start all the way from the beginning to correct for mistakes. 
  • On-target development in the Ubuntu environment is not well polished, and eventually did not work for the engineer performing this review.


Comments and Observations:

  • In-depth familiarization with the Xilinx software stack and how to use the available tools to develop applications will take time to be proficient. 
  • The Kria KV260 Vision AI Starter Kit hardware and AI vision Applications solution works very well, but a novice will not master this integration in a short time. 
  • The expectation that mastering the software and hardware integration for the Kria KV260 solution should be easy may detract some users when real issues inevitably arise. 
  • Integration of the AMD/Xilinx embedded toolchain can be problematic.
  • Integration of the software development toolchain was a weak point that took some time to resolve, and in some cases was not possible to resolve in the allotted time.
  • The user of the Kria KV260 Vision AI Starter Kit  must become knowledgeable with the AMD/Xilinx AI models. 
  • The available AI vision applications are very powerful and relatively easy to use after some initial effort (as expected).
  • Novice engineers may find the hardware/software integration a little daunting, but everyone should be able to rise to the challenge and learn from working with this kit. 
  • The available documentation does not make it clear that some information found in the various links are outdated or meant for a specific platform.
  • All efforts to develop new AI vision software was focused in the use of on-board capabilities only. No effort was taken to generate vision applications using off-target tools. 
  • In this review, no attempt was made to use tools for customization via design environments from application software to AI model to FPGA design.
  • The initial goal of the out-of-box experience is to get applications up and running in under one (1) hour, with no FPGA experience needed. This goal was not met due to the following:
    • need to update the boot firmware required reading, learning and experimenting. These efforts required more than one hour of labor.
    • there is a need to learn the AI vision semantics. This requires some time as well.
    • inevitable issues do arise at times that will require considerable time to resolve. 
    • once (a) the boot firmware is updated, (b) some reading and learning has taken place, and (c) hardware/software issues have been resolved, then (d) applications can be run in under one hour. 
  • On-board software development require a set of tools that are at times not easily accessible. 
  • When all the tools are in place (see section: Experimenting and Developing with Vitis AI Libraries and PetaLinux 2022.2 Boot FW), on-board development of AI applications is easily done. 
  • This kit does provides simplified hardware and software development with the aim to to become the fastest and easiest platform for application development with the goal of volume deployment on Kria K26 SOMs.
  • Disclaimer: The engineer performing the review acknowledges that some training and additional time may be needed to successfully develop new AI vision software using off-target tools and the Kria KV260 Vision AI Starter Kit. This roadTest review focuses on the on-target experience of the Kria KV260.  Existing on-target AI vision applications do work well however. 


Acknowledgment

Appreciation to AMD and element14 for providing the opportunity to review the AMD Xilinx Kria KV260 Vision AI Starter Kit. The RoadTest review program experience allows individuals to learn about new hardware and software solutions, and to provide service to the community by submitting a review of various products. 

Special note of gratitude to  AMD and element14 for providing a second KV260 board to help troubleshoot a video output issue with the original board. The availability of a second KV260 board helped identify a physical problem with the original board that was subsequently fixed. The second test board was subsequently returned to AMD.

Table of Contents


General Overview element14 RoadTest

The RoadTest program is the element14 community’s flagship product review program. Testers obtain a product to experiment and to provide element14 a written review of their experiences with the product. The following are important points pertaining to this program.

  • RoadTesters have 60 days from the receipt of the product to complete testing and review writing on element14.

  • The review must be filed on the special element14 Roadtest form.

  • Roadtesters who do not complete their reviews will not be eligible to participate in the program in the future. 

  • Roadtesters are shipped the kit free of charge (including customs and/or other fees).


RoadTest AMD Xilinx Kria KV260 Vision AI Starter Kit

This particular RoadTest  relates to the Kria KV260 Vision AI Starter Kit (see figure below). This kit intends to facilitate advanced vision application development out-of-the-box. The board is a non-production K26 System on Module (SOM) mounted to an evaluation carrier card optimized for vision applications. It is meant to provide multi-camera support via ON Semiconductor Imager Access System (IAS) and Raspberry Pi connectors.

The initial goal of the out-of-box experience is to get applications up and running in under one (1) hour, with no FPGA experience needed. Customization is possible via preferred design environments from application software to AI model to FPGA design.

This kit provides simplified hardware and software development with the aim to to become the fastest and easiest platform for application development with the goal of volume deployment on Kria K26 SOMs.

image

Specific RoadTest Goals 

  1. Produce a 2 to 3 minute unboxing video. 
  2. Test the out-of-box experience of the product.
  3. Build a project and show how you did it.


Documentation Summary


• Product Brief
• Datasheet
• User Guide
• Getting Started Guide
• Github Applications
• Kria SOM Github
• Avnet Page Brief
• Getting Started Video

The  Getting Started web page provides a pre- built reference image that can be written to a microSD card for out-of-the-box functionality. 

Main Function and Use:

The Xilinx® KriaTm KV260 Vision AI Starter Kit is comprised of a non-production version of the K26 system-on-module (SOM), carrier card, and thermal solution. The SOM is very compact and includes key components such as a

  • Zynq® UltraScale+Tm MPSoC based silicon device,
  • memory module,
  • boot module,
  • security module.

The carrier card allows various interfacing options and includes a power solution and network connectors for camera, display, and microSD card. The thermal solution has a heat sink, heat sink cover, and fan. The Kria KV260 Vision AI Starter Kit is designed to provide customers a platform to evaluate their target applications and ultimately design their own carrier card with Xilinx K26 SOMs. Target applications for the Kria KV260 Vision AI Starter Kit include

  • smart city vision
  • machine vision,
  • security cameras,
  • retail analytics,
  • other industrial applications.


AMD Xilinx Kria KV260 Vision AI Starter Kit Hardware Features:

  • KV260 Development platform for Kria K26 SOMs
  • Accessory pack for the Kria KV260 Vision AI Starter Kit:
    • KV260 Power Supply & Adapter
    • USB-A to micro-B Cable
    • Ethernet Cable
    • HDMI Cable (Male to Male)
    • MicroSD card and MicroSD to SD Adapter
    • 13MP Auto Focus RGB Camera Module


AMD Xilinx Kria KV260 Vision AI Starter Kit Sensors

The only sensor provided with the kit is 

  • 13MP Auto Focus RGB Camera Module

The kit can work with other USB cameras simultaneously. This RoadTest did not test a multi camera setup. 

First Contact and First Impressions of AMD Xilinx Kria KV260 Vision AI Starter Kit

  • First Second: 
    • compact hardware
    • all the necessary pieces seem to be present
    • this promises to be a good experience.
  • First sixty (60) seconds:
    • read documentation...
    • ok, need to update the board firmware
    • how do you update the boot firmware without messing up?
    • read documentation...
  • First Hour:
    • got the firmware in place
    • burn Linux in SD
    • boot machine
    • nothing happens...
    • got a live board, but no video output
  • First 24 Hours:
    •  board seems to be working but,
    • no video output
    • enter deep and heavy troubleshoot mode.
    • try different approaches, but no video output.

This particular board did not initially have video output. After much effort, nothing seemed to work still. AMD sent a replacement board to help troubleshoot the issues with the original board. As it turned out the camera socket had a short that Linux detected and kept it from utilizing vido output to the monitor. After cleaning the camera socket with compressed air and alcohol, the video output started to work as expected. 


Hardware Description

{gallery}My Gallery Title

image

KV260 Vision AI Starter Kit with Flexible Connectivity

KV260 Vision AI Starter Kit 

image

KV260 Starter Kit Block Diagram

image

Applications

KV260 Starter Ki


Software Description:

The following link provides a general overview of the Kria KV260 Vision AI Starter Kit in a form of a User Guide.

Kria KV260 Vision AI Starter Kit User Guide

The link below provides a flow for upgrading the firmware and selecting the Linux Operating System (OS)

 Getting Started with Kria KV260 Vision AI Starter Kit

The above web page provides a pre- built reference image that can be written to a microSD card for out-of-the-box functionality. This page also contains the Xilinx SOM Starter Linux image to a microSD card. In this website we find the following warning:

Important: Critical Firmware Update Required

To enable complete board functionality, compatibility with latest Operating Systems, and best performance, be sure to install the latest AMD provided boot firmware following the firmware update instructions available on the K26 Wiki

To update the firmware details are found in the following link

Kria K26 SOM

The purpose of this page is to provide developers with information and links to collateral available for the Kria K26 SOM, including documentation, pre-built images, firmware updates, and GitHub repositories.

Note: This RoadTest uses Ubuntu to run the latest of several accelerated applications from the App Store to evaluate KV260.

Firmware Update

The initial image update is done via the "Image Recovery Tool” which is a stand alone application for manually loading and configurating content of both A and B boot partitions. To install the latest AMD provided boot firmware following the firmware update instructions available on the K26 Wiki. Care must be given to do the initial update from a Firefox browser. Other browsers will fail the firmware update. The latest firmware can be dowloaded from the following link:

Xilinx download - 2022.1_update3_BOOT.BIN

Once the firmware has been updated, the software update detailed in the next section can be done. Once the Linux software is up to date, the other bootable image can be updated via the xmulti tool as specified below:

% sudo xmutil bootfw_update -i BOOT_xilinx-k26-starterkit-v2022.1-09152304_update3.BIN

After the image write is completed issue a power-on reset by pressing the RESET push-button or power cycling the board. After restart it is required by the user verify that Linux fully boots with the new boot FW to verify functionality. This is completed by executing “sudo xmutil bootfw_update -v” to validate successful boot against the new firmware. Note this must be completed on the platform restart immediately following the update, else the platform will fall back to the other boot partition on the next restart.

Once the firmware has been updated we verify the current bootable firmware as such:

$ sudo xmutil bootfw_update -v
[sudo] password for ubuntu: 
Marking last booted image as bootable
ubuntu@kria:~$ sudo xmutil bootfw_status
Image A: Bootable
Image B: Bootable
Requested Boot Image: Image A
Last Booted Image: Image A
XilinxSom_QspiImage_v1.1_20210422

ImageA Revision Info: XilinxSOM_BootFW_20220915

ImageB Revision Info: XilinxSOM_BootFW_20220915

In the case above both image A and B are bootable with the latest available firmware 

XilinxSOM_BootFW_20220915

Software Update: Linux Ubuntu

The Ubuntu Desktop 20.04.3 LTS software download page is found in the links below

Install Ubuntu on Xilinx

Getting Started with Kria KR260 Robotics Starter Kit

Ubuntu 22.04 + Ubuntu AI Demos

To access the successfully boot of Ubuntu from a computer running macOS, issue the following command to observe which COM ports appear when you plug in the USB cable attached to the KV260 into your computer:

 % ls /dev/tty.*                                     
/dev/tty.usbserial-XFL10PJXULJ40	/dev/tty.usbserial-XFL10PJXULJ42
/dev/tty.usbserial-XFL10PJXULJ41	/dev/tty.usbserial-XFL10PJXULJ43

Four serial ports are enumerated where the second numbered port  corresponds to the KV260 UART. To access the KV260 type the following:

% screen /dev/tty.usbserial-XFL10PJXULJ41 115200,cs8

Once the firmware update (from the previous section) has successfully completed and Linux successfully boots on the KV260, we have the following at the first terminal login:

Ubuntu 20.04.3 LTS kria ttyPS0

kria login: ubuntu
Password: 
You are required to change your password immediately (administrator enforced)
Changing password for ubuntu.
Current password: 
New password: 
Retype new password: 
Welcome to Ubuntu 20.04.3 LTS (GNU/Linux 5.4.0-1017-xilinx-zynqmp aarch64)

Once logged into the KV260 issue an update/upgrade cycle:

$ sudo apt update
$ sudo apt upgrade

Next set up the Xilinx Development & Demonstration Environment for Ubuntu 22.04 LTS by install the xlnx-config snap that is required for system management:

sudo snap install xlnx-config --classic --channel=2.x

Run the xlnx-config.sysinit command to install Kria specific Personal Package Archive (PPA) :

sudo xlnx-config.sysinit

Note on the use of screen for serial port communication

If using in macOS, the screen app may say that there is an issue regarding no pty available. This indicates that there is a zombie screen using the pty which can happen for any number of reasons such as the remote host terminating the connection to screen. To find if there is a zombie screen issue the following command from the terminal:

% screen -ls
There is a screen on:
	22652.ttys002.2021	(Detached)
1 Socket in /var/folders/r_/h5vt2q1x05b5f1jblnxxdvym0000gn/T/.screen.

To terminate the zombie screen issue the command:

% screen -XS 22652 quit

where the number 22652 is the screen id. The above commands are universal and apply to all platforms running screen. 

Accelerated Application Package Selection

General documentation for the  Xilinx® KriaTm KV260 Vision AI Starter Kit can be found here:

Kria KV260 Vision AI Starter Kit User Guide

Note: the above link is general in scope. Do not follow the links provided in this page as guide or tutorials for smart applications. 

The following link will take the user to a signup place where you can enter some information and in return a link is provided.

Smart Camera Accelerated Application

Once the personal information is accepted, follow the provided links to find the following selections. The landing page (link [1] in the figure) provides links to a number of links pertaining to the Kria SOM support. The [2] Kria KV260 takes the user to the Smart Application Landing page [3] shown in the figure below. Finally link [4] takes the user to the Smart Camera application (one of many).

[1] SOM Landing Page

[2] Kria KV260 Vision AI Starter Kit Applications

[4] Smart Camera

[1] Landing Page, [2] Pertaining to the Kria KV260, [3] Landing Page for the Kria kv260 Smart Applications. [4] Specific Links to the various applicable Smart Applications. 

A word of Caution

There are many choices to try pre-built smart applications. Read carefully to avoid going down a wrong path. Some accelerated applications such as the NLP-SmartVision only run in the Ubuntu 20.04 platform. Some other Accelerated Applications seem to run better in PetaLinux 2021.1 +. 

In addition, the documentation does not make it clear that some information found in the various links are outdated or meant for a specific platform. For example, in some instances the instructions indicate to install accelerated applications to your platform by executing a DNF install for the chosen application package group. This bit of information will tell a careful user that the instructions are mean for the PetaLinux platform. Even then, in some instances the above will not work since the PetaLinux distribution will not find the software to install. 

Successful: Smart Camera Application

The following link takes the user to the Quick Start portion of the how-to

Smart Camera Quick Start

Disable the desktop.

sudo xmutil      desktop_disable

Packages compatible with Kv260 are fond dusty:

$ sudo apt search xlnx-firmware-kv260

Full Text Search... Done
xlnx-firmware-kv260-aibox-reid/jammy 0.8-0xlnx1 arm64
FPGA firmware for Xilinx boards - kv260 aibox-reid application

xlnx-firmware-kv260-benchmark-b4096/jammy 0.8-0xlnx1 arm64
FPGA firmware for Xilinx boards - kv260 benchmark-b4096 application

xlnx-firmware-kv260-defect-detect/jammy 0.8-0xlnx1 arm64
FPGA firmware for Xilinx boards - kv260 defect-detect application

xlnx-firmware-kv260-nlp-smartvision/jammy,now 0.8-0xlnx1 arm64 [installed]
FPGA firmware for Xilinx boards - kv260 nlp-smartvision application

xlnx-firmware-kv260-smartcam/jammy,now 0.8-0xlnx1 arm64 [installed]
FPGA firmware for Xilinx boards - kv260 smartcam application

To install a package do:

sudo apt install xlnx-firmware-kv260-smartcam

Verify that it is captured under the listapps function, and to have dfx-mgrd re-scan and register all accelerators in the FW directory tree.

sudo xmutil listapps


Accelerator          Accel_type Base               Base_type #slots(PL+AIE) Active_slot

k26-starter-kits      XRT_FLAT k26-starter-kits      XRT_FLAT (0+0)          0,
kv260-smartcam        XRT_FLAT kv260-smartcam        XRT_FLAT (0+0)         -1
kv260-nlp-smartvision XRT_FLAT kv260-nlp-smartvision XRT_FLAT (0+0)         -1

The above says that the k26-starter-kits application is active on slot 0. This needs to unload first, then switch to kv260-smartcam application.

sudo xmutil unloadapp

Look for print out “remove from slot 0 returns: 0 (Ok)” to know that the firmware was unloaded correctly. Load the kv260-smartcam application next.

sudo xmutil loadapp kv260-smartcam

Look for "kv260-smartcam: loaded to slot 0" to know that the application loaded correctly. Ignore the warning "IRQ index 8 not found". At this point the smart camera application is ready for use.

Debug Tips

Visit the following link to read about some debug tips. 

Frequently Asked Questions / Common Debug Tips

There are a number of debug information issued after entries, and most of them seem ominous, but they are not relevant. Most importantly:

  • The Starter Kit needs an updated boot firmware.
  • Set timezone, the locale and the time and date.
  • Installing firmware binaries may cause dfx-mgr to crash and a restart is needed.
  • If dfx-manager crashes, restart it with this command:

sudo systemctl restart dfx-mgr.service

  • xmutil or dfx-mgr runs only in base OS, they do not run in Docker containers.
  • After invoking the command xmutil loadapp to load firmware, it needs several seconds for the whole firmware to be ready.
  • If you launch docker before the firmware is loaded, it will not be able to use DPU node properly and you may see the below error while launching application
  • To resolve the above issue do:
root@xlnx-docker/# exit
ubuntu@kria:~$ sudo xmutil unloadapp
ubuntu@kria:~$ sudo rm -rf /etc/vart.conf/
  • Do not have to worry about errors logged by the Linux kernel while executing the following specified commands, they are benign and can be ignored. The “ERROR: memory leak” error is a result of upstream Linux device tree framework.
xmutil unloadapp

... xilinx-kv260-starterkit-20221 kernel: OF: ERROR: memory leak, ...
... xilinx-kv260-starterkit-20221 kernel: OF: ERROR: memory leak, ...
  • Look for print out “remove from slot 0 returns: 0 (Ok)” to know that the firmware was unloaded correctly.
  • Look for print out "kv260-smartcam: loaded to slot 0" to know that the firmware was loaded correctly,
xmutil loadapp kv260-smartcam

... xilinx-kv260-starterkit-20221 kernel: debugfs: Directory '4-003c' with parent 'regmap' already present!
... xilinx-kv260-starterkit-20221 kernel: zocl-drm axi:zyxclmm_drm: IRQ index 8 not found
... xilinx-kv260-starterkit-20221 kernel: xilinx-video axi:isp_vcap_csi: Entity type for entity 80000000.csiss was not initialized!
  • Ignore the warning "IRQ index 8 not found". 
  • Important Note Regarding the File Structure: Files structure of the application are only available once the application has been loaded onto a docker. There may be other ways to access these files, but at least they are available once the docker is loaded. This may not be obvious to the user.
  • The MIPI Input (IAS sensor input) works well.
  • When running the smart cam application, information is stored in overlay. This decreases the space available for the OS to run. In some cases, the information stored will deplete all available space. In this case, find the available space with the following command:

sudo du -a /var | sort -n -r | head -n 10

  • If need be, you may have to delete files to increase file size. Some commands that will help:
docker  system prune

Docker based application

At this point the kv260-smartcam smart camera application has been loaded and is ready for use. The instructions on the docker based application work well, and are reproduced here for convenience. 

  • find the docker images installed with command:
docker images

REPOSITORY        TAG       IMAGE ID       CREATED        SIZE

xilinx/smartcam   2022.1    aa0270aef908   6 months ago   1.41GB

  • If needed, remove any unwanted docker image to save storage volume in the SD card:
docker rmi --force <other containers>
  • Note: when the smart camera application kv260-smartcam  runs for a long time, this may consume a lot of limited disk space in the SD. In some cases all the space available is consumed, and the Linux Operating System (OS) stops working properly. A solution is to free disk space, and a place to do this would be in the /var/lib/*/overlay2 space. This will (1) return space to the OS so that the OS is stable again, and (2) render the docker unusable, and the docker may have to be removed and pulled again once the OS is operationally stable once again. To find space utilization in the /var directory, issue the following command:

sudo du -a /var | sort -n -r | head -n 10

  • pull the 2022.1 docker image for smartcam using the below command (this may take some time)
docker pull xilinx/smartcam:2022.1
  • launch the docker using the below command
docker run \
--env="DISPLAY" \
-h "xlnx-docker" \
--env="XDG_SESSION_TYPE" \
--net=host \
--privileged \
--volume="$HOME/.Xauthority:/root/.Xauthority:rw" \
-v /tmp:/tmp \
-v /dev:/dev \
-v /sys:/sys \
-v /etc/vart.conf:/etc/vart.conf \
-v /lib/firmware/xilinx:/lib/firmware/xilinx \
-v /run:/run \
-it xilinx/smartcam:2022.1 bash
  • after a while, once done the following indicates successful operation:

2022.1: Pulling from xilinx/smartcam

Digest: sha256:da2e52629011aeec332152a0f468d3ff156917dba9b596cf6d0de958d5dc29d7
Status: Downloaded newer image for xilinx/smartcam:2022.1
docker.io/xilinx/smartcam:2022.1

  • the smartcam image will launch in a new container (see picture below)
root@xlnx-docker/#


Figure kv260-smartcam application loaded in a docker.
  • at this point the file structure will be available for further action

Run the Smart Camera kv260-smartcam Application

The Smart Camera kv260-smartcam Application will run via Jupyter notebook. This is a polished method that is suitable to learn and run the application. The instructions in the following link are self explanatory, but are reproduced here for convenience with added comments. 

Smart Camera Application Deployment

At this point it is beneficial to monitor the SD disk space usage and availability:

$ df -h

/dev/mmcblk1p2 14G 13G 759M 95% /

The disk space is at 95% full. The docker now contains the smart camera tree:

root@xlnx-docker:/opt/xilinx/kv260-smartcam# ls -al
total 40
drwxr-xr-x 5 root root 4096 Sep 26 2022 .
drwxr-xr-x 3 root root 4096 Sep 26 2022 ..
-rw-r--r-- 1 root root 19198 Sep 26 2022 README_SMARTCAM
drwxr-xr-x 2 root root 4096 Sep 26 2022 bin
drwxr-xr-x 2 root root 4096 Sep 26 2022 lib
drwxr-xr-x 5 root root 4096 Sep 26 2022 share

Run the command smartcam-install.py to install the package shipped notebooks which reside in /opt/xilinx/kv260-smartcam/share/notebooks to the folder /root/notebooks/smartcam

root@xlnx-docker:/opt/xilinx/kv260-smartcam/bin# ./smartcam-install.py
Info: Notebook files under /opt/xilinx/kv260-smartcam/share/notebooks are copied to /root/notebooks/smartcam.

Find the IP address for the board, and next launch Jupyter notebook on the target (note: substitute ip=x.x.1.17 with a proper address):

root@xlnx-docker:~# jupyter-lab --notebook-dir=/root/notebooks/smartcam --allow-root --ip=x.x.1.17 &

root@xlnx-docker:~# [I 02:18:02.593 ServerApp] jupyterlab | extension was successfully linked.
[I 02:18:02.653 ServerApp] nbclassic | extension was successfully linked.
[I 02:18:02.660 ServerApp] Writing Jupyter server cookie secret to /root/.local/share/jupyter/runtime/jupyter_cookie_secret
[I 02:18:03.725 ServerApp] notebook_shim | extension was successfully linked.
[I 02:18:03.814 ServerApp] notebook_shim | extension was successfully loaded.
[I 02:18:03.820 LabApp] JupyterLab extension loaded from /usr/local/lib/python3.10/dist-packages/jupyterlab
[I 02:18:03.820 LabApp] JupyterLab application directory is /usr/local/share/jupyter/lab
[I 02:18:03.839 ServerApp] jupyterlab | extension was successfully loaded.
[I 02:18:03.859 ServerApp] nbclassic | extension was successfully loaded.
[I 02:18:03.861 ServerApp] Serving notebooks from local directory: /root/notebooks/smartcam
[I 02:18:03.861 ServerApp] Jupyter Server 1.18.1 is running at:
[I 02:18:03.861 ServerApp] http://10.137.1.17:8888/lab?token=31ec81178347d467146131c34dd3506e039fa7dc45124804
[I 02:18:03.861 ServerApp] or http://127.0.0.1:8888/lab?token=31ec81178347d467146131c34dd3506e039fa7dc45124804
[I 02:18:03.862 ServerApp] Use Control-C to stop this server and shut down all kernels (twice to skip confirmation).
[W 02:18:03.879 ServerApp] No web browser found: could not locate runnable browser.
[C 02:18:03.880 ServerApp]

To access the server, open this file in a browser:
file:///root/.local/share/jupyter/runtime/jpserver-19-open.html
Or copy and paste one of these URLs:
http://x.x.1.17:8888/lab?token=31ec81178347d467146131c34dd3506e039fa7dc45124804
or http://127.0.0.1:8888/lab?token=31ec81178347d467146131c34dd3506e039fa7dc45124804

To access the server, go to a remote computer and type the below line to access the Jupyter notebook (see above):

http://x.x.1.17:8888/lab?token=31ec81178347d467146131c34dd3506e039fa7dc45124804

The following interface shown in the figure below runs on the browser:

Figure: Jupyter notebook running on a browser in a remote machine. [1] select and double-click on the smartcam notebook. [2] select, edit and modify a cell to run. [3] click on the forward arrow to run the selected cell and advance to the next one. 

At this point the smarcam notebook is active and ready to run. Select each consecutive cell and edit, modify and run as desired. In this particular case we choose the mipi camera supplied by the vendor. 

source = "mipi" # choose either 'mipi' or 'usb'

We also choose to have RTSP output to be able to stream from a remote computer. 

DP_output=False # True to choose DP output, False to choose RTSP output

After all the cells have been run for the RTSP output branch, the following output indicates what to do next:

Video is now streaming from mipi source. 
    Run the command "ffplay rtsp://x.x.1.17:5000/test" in another PC which have network access to the SoM board to view the video.

From a remote computer run the command line 

ffplay rtsp://x.x.1.17:5000/test

The following is a screen capture of the working application:

Figure: Smart Camera kv260-smartcam Application running. 

The figure above shows the Smart Camera kv260-smartcam Application capture three faces simultaneously. The app captures the faces in real-time while both the camera itself is in motion and the subject is in motion. The following video demonstrates the application working in real-time.

Video: Smart Camera kv260-smartcam Application running in real-time. 

Stop the Smart Camera kv260-smartcam Application and docker container

Verify which docker is active by using docker ps command to see it in the running containers list.

$ docker ps
CONTAINER ID IMAGE COMMAND CREATED STATUS PORTS NAMES
4d4e8a0dd2dd xilinx/smartcam:2022.1 "bash" 11 hours ago Up 11 hours optimistic_chandrasekhar

$ docker images
REPOSITORY TAG IMAGE ID CREATED SIZE
xilinx/smartcam 2022.1 aa0270aef908 6 months ago 1.41GB


Next we stop and then remove the docker

$ docker stop optimistic_chandrasekhar
$ docker rm optimistic_chandrasekhar

Verify that the docker is not running any longer 

$ docker ps -a
CONTAINER ID IMAGE COMMAND CREATED STATUS PORTS NAMES

The docker image is still loaded

$ docker images
REPOSITORY TAG IMAGE ID CREATED SIZE
xilinx/smartcam 2022.1 aa0270aef908 6 months ago 1.41GB

The following command will remove all containers

$ docker rm `docker ps -a -q`

Remove all “Exited” containers:

$ docker rm $(docker ps -a | grep 'Exited' | awk '{print $1}')

Remove all images matching a name (xilinx in this case):

$ docker rmi $(docker images | grep xilinx | awk '{print $3}')

Docker has a single command that cleans up all dangling resources, such as images, containers, volumes, and networks, not tagged or connected to a container.

$ docker  system prune

For our particular case,  we verify disk space use before we rm the docker image

$ sudo du -a /var | sort -n -r | head -n 10
[sudo] password for ubuntu:
4240500 /var
4022796 /var/lib
2130392 /var/lib/snapd
1506484 /var/lib/docker
1505588 /var/lib/snapd/snaps
1502732 /var/lib/docker/overlay2
636052 /var/lib/docker/overlay2/1d11636fc2d2f5dff498c2c1411948dbb705144ec2567be2e4cb276df534c431
636036 /var/lib/docker/overlay2/1d11636fc2d2f5dff498c2c1411948dbb705144ec2567be2e4cb276df534c431/diff
622340 /var/lib/snapd/seed
622244 /var/lib/snapd/seed/snaps

next we remove the docker image with the command

$ docker rmi $(docker images | grep xilinx | awk '{print $3}')

Finally we verify that the disk space has been returned

$ sudo du -a /var | sort -n -r | head -n 10
2734428 /var
2516716 /var/lib
2130392 /var/lib/snapd
1505588 /var/lib/snapd/snaps
622340 /var/lib/snapd/seed
622244 /var/lib/snapd/seed/snaps
458588 /var/lib/snapd/snaps/gnome-42-2204_69.snap
342056 /var/lib/snapd/snaps/gnome-3-38-2004_138.snap
239004 /var/lib/snapd/seed/snaps/gnome-3-38-2004_107.snap
221168 /var/lib/snapd/snaps/firefox_2486.snap

And verify the total disk space has returned from 95% utilization after we loaded the docker image to a reasonable 84% disk utilization after we remove the docker image. 

$ df -h
Filesystem Size Used Avail Use% Mounted on

/dev/mmcblk1p2 14G 11G 2.2G 84% /

Learning and Experimenting with the AMD Xilinx Kria KV260 Vision AI Starter Kit

Xilinx provides a plethora of hardware, AI tools and AI libraries to users. The combination of hardware, tools, models types and samples is very rich. This section will explore the availability of the universe composed of hardware, tools, libraries and experiment with how easily these can be manipulated and utilized. The primary reason to explore with the VitisTm AI Libraries is to use pre-trained Xilinx models to quickly build applications. 

Successful On-Board Development: Experimenting and Developing with VitisTm AI Libraries and PetaLinux 2022.2 Boot FW

The primary link for this section is found below.

Running Vitis AI Library Examples

The original SD card that came with the AMD Xilinx Kria KV260 Vision AI starter Kit had too little room for all the development tools and example images needed to experiment with the  Vitis AI Libraries. A larger SD was used to instal a PetaLinux Board Image.

SD Image for xilinx-kv260-dpu-v2022.1-v2.5.0

This image is used exclusively for experimenting with Vitis AI Libraries and quickly building examples projects. Current designs only supports Vitis AI 2.5.0 libraries. At the very least, If a developer or user has custom models that are completely different from the models supported by the Vitis AI Library or have specialized post-processing requirements, the user can use the Vitis AI library implementations for reference. The figure below shows the portal to the Vitis AI 2.5.0 libraries.

Vitis AI Library

The Vitis AI Library contains four parts:

Base libraries
The base libraries provide the basic programming interface with the DPU and the available post-processing modules of each model. dpu_task is the interface library for DPU operations. cpu_task is the interface library for operations that are assigned to the CPU. xnnpp is the post-processing library for each model, with built-in modules such as optimization and acceleration.
Model libraries
The model libraries implement most of the open-source neural network deployment including common types of networks, such as classification, detection, segmentation, and others. These libraries provide an easy-to-use and fast development method with a unified interface, which apply to the Xilinx models or custom models.
Library test samples
The library test samples are used to quickly test and evaluate the model libraries.
Application demos
The application demos show you how to use the Vitis AI Library to develop applications.

The figure below shows the block diagram for the Vitis AI 2.5.0 libraries. 

Compiling the Example

The PetaLinux image contains all the libraries and tools for on-target development. Xilinx provides the resources for programing with cross compilation tools in a host and then transfer the executable to the board. In our case we compile directly on the target board the Kria KV260.

The first step is to install the board image by  flashing the SD card with Etcher. The Vitis AI runtime packages and the Vitis AI Library model packages and library packages and other samples and models are built into the board image. Therefore the user does not have to install these on the board separately. 

The following is an example of source files for example source code that will pair a neural network model type with model data to generate a result. 

root@xilinx-kv260-starterkit-20221:~/Vitis-AI/examples/Vitis-AI-Library/samples/yolov3# ls -al
total 1112
drwxr-xr-x 2 root root 4096 Apr 3 11:56 .
drwxr-xr-x 53 root root 4096 Apr 3 11:48 ..
-rwxr-xr-x 1 root root 1190 Mar 9 2018 build.sh
-rw-r--r-- 1 root root 1867 Mar 9 2018 process_result.hpp
-rw-r--r-- 1 root root 6258 Mar 9 2018 readme
-rw-r--r-- 1 root root 3262 Mar 9 2018 test_accuracy_tiny_yolov3_vmss.cpp
-rw-r--r-- 1 root root 3225 Mar 9 2018 test_accuracy_yolov3_adas_pruned_0_9.cpp
-rw-r--r-- 1 root root 3271 Mar 9 2018 test_accuracy_yolov3_bdd.cpp
-rw-r--r-- 1 root root 4095 Mar 9 2018 test_accuracy_yolov3_coco_416_tf2_mt.cpp
-rw-r--r-- 1 root root 4161 Mar 9 2018 test_accuracy_yolov3_mt.cpp
-rw-r--r-- 1 root root 3387 Mar 9 2018 test_accuracy_yolov3_voc.cpp
-rw-r--r-- 1 root root 3512 Mar 9 2018 test_accuracy_yolov3_voc_tf.cpp
-rw-r--r-- 1 root root 1070 Mar 9 2018 test_jpeg_yolov3.cpp
-rw-r--r-- 1 root root 865 Mar 9 2018 test_performance_yolov3.cpp
-rw-r--r-- 1 root root 1071 Mar 9 2018 test_video_yolov3.cpp

To compile the source code on target (i.e. Kria KV260) the simply run the build.sh command on a terminal. 

# sh build.sh 

After a short while the executable programs are available for testing. In our case we issue the following command:

# ./test_jpeg_yolov3 yolov3_bdd yolov3/sample_yolov3.jpg 

After successful completion the result is shown on the terminal

I0403 12:51:29.856228 2106 demo.hpp:1183] batch: 0 image: /home/petalinux/samples2/samples/yolov3/sample_yolov3.jpg
I0403 12:51:29.856499 2106 process_result.hpp:44] RESULT: 2 355.623 143.204 416.623 164.574 0.843508
I0403 12:51:29.856628 2106 process_result.hpp:44] RESULT: 2 115.72 139.289 185.977 182.711 0.730628
I0403 12:51:29.856691 2106 process_result.hpp:44] RESULT: 2 401.178 135.767 512 245.528 0.730601
I0403 12:51:29.856755 2106 process_result.hpp:44] RESULT: 2 323.695 141.1 360.952 158.049 0.705315
I0403 12:51:29.856813 2106 process_result.hpp:44] RESULT: 2 299.126 135.785 334.126 153.827 0.698933
I0403 12:51:29.856869 2106 process_result.hpp:44] RESULT: 2 164.063 136.371 196.942 159.537 0.592455
I0403 12:51:29.856925 2106 process_result.hpp:44] RESULT: 2 -0.840607 131.914 129.028 256 0.561093

A different test run and its output:

# ./test_performance_yolov3 yolov3_bdd test_performance_yolov3.list -t 8

I0403 13:02:05.918325 2986 benchmark.hpp:184] writing report to <STDOUT>
I0403 13:02:08.667546 2986 benchmark.hpp:211] waiting for 0/30 seconds, 8 threads running
I0403 13:02:18.667785 2986 benchmark.hpp:211] waiting for 10/30 seconds, 8 threads running
I0403 13:02:28.668031 2986 benchmark.hpp:211] waiting for 20/30 seconds, 8 threads running
I0403 13:02:38.668344 2986 benchmark.hpp:219] waiting for threads terminated
FPS=14.2527

These simple tests confirm the following:

  • AI libraries are readily available to users.
  • The  VitisTm AI Libraries provide the bases to quickly build applications. 
  • Developing with User Model and AI Library can be readily done by working within the scope of the Vitis AI Library.

Experimenting and Developing with the Ubuntu 2022.4 Image as a Development Environment

As a review point, the Ubuntu image used is found in the link below:

https://ubuntu.com/download/amd-xilinx

Some other links used in this effort:

https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/1641152513/Kria+K26+SOM

https://www.xilinx.com/products/som/kria/kv260-vision-starter-kit/kv260-getting-started/getting-started.html

https://www.hackster.io/dsp2/easy-machine-learning-on-ubuntu-with-the-xilinx-kria-kv260-c77ed1

Some useful commands:

sudo apt install vitis-ai-runtime  vitis-ai-library

sudo snap install xlnx-vai-lib-samples

sudo xmutil desktop_disable

xdputil query

To change the ssh keys:

ssh-keygen -f ~/.ssh/known_hosts -R ip.addr

Some comments and conclusions:

  • This effort was unsuccessful. Some tools were missing, and some tools could not be found. 
  • Failure in this effort may be related to the engineer's inexperience, but after some considerable effort, the engineer was still not able to make this work.
  • Firmware not easily available.
  • Development in the Ubuntu environment is not well polished.
  • Some development tools were not found or not available at the time of this review.
  • Ambiguity regarding tools availability. 
  • Was not possible to generate new software in this environment. 

Experimenting and Developing with the PetaLinux Image 2021.1 as a Development Environment

Please note: 

for later version of DPU designs you may check with "xdputil query" instead of "dexplorer -w"!

This below link

https://www.xilinx.com/member/forms/download/xef.html?filename=petalinux-sdimage-2021.1-update1.wic.xz

Will provide the file:  

petalinux-sdimage-2021.1-update1.wic.xz

After initial boot of a new SD card image it is best practice to execute sudo dnf update in order to update core utilities that may have been released following the SD card image release.

Some comments and conclusions:

  • Considerable effort to find all the necessary tools
  • When found, some tools were non-functional or required other tools that were not available.
  • Some missing tools were not possible to be found, and no solution was found
  • Not possible to develop in this PetaLinux 2021.1 environment within the allowed time. 

Final thoughts on on-board development of AI vision applications:

  • It is difficult to find all the tools needed to generate on-board Ai vision applications. 
  • This RoadTest has demonstrated that it is possible to successfully generate new AI vision applicants with on-board tools only. 

Documentation and Integration Review

The work has been presented above. These are some compact itemized reviews for the documentation and for the hardware/software integration.

Documentation Review

  • Documentation is readily available
  • Documentation is ample. 
  • Documentation is not clear or specific at times.  
  • Sometimes the available documentation seems to be outdated. 

Hardware/Software Integration Review

  • Robust hardware
  • Robust hardware and existing AI vision application software integration
  • Hardware/Software works out-of-the-box as expected.
  • Easy to re-purpose existing AI vision applications
  • Development of new AI vision applications needs polish
  • Workflow for software development requires more learning and training.
  • The AMD/Xilinx hardware and AI vision application solution is a viable powerful platform for IoT applications. 

Results

The following are results and take away of the AMD Xilinx Kria KV260 Vision AI Starter Kit RoadTest:

  1. Out of the box experience of the AMD Xilinx Kria KV260 Vision AI Starter Kit is positive. All the hardware and available AI vision software worked as expected.
  2. The Kria KV260 hardware integration with the existing AMD/Xilinx AI application software is effective and error free.
  3. Building an AI vision application with current on-board development tools requires some effort. 
  4. The 13MP Auto Focus RGB Camera Module was tested and worked well. 
  5. The Kria KV260 board is robust and highly capable hardware on its own that is easy to integrate in/with any number of embedded projects.
  6. The AMD Xilinx Kria KV260 Vision AI Starter Kit provides a powerful AI vision solution that works out of the box.
  7. The available documentation is ample, complete, readily available, and comprehensive with some exceptions.
  8. The documentation itself was tested, and we found that all information needed was available in one form or another within the available documentation.
  9. On-Board Software Development tools and related workflow could be more polished.
  10. At times, development workflow simply does not work due to tools not being available or poorly integrated. This may be the result of poor training of the engineer performing the evaluations. 
  11. Additional Camera sensors could be added to the hardware but were not tested in this review.
  12. This kit does provides simplified hardware and software development.
  13. On-Board Application development is possible, and when the tools are properly setup, development is fast and relatively easy.  
  14. Section: Experimenting and Developing with Vitis AI Libraries and PetaLinux 2022.2 Boot FW), demonstrates that on-board development of AI applications is easily done. 
  15. Once an application has been developed, it is very easy to perform volume deployment on Kria K26 SOMs hardware.

Conclusions

All the RoadTest objectives were met satisfactorily and are summarized in the Results section above this one. 

The AMD Xilinx Kria KV260 Vision AI Starter Kit board is a capable hardware that can be the starting point for any number of embedded projects, and it is highly recommended all on its own. Existing documentation is ample and comprehensive. We recommend the AMD Xilinx Kria KV260 Vision AI Starter Kit and the available AI vision software application as an efficient starting platform for AI vision applications. 

Anonymous