Roadtest: Nordic Bluetooth LE Audio Development Kit nRF5340 DK by Steve K

View table of contents ...  

RoadTest: Nordic Bluetooth LE Audio Development Kit nRF5340 DK

Author: skruglewicz

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Other Nordic products that use nRF Connect SDK. nRF9160 Thingy-53.

What were the biggest problems encountered?: Getting myself familiar with the usage of the toolchains again and not being able to use the nRF-Connect extensions for VS Code, was a bit of a challenge. I was unable to follow the Audio example and get the Firmware programmed onto the boards, so I could test, Very frustrating.. I hope this will improve and bring in VSCode support...

Detailed Review:

This is a review of the Nordic nRF5340 Audio DK  (Development Kit).  This Development Kit was supplied to me by the RoadTest sponsor Nordic Semiconductor. I was supplied with 2 DK's to experiment with. I'm a little late to the game, since another member was unable to do the review. So, I'll try my best to give this product a fair review. The Nordic Semiconductor nRF5340 Audio Development Kit (DK) is an impressive platform for Bluetooth LE Audio products. It is a comprehensive kit that contains everything needed to start development, including the nRF5340 SoC, nPM1100 PMIC, and Cirrus Logic’s CS47L63 Audio DSP. These are depicted in the following photo courtesy of figure 7 located on the element14 blog 

Learn the Basics and Implementations of Bluetooth LE Audio and its Applications

 

image

I took the quiz that was included on this blog at Take the Bluetooth LE Audio Quiz.

image

This is an excellent resource that I used to get familiar with  Bluetooth LE Audio

One of the most interesting features of this DK is its configurability. It can function as a USB dongle to send or receive audio data from a PC, a Business Headset, or a True Wireless Stereo (TWS) Earbud. The kit also supports all Auracast features.

The CS47L63 Audio DSP is optimized for direct connection to an external headphone load, making it perfect for earbuds with mono-only and direct speaker output. It also supports the new “Low Complexity Communications Codec” (LC3), which has superior audio quality compared to Bluetooth Classic’s “Low Complexity Subband Codec” (SBC).

The nRF5340 SoC combines a high-performance application processor with a fully programmable ultra-low-power network processor. This dual core architecture allows for optimal power efficiency. The 128 MHz Arm Cortex-M33 Application Processor has 1 MB flash and 512 KB of RAM, which is perfect for handling custom applications and audio codecs like LC3. The 64 MHz Arm Cortex-M33 Network Processor has 256 KB Flash and 64 KB RAM and is power optimized to run Nordic’s Bluetooth LE Audio stack.

The nPM1100 power management IC has a highly efficient configurable buck regulator and includes an integrated battery charger with a charge current up to 400mA. It is extremely small and ideal for size-constrained applications like True Wireless Earbuds.

The nRF Connect SDK is the software development kit for the nRF5340 SoC, and it has board support for the nRF5340 Audio DK. It supports the development of Bluetooth LE Audio, Bluetooth Low Energy, Thread, and other applications. The Zephyr RTOS, protocol stacks, samples, hardware drivers, and much more are integrated in the nRF Connect SDK. The kit also includes two 3.5 mm audio jacks for analog in and headphones out, five user-programmable buttons and LEDs, a battery, an SD-Card holder for extra storage if needed, a J4 connector for an NFC antenna, and connectors to access the analog/digital interfaces and GPIOs.

Overall, the Nordic Bluetooth LE Audio Development Kit nRF5340 DK is an excellent development platform that provides exceptional performance, power efficiency, and flexibility. It is highly recommended for developers who want to create Bluetooth LE Audio products with superior audio quality. It can be used to develop proof-of-concept firmware demonstrating the usage of the nRF5340 SoC, nPM1100 PMIC, and Cirrus Logic’s CS47L63 Audio DSP.

Getting Started

I usually do an unboxing with roadtest reviews. I chose not to for this review because, there are 3 items in each box, and the documentation explains much of the DK in detail

I am a musician (a Drummer)  and have always wanted to experiment with Digital Signal Processing. I'm excited to get into this review. When my package arrived it contained 2 boxes.  Each box contained a Kit, Battery and a Leaflet.. The leaflet has a link to the kit introduction page, which I read through. A quarter way down the page, there are navigation tabs that include the following links :  Overview, Development Tools, Downloads, and Get Started.

image

Unless your familiar with Nordic documentation, this could be a little confusing for a start page where one wants to start using the board. Also, putting the "Geat Started” at the end of the tab bar, in my option seems to be misplaced. It should be at the beginning of the page, in my humble opinion.

I read through all the tabs and on the "Get Started" tab, I followed the 4 step wizard titled  "Connect and test the nRF5340 Audio DK"   This is a simple Blinky program that comes .pre installed on the DK. It is used primarily , I believe, to test If the Board and Battery are working.

I observed a few discrepancies,  on step 3  it is stated that "the Nordic logo should light up yellow now". It actually more green than yellow. and LED 3 is blinking and another LED to the Left is a solid green?

Second, on step 4, "unplug the usb-c cable and connect the included battery". I received 2 kits for the roadtest, and in my hast getting started, I never noticed the battery tucked away in the bottom of the box. Once I found them well into my review I connected them and they worked fine. The kit items come in a compact little box, so make sure you don't make the same mistake I did.

The rest of the "Get started" tab contains links to more Nordic documentation. 

  1. if you are new to development with Nordic you can start at the  Getting started with nRF Connect SDK.
  2. If you are already familiar with the nRF Connect SDK go to our nRF5340 Audio documentation.
  3. If you need answers, the Community - DevZone Explore DevZone, is an excellent resource.

nRF Connect SDK

I have used the nRF Connect SDK before, so I skipped over this link. I have 2 Nordic products that I used the nRFConnect SDK on. The first  for an Element14 roadtest on another Nordic product, the  nRF9160. and a Hackster.io project for the Thingy53. I needed  to refresh my memory on using the nRF SDK again. But I will not be focusing on the usage of the development toolchain in this review. The following section describe these 2 project, with links to the blogs pages ,if you have an interest.

Element 14 ROADTEST-  This was a very interesting board. I enjoyed my time developing with the nRF SDK and the Toolchains along with using VS Code to develop code. The LTE implementation went flawless. the Product Performed to Expectations I was expecting to have connection issues . Overall the product was easier to get up and running then the AVNET Monarch LTE-M Development Kit.

Nordic nRF9160 DK -- A single board development kit for evaluation and development on the nRF9160 for LTE-M - element14 Community

Hackster.IO - I entered a challenge on hackster Smarter Sustainable World Challenge. In this challenge I was awarded A FREE Nordic Thingy-53 to experiment with. It was far different than the nRF8160. I did not have a much luck getting my project completed, but I did do 3 projects devoted to the Thingy-53. 

 Research & Experimentation with the Nordic Thingy:53 - Hackster.io

Thingy:53 – Home Energy Monitoring Station - Hackster.io

A Thread Border Router with Pi 4 and nRF9160 - Hackster.io

nRF Connect SDK- NRF5340 Audio.

Now, lets get going with the audio.

image

I have many audio devices as I've depicted here. Including

  • Bluetooth Headphones and Speakers.
  • Direct Headphones
  • In ear monitors that I use for gigs.
  • Berringer audio amplifier's, that I use with my In-ears at gigs.

I used some of these in my experiments.

The following two links were helpful in experimenting with the audio.

InfoCenter - nRF5340 Audio DK Hardware

This page located on Nordic's InfoCenter site,  it contains hardware infomation on the board. It is helpful to describe Pin and peripherals of the Kit. I referred to it during my review, to learn more about the hardware used in the application document, to better understand the workings of the kit.

image

nRF Connect SDK- NRF5340 Audio - Application

nRF Connect SDK- NRF5340 Audio.

image

This page contains an application that offers a way to experiment with the kit. It is located on the Nordic nRFConnect SDK doc page. I spent most of my time on this document and describe my experience in the remainder of this review.

The NRF audio application is described in this NRF SDK documentation .The nRF5340 Audio application is a software developed for audio playback over isochronous channels (ISO) using LC3 codec compression and decompression, following the Bluetooth® LE Audio specifications. It is designed to work with the nRF5340 Audio development kit and includes various tools, such as the buildprog.py Python script for building and programming the firmware.

It should be noted that the application is undergoing a restructuring process, which involves moving drivers and modules to more suitable locations in the nRF Connect SDK or Zephyr, making it currently more complex to develop out-of-tree applications.

Again  This document is very dense and concise. Be prepared to study it thoroughly before experimenting with the kit. It Contains several sections on the explanation of the audio application. The first section, overview is a very intensive overview of the application design and logic two boards will be able to do gateway and one side of the audio if you had three boards and you could have a gateway right side and left side.

My Nordic BLE board will not be able to be used as a gateway as I thought. It does not contain the audio chip that the kit board has unfortunately.

To build and program the firmware You will need to use the command line tool chain and the Python script builder. It is noted that the NRF connect for VS code is not supported for the example. not sure why?  Again, it is noted that development toolchains are presently in a state of flux, so that might be the reason..

Building Process of Nordic nRF5340 Audio DK

In this section, I will discuss the challenges encountered during the building process of the Nordic nRF5340 Audio DK Application example and propose potential improvements for the documentation. Specifically, we will address the difficulties faced when using Visual Studio Code (VSCode) and the issues with the provided build options, as highlighted by fellow Road testers. 

A review by Gough Lui  Nordic Semiconductor nRF5340 Bluetooth Low-Energy Audio Development Kit RoadTest Review

A review by Fred27  Nordic nRF5340 Audio Development Kit review

Building Difficulties with VSCode:

The documentation clearly states that VSCode is not supported for the nRF Connect Extensions, causing problems for users who are accustomed to working with this popular IDE. It is essential to highlight this limitation upfront to avoid wasted efforts and frustration among developers attempting to use VSCode. Clear instructions on alternative IDEs or workarounds would greatly assist users in finding compatible development environments.

For example the environment variables for the WEST toolchains are not installed as the following screenshot clearly shows.

image

Challenges with Build Options:

The provided documentation offers two build options: using the command line or a Python script. However, both options seem to present challenges, as reported by other Road testers.

Command Line Approach:

Both Gough and I encountered issues while following the command line instructions. Although Gough eventually succeeded after overcoming these challenges, it is evident that the process can be confusing and time-consuming. This indicates a need for enhanced clarity and detailed troubleshooting steps to assist users in resolving common issues.

Python Script Approach:

Fred27's experience with the Python script approach also highlighted challenges. While the script eventually worked after resolving some issues with dependencies, the process of building the example should ideally be streamlined. Relying on manual dependency management and troubleshooting is not an optimal solution. Providing a more seamless and straightforward method for building with the Python script would greatly benefit users.

 For example the following command line error running the script

image

BUILDING AND PROGRAMMING the AUDIO Example using the script

Development platform used

  • Windows10
  • nRFConnect SDK version v2.4.0
  • nRF Connect for VS Code Extension Pack  v2022.9.6

BUILDING 

run from C:\A\s1

to build the script go to the directory    cd C:/A/s1/tools/buildprog

documentation is here:

https://developer.nordicsemi.com/nRF_Connect_SDK/doc/latest/nrf/applications/nrf5340_audio/README.html#building-and-programming-using-script

The idea is that you 

  • find out the serial numbers of your Audio DKs, 
  • enter them into a JSON file to specify them as a gateway or earbud (left or right) 
  • and the script will program them as appropriate. 

Use the python script: buildprog.py on the tools directory under the copied audio directory

image

Preparing the JSON file

The script depends on the settings defined in the nrf5340_audio_dk_devices.json file. Before using the script, make sure to update this file with the following information for each development kit you want to use:

  • nrf5340_audio_dk_snr – This field lists the SEGGER serial number. You can check this number on the sticker on the nRF5340 Audio development kit. 
    • Alternatively, connect the development kit to your PC and run nrfjprog -i in a command window to print the SEGGER serial number of the kit.
    • image
  • nrf5340_audio_dk_dev – This field assigns the specific nRF5340 Audio development kit to be a headset or a gateway.
  • channel – This field is valid only for headsets operating in the CIS mode. It sets the channels on which the headset is meant to work. When no channel is set, the headset is programmed as a left channel one.

image

1050171701 = headset left (Orange USB)

1050131916 – gateway (BLACK USB)

Running the script

NOTE: from here on I used VSCode to run the script and edit file.

Right click on the folder and select “open with code”

image

After editing the nrf5340_audio_dk_devices.json file, run buildprog.py to build the firmware for the development kits. The building command for running the script requires providing the following parameters, in line with nRF5340 Audio configuration files:

  • Core type (-c parameter): appnet, or both
  • Application version (-b parameter): either release or debug
  • Device type (-d parameter): headsetgateway, or both
  • DFU type (-m parameter): internalexternal
  • Network core bootloader minimal size (-M)

I ran example 2

python buildprog.py -c both -b debug -d both -m internal  -M 

Just as FRED27 stated there were problems with this build command

  • Buildprog.py failed with "No module named 'colorama'
  • Bildprog.py failed with "No module named ‘prettytable’"
  • 'west' is not recognized as an internal or external command

The following solution was suggested by a fellow element14 user  I also spent many hours with the "automated" install. About installing "colorama" etc, i don’t think this is the optimal solution because they are already installed, you just have to use environment variables in the terminal in order to find the correct python environment (maybe like this) or you can use the terminal created from Toolchain Manager.The PAGE instructs you to enter the command zephyr\zephyr-env.cmd

 image

I decided to get out of VSCode and run the python script from the Tool Manager as described in the next section

Running the script from Tool Manager bash 

The Bash command is available from the Toolchain manager “SDK Environments”  sdk version tab pull down menu. Getting there is a little confusing, so I included the following screenshot to illustrate selecting it. I’m using the version nRF Connect SDK v2.4.0.

image

Getting help on the script arguments

Run python buildprog.py -h for information about all available script parameters.

image

The building command for running the script requires providing the following parameters, in line with nRF5340 Audio configuration files:

  • Core type (-c parameter): appnet, or both
  • Application version (-b parameter): either release or debug
  • Device type (-d parameter): headsetgateway, or both
  • DFU type (-m parameter): internalexternal
  • Network core bootloader minimal size (-M)

Now you're ready to run the script.

  1. Copy the sample example from the SDK version directory to C:\A\s1. I used v2.4.0, so here is the directory where the code is: C:\ncs\v2.4.0\nrf\applications\nrf5340_audio
  2. After this is copied, EDIT the JSON config file nrf5340_audio_dk_devices.json  as described 
  3. To build the script go to the directory    cd C:/A/s1/tools/buildprog
    1. python buildprog.py -c both -b debug -d both -m internal –M
    1. TURN on BOTH BOARDS
    2. Enter in the following command:
  4. it starts to build with the following output.

image

But I ran into a fatal error with building zephyr FLASH OVERFLOW

image

Is it a gateway board? NO , because I Switched the boards in the JSON file and still the same flash error.

Is it the SDK version? No, because I tried another version and still no build. Tried an older SDK /c/ncs/v2.1.0-rc2, with fresh software the following error occurred and did not get as far as the other code.

image

Now I tried to run the script with different arguments I used the external DFU type and release instead of debug as described here:

python buildprog.py -c both -b release -d both -m external 

SUCCESS I WAS ABLE TO BUILD using the args -b release -m external  for the python script

HERE IS THE END OF THE COMMAND to PROVE IT. I also saved the whole log into a WORD doc.

image

PROGRAMMING 

Programming with the script

The development kits are programmed according to the serial numbers set in the JSON file. Make sure to connect the development kits to your PC using USB and turn them on using the POWER switch before you run the command.

The following parameters are available for programming:

  • Programming (-p parameter) – If you run the building script with this parameter, you can program one or both of the cores after building the files.

The command for programming can look as follows:

python buildprog.py -c both -b debug -d both -p

FIRST TRY

Since I built the code in RELEASE MODE I will use the –b release argument instead of debug

python buildprog.py -c both -b release -d both –p 

Received: buildprog.py: error: unrecognized arguments: –p   WHY? I have the –p

image

Tried what FRED27 discovered SEE below with underscores for arg –recover_on_fail

python buildprog.py -c both -b release -d both -p –recover_on_fail

But did not build with –p on the end so I tried putting the –p at the beginning and dropped the –recover_on_fail

python buildprog.py -p -c both -b release -d both

Results: went a little farther  but failed on 

input hex name C:\ncs\v2.4.0\nrf\lib\bin\bt_ll_acs_nrf53\bin\ble5-ctr-rpmsg_shifted_3349.hex

relative path

Traceback (most recent call last):

  File "buildprog.py", line 404, in <module>

    __main()

  File "buildprog.py", line 395, in __main

    __populate_hex_paths(dev, options)

  File "buildprog.py", line 194, in __populate_hex_paths

    raise Exception(

Exception: Found zero or multiple NET hex files in folder: C:\lib\bin\bt_ll_acs_nrf53\bin

`image

Is the hex file present? YES see the pic below?

image

image.py: sign the payload

input hex name C:\ncs\v2.4.0\nrf\lib\bin\bt_ll_acs_nrf53\bin\ble5-ctr-rpmsg_shifted_3349.hex       relative path 

But why then does the script log say the following location for the hex name? it exist?

And why does the exception give a directory that does not exist?

Exception: Found zero or multiple NET hex files in folder: C:\lib\bin\bt_ll_acs_nrf53\bin

SECOND TRY

So I created and copied the contents of C:\ncs\v2.4.0\nrf\lib\bin\bt_ll_acs_nrf53\bin to C:\lib\bin\bt_ll_acs_nrf53\bin as shown below

image

And voila it WORKED

 image

But I did get the error 

ERROR: your device. Please use --recover to unlock the device. As seen below?

image
Incorrect programming instructions

FRED27 experienced the following:

So now I’d successfully built the code, it needed to be flashed to the devices. I followed the instructions and used "python buildprog.py -c both -b debug -d both -p --recover-on-fail". This promptly failed with unrecognized option recover-on-fail. I tried reducing it to “-r” and my PC crashed. I tried leaving the option off and was told I needed the recover option. I tried –recover and something worked. Eventually I worked out that the option should have been --recover_on_fail (with underscores)

Another indication that the programming was unsuccessful was that the LEDS are not the same as Roadtester: Gough Lui? As described below

Once the firmware is correctly loaded on the boards, they will change from the yellow color (as shipped) to green (gateway), blue (headset-left) or magenta (headset-right).

image

THIRD TRY

Try another round to get the proper results without error.

  1. Copy code to s4
  2. Change JSON file to add device ides for gateway left devices.
  3. Go to cd C:/A/s4/tools/buildprog
  4. Turn on both devices and USB cables to PC
  5. 1 BUILD with Debug not Release
    1. python buildprog.py -c both -b debug -d both -m external 
  6. 2 PROGRAM with Debug not release
    1. python buildprog.py -p -c both -b debug -d both

NO GOOD cannot program net core on both devices? 

ERROR: Due to readback protection?
Here’s the end of the log

image

Here’s the section showing the error

[6/6] Running post-build ble5-ctr signing step...
0x00000001
image.py: sign the payload
input hex name C:\ncs\v2.4.0\nrf\lib\bin\bt_ll_acs_nrf53\bin\ble5-ctr-rpmsg_shifted_3349.hex
relative path
Using NET hex: C:\lib\bin\bt_ll_acs_nrf53\bin\ble5-ctr-rpmsg_3349.hex for 1050171701 headset left
Using NET hex: C:\lib\bin\bt_ll_acs_nrf53\bin\ble5-ctr-rpmsg_3349.hex for 1050131916 gateway
Programming net core on: 1050171701 headset left
Programming net core on: 1050131916 gateway
ERROR: The operation attempted is unavailable due to readback protection in
ERROR: your device. Please use --recover to unlock the device.
NOTE: For additional output, try running again with logging enabled (--log).
NOTE: Any generated log error messages will be displayed.
ERROR: The operation attempted is unavailable due to readback protection in
ERROR: your device. Please use --recover to unlock the device.
NOTE: For additional output, try running again with logging enabled (--log).
NOTE: Any generated log error messages will be displayed.
build_prog.py finished.  Report:
+-----------------+------------+-----------+-------------------+-------------------------------+------------------------------+

|    snr              | snr conn |  device | only reboot  | core app programmed | core net programmed |

+-----------------+-------------+-----------+------------------+-------------------------------+------------------------------+

| 1050171701 |   True     | headset | Not selected |        Selected TBD          |        Failed                      |

| 1050131916 |   True     | gateway| Not selected |        Selected TBD          |        Failed                      |

|     10               |  False     | headset | Not selected |        Not selected          |        Not selected          |

+---------        ---+--------  --+-------    --+---      -----------+------            ---------------+---            ------------------+

6/25/2023 –Update – Success with Building and Programming using the Python script.

After many trials and errors with both the BUILD and The Programmer arguments to the script, as mentioned above, I came up with the following to successfully Build & Program the two devices:

  1.  To Build use the command:
    1.  python buildprog.py -c both -b debug -d both -m external
    2. Results: the report showing a successful build
    3. image
    4. Note: I'm using "-m external" because '-m internal" did not work because the debug firmware was too big, I mentioned this above.
  2. To Program Use the command:
    1. python buildprog.py -c both -b debug -d both -p --recover_on_fail
    2. Results: the report showing that both the App and the net have been programmed to the boards.
    3. image
      Still get the use recover arg error in the output, even though I ran the command with “--recover_on_fail” ?
    4. NOTE: The App doc page is incorrect the program command has an incorrect argument “--recover-on-fail”! It should be defined with underscores not dashes.
      THIS NEEDS TO BE FIXED ON THE DOC PAGE TO STOP CONFUSION WHEN USING THE AUDIO EXAMPLE TO BUILD & PROGRAM the KIT

6/29/2023 –Update --Testing the default CIS mode

After building and programming the application, you can test it for the CIS mode. The following testing scenarios assume you are using USB as the audio source on the gateway. This is the default setting. After programming, RGB2 starts blinking green on every device to indicate the ongoing CPU activity on the network core. LED3 starts blinking green on every device to indicate the ongoing CPU activity on the application core.

After programming the above indicated LEDs are in question? They are not BLINKING or illuminating. And the board lights do not illuminate like describe by reviewer Gough.

I Posted a DEVZONE ticket. Ticket nRF5340 Audio DK with the audio application nrf5340_audio.. This ticket helped me figure out why the LEDs and the Board lights were not working on  Audio Gateway and Headset. Ticket was SOLVED June 28 and the above link details what I went through to solve it

Basically here are the steps I took to Build and Program the Audio Example on both devices.

  1. I rebooted my PC and started with a fresh directory (not sure why this helped but it did)
  2. changed the devices in the file nrf5340_audio_dk_devices.json as indicated in previous sections of this review.
  3. Build and Program using no -m internal -M on the build
    1. BUILD: python buildprog.py -c both -b debug -d both
    2. PROGRAM: python buildprog.py -c both -b debug -d both -p --recover_on_fail

This worked great The LEDS are working on the boards and they change colors to indicate the Gateway GREEN and Headset BLUE as shown

.

The audio example page in the testing section indicates that after programming,

  • RGB2 starts blinking green on every device to indicate the ongoing CPU activity on the network core.
  • LED3 starts blinking green on every device to indicate the ongoing CPU activity on the application core.
  • Wait for the LED1 on the gateway to start blinking blue. This happens shortly after programming the development kit and indicates that the gateway device is connected to at least one headset and ready to send data. 

They are different for me however

  1. The RGB2 never blinks and is not illuminated on both devices.
  2. LED3 is blinking YELLOW not GREEN on both devices
  3. The LED1 is blinking BLUE on the gateway and Left headset

The engineers at DevZone claim that this is a known issue and that it doesn’t affect anything.

I completed the following steps to test the unidirectional CIS mode for one gateway and a left headset.

  1. Make sure that the development kits are still plugged into the USB ports and are turned on.
  2. Note: Make sure to check the nRF5340 Audio application known issues related to serial connection with the USB.
  3. After programming, the LED3 starts blinking YELLOW ( NOTE: NOT GREEN as the Doc page indicates) on every device to indicate the ongoing CPU activity on the application core. Wait for the LED1 on the gateway to start blinking blue. This happens shortly after programming the development kit and indicates that the gateway device is connected to at least one headset and ready to send data.
  4. Search the list of audio devices listed in the sound settings of your operating system for nRF5340 USB Audio (gateway) and select it as the output device. On my PC (your OS might be different) go to settings/system/sound to set the sound output and set the output to “Headset Earphone (nRF5340 USB Audio)” as described.
    1. image
  5. Connect headphones to the HEADPHONE audio jack on both headset devices.
  6. Start audio playback on your PC from any source.
  7. Wait for LED1 to blink blue on both headsets. When they do, the audio stream has started on both headsets.
  8. Wait for LED2 to light up solid green on the headsets to indicate that the audio synchronization is achieved. NOTE: This never happened for me? But everything worked great for me.
  9. Press the VOL+ button on one of the headsets. The playback volume increases for both headsets.
  10. Press the VOL- button on the gateway. The playback volume decreases for both headsets.
  11. Press the PLAY/PAUSE button on any one of the headset. The playback stops for both headsets and the streaming state for all devices is set to paused. NOTE: I was unable to test this feature because I had only one headset.
  12. Press the RESET button on the gateway. The gateway resets and the playback on the un-paused headset stops. After some time, the gateway establishes the connection with both headsets and resumes the playback on the un-paused headset.
  13. Press the PLAY/PAUSE button on any one of the devices. The playback resumes in both headsets. NOTE: I was unable to test this feature because I had only one headset.
  14. Press the BTN 4 button on the gateway multiple times. For each button press, the audio stream playback is stopped and the gateway sends a test tone to both headsets. These tones can be used as audio cues to check the synchronization of the headsets.
  15. NOTE: I was unable to get this to work, maybe because I have only one headset.
    1. Hold down the VOL+ button and press the RESET button on the left headset. After startup, this headset will be configured as the right channel headset.
    2. Hold down the VOL- button and press the RESET button on the left headset. After startup, this headset will go back to be configured as the left channel headset. You can also just press the RESET button to restore the original programmed settings.

After the kits have paired for the first time, they are now bonded. This means the Long-Term Key (LTK) is stored on each side, and that the kits will only connect to each other unless the bonding information is cleared. To clear the bonding information, press and hold BTN 5 during boot.

When you finish testing, power off the nRF5340 Audio development kits by switching the power switch from On to Off.

 

RESULTS of the TEST

Seeking Improvements:

I was given, an insightful comment from Uzer123 offered a potential solution using environment variables in the terminal or utilizing the terminal created by the Toolchain Manager. Incorporating this valuable information into the documentation can save users from unnecessary troubleshooting.

The Documentation is sometimes giving invalid script information(like dashes instead of underscores, improper argument placement etc.) For this reason I’m lowering my ratings for documentation in this review.

The page should include the supported SDK versions to use. It should have a release date and an indication of updates to the documentation.

The building and programming sections need to be improved with solutions that work with the supported SDK version.

Conclusion:

In conclusion, the building and programming process for the Nordic nRF5340 Audio DK example application presents challenges due to limitations with VSCode support and the complexities encountered in both the command line and Python script approaches. To improve the user experience, it is crucial to provide clear instructions, address limitations with supported IDEs, and streamline the build process, especially with the Python script option. Incorporating the discovered solutions and enhancing troubleshooting guidance will significantly reduce frustration and enable a smoother building experience for developers relying on the provided documentation.

RANKINGS

I raised my my rankings due to the DEVZONE support I received with the build and programming issues of the Audio example page.

  • Product Performed to Expectations -- 3 stars
    • I never was able to test the board using the audio example, due to errors in firmware programming using python script.The other examples worked fine.
  • Specifications were sufficient to design with -- 3 stars
    • I followed the starting guide and the nRF5340 DK SDK Documentation.
  • usage Demo Software was of good quality -- 4 stars
    • Example code is very well documented, but contained improper instructions to get the Example app working. Very frustrating for me.
    • Code exist for all the audio capabilities of the nRF5340 DK
  • Product was easy to use -- 3 stars
    • It was as easy as expected, but not the Audio example which I was unable to get Programmed
  • Support materials were available -- 4 stars
    • Not for the problems I was having
  • The price to performance ratio was good. -- 3 stars
    • The price is a little high if you intend to purchase 3 boards which are needed to run the example with a gateway and stereo (left, right) channels 

Nordic nRF5340 Audio DK reviews from other members, is another excellent resource and are very informative on the usage of the kit

  1. A review by   Nordic Semiconductor nRF5340 Bluetooth Low-Energy Audio Development Kit RoadTest Review
  2. A review by   Nordic nRF5340 Audio Development Kit review
Anonymous
  • UPDATE

    Hello element14 members.

    I finally was able to successfully build and program the audio example so I could start testing. The previous update programmed the 2 kits but the lights were not blinking?

    if your interested, check out the section titled "6/29/2023 –Update --Testing the default CIS mode"

    In this section I describe how I tested the 2 audio kits. One is a GATEWAY and the other is the LEFT HEADSET..

    Let me know what you think?

    Regards 

    Steve K

  • UPDATE

    After many trials and errors with both the BUILD and The Programmer arguments to the script, I came up with the following to successfully Build & Program the two devices:

    If your interested look for the 6/25/2023 –Update – Success with Building and Programming using the Python script Section in my review.

  • Hello everyone,

    If you are following my review on the Nordic nRF5340 Audio DK, I just updated it and brought the rankings down to a total of 2 1/2 stars. f have been trying for weeks to get the Audio example Built and Programmed onto the 2 boards that were supplied to me. I am very frustrated with the Audio example documentation. I was eventually able yo build the example but unable to program the kits with the example application. Due to this I have not been able to TEST the application with the given instructions.

    In conclusion, the building and programming process for the Nordic nRF5340 Audio DK example application presents challenges due to limitations with VSCode support and the complexities encountered in both the command line and Python script approaches. To improve the user experience, it is crucial to provide clear instructions, address limitations with supported IDEs, and streamline the build process, especially with the Python script option. Incorporating the discovered solutions and enhancing troubleshooting guidance will significantly reduce frustration and enable a smoother building experience for developers relying on the provided documentation.

    I will continue to seek help from DevZone and try to resolve any remaining issue with programming the kits to be able to start testing the Audio example. It shouldn't be this hard to program the application, I know that it is a complex piece of software but other Nordic DK's,  I have experience with, were not as troublesome as this one. .So sorry for the Rant. I hope I can get to Testing the application soon. If anyone in the community can shed some light on what I'm doing wrong, it would be appreciated.

    This application example is not easy.

    Thanks

    SteveK

  • This concludes my review of the Nordic nRF5340 Audio DK. I would like to thank Nordic Semiconductor for the opportunity to experiment with this kit and I'll be using the Kits to experiment further with audio . 

    Regards Steve K

  • Wow thanks for the comment mp2100.

    NORDIC does a good job with there Development kits. The nRFConnect-SDK and other toolchains, take a little learning curve, but once mastered, it gets easier to develop firmware with

    I'm in a cover band that plays Bars and Events.. I do it for fun and relaxation along with embedded system experimenting.

    Thanks 

    SteveK

  • Even if it is draft form, the comments are interesting to read. Looking forward to what you learn. Let’s hear some drumming!

  • thanks for responding

     

    I know , this is an easy mistake and different from the other blogs on element 14.
    It’s a pain at this point to save all the content to another editor bringing over the images, and delete the published blog and start over. 
    That is why I commented on it , but I’ll put the disclaimer at the top as you suggested. And rate the review.  I’m updating from my notes and editing as I go.
  • Hi,

    Good starting though. I have had the same issue some time ago regarding editing and saving the roadtest. But then I started using Libre office and then paste everything to the roadtest. That worked for me but font editing was required along with image inserting.

    One more question...

    Your scoring seems very low? Is it by mistake or are you going to edit it?

    Thanks,

    Ujjval

  • I am no where near finishing this review now , but it was published by mistake and there is no way to save it as DRAFT once published???

    I will continue to work on this review.