RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Polls Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 14 Aug 2020 9:36 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 6037 views
  • Likes 2 likes
  • Comments 47 comments
Related
Recommended

Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?

I will be roadtesting the Eaton easyE4 Nano Programmable Logic Controller in the very near future. If you haven't heard about it, let me tell you a few facts:

 

The easyE4 nano programmable logic controllers combine timers, relays, counters, special functions, inputs and outputs into a compact device that is easily programmed. It provides an

exceptional level of flexibility together with a substantial savings of commissioning time and effort. The easyE4 is available in six styles with 12 I/O that can be expanded to 188 I/O points, which provides the ideal solution for material handling, HVAC, pump control, irrigation, lighting, energy management, industrial control, and home automation. The easyE4 nano programmable logic controller excels in traditional applications where multiple relays, timers and pushbuttons are used.

 

For the purpose of ordering the roadtest units, a question arose about the input voltage while discussing the roadtest with Eaton. The two types I am considering is 24VDC or 110-220VAC. While both versions are available, and I could get both, I just wanted to get a sense what would be a roadtester's preference. This is more a logistics question than a tech question. Both versions have the same functionality.

 

Here's the 24VDC version

 

**Image is updated***

 

easyE4 Nano Programmable Logic Controllers 24vdc

**** Datasheet is updated**** Datasheet EASY-E4-UC-12RC1

 

 

Here's the 110-220VAC version

 

easyE4 Nano Programmable Logic Controllers 110-220VAc

Datasheet

 

Poll question: Which version do you prefer AC or DC?

  • scasny
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 6 years ago +6
    I will ask about the EasySoft7 software. But it seems there is a desire for both AC and DC. I will ask for both. I'll ask for these two models: Easy-E4-UC-12RC1 and Easy-E4-AC-12RC1 Randall --element1…
  • michaelkellett
    michaelkellett over 6 years ago +5
    Definitely DC, kind of places you use these devices often have limited access and very frequently need live commissioning and/or debugging. A 24V DC based solution may cost a little more (needs more 24V…
  • cghaba
    cghaba over 6 years ago in reply to hugohu +5
    When you talk about programming PLCs you talk about programmming in Ladder Diagrams, Instruction List, Structrued Text, Function Blocks languages. For this PLC it is used the Ladder Diagram language.
  • mstewart197930
    mstewart197930 over 6 years ago

    24v is the industry standard and what we use for the Rockwell ones at work, whereas the 220-240v one would be more ideal for home users, as it doesnt involves extra costs.

    but personally 24v.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rikv
    rikv over 6 years ago

    24Vdc is standard I/O voltage in industry. Furthermore any expansion modules with solid state outputs will not be compatible with the 220V main module.

    On the other hand, these devices are widely used in fi greenhouse climatisation and so forth. In this world 220Vac is the norm: control valves, relays... all are 220V (bizarre since water is omnipresent).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to rscasny

    Great!

     

    I'm fine with both but if I get the DC one it will just be an excuse to get a PSU, something I've been holding off for quite a bit.

     

    I think the analog modules might be useful in the future but I can't think of anything to do with them so if I need it, I'll get it myself.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 6 years ago in reply to rscasny

    Hi Randall rscasny  ,

    https://www.element14.com/community/servlet/JiveServlet/showImage/105-263779-914912/easy4.JPG

    There is a mistake in the table, the dash under "features/display" ist wrong for the base unit EASY-E4-UC-12RC1.

     

    easy-E4 - .C - .. ... - x1(P)

    AC, DC, UC - Power rating Type of supply voltage

    12 - Number of inputs/outputs (8in, 4out)

    Type of output: R-Relay T-Transistor A-Analog P-Temperature

    E - Expansion

    CX - Base device with LED diagnostics

    C - Base device with display and buttons

    1- Version

    P- Type with push in connection instead of with screw terminal connection.

     

    !!! Please look for the actual firmware version because some functions of the user software can be used just with the lastest firmware version.

    - > V1.2 or newer (if I remember V1.3 is actual ???).

     

    ( user manual, page 13)

    11/2018 New edition

    11/2018 V1.1

    Real-time clock characteristic curve Sample program Cat No. MEMORY-SUD-A1

    1/2019 V1.2

    ff Corrections

    2/2019 Added models EASY-E4- AC-... and EASY-E4-DC-4PE1; added AC, AV, PM, and RE function blocks

    4/2019 Webserver, E-Mail function, time response, micro SD card

    10/2019 ff Device versions with push in terminals,EASY-E4-AC (cULus)

     

    The SD-Card slot is for the user programmed software. Here can be inserted a micro SD card.

    (Programming languages: Ladder diagram (LD), Function Block Diagram (FBD), Structured Text (ST), and easy Device Programming (EDP) on device and in easySoft 7)

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago

    I am going to ask the sponsor for:

     

    Easy-E4-UC-12RC1 (quantity 3)

     

    and

     

    Easy-E4-AC-12RC1 (quantity 2)

     

    This is the basic. If anyone wanted to get the analog modules (Gerald mentioned) they would need to mention it in the roadtest application and I would ask the sponsor.

     

    Randall

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago in reply to mp2100

    I am not sure what that dash means because the datasheets and Eaton's website says it comes with a display.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago in reply to mp2100

    I checked again.

     

    I went to Eaton's site. And I looked at the datasheet's again, just as Cristian-Gyobo did. Both come with a display.

     

    Now, it looks like it comes with a slot for an SD card. So, you will get the software for programming.

     

     

     

    https://www.farnell.com/datasheets/2906081.pdf?_ga=2.36104099.2008925075.1597260425-982436643.1585328086&_gac=1.21732829…

     

    https://www.farnell.com/datasheets/2906081.pdf?_ga=2.36104099.2008925075.1597260425-982436643.1585328086&_gac=1.21732829…

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to rscasny

    That's great.

     

    Does the DC version come with the screen and keypad or not?

     

    Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago

    I took the day off on Friday, so I am just catching up on my email.

     

    But the sponsor, Eaton, told me the software comes with the product.

     

    Randall

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cghaba
    cghaba over 6 years ago in reply to mp2100

    In the user guide for both models is specified "Base device with display". You can also see on the parts (PN: 197211 and PN:127215) webpages:

    https://datasheet.eaton.com/datasheet.php?model=197211&locale=en_GB&_lt=

    and 

    https://datasheet.eaton.com/datasheet.php?model=197215&locale=en_GB&_lt=

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>