RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Polls Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 14 Aug 2020 9:36 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 6037 views
  • Likes 2 likes
  • Comments 47 comments
Related
Recommended

Roadtesting the easyE4 Nano PLC: AC or DC, What's Your Preference?

I will be roadtesting the Eaton easyE4 Nano Programmable Logic Controller in the very near future. If you haven't heard about it, let me tell you a few facts:

 

The easyE4 nano programmable logic controllers combine timers, relays, counters, special functions, inputs and outputs into a compact device that is easily programmed. It provides an

exceptional level of flexibility together with a substantial savings of commissioning time and effort. The easyE4 is available in six styles with 12 I/O that can be expanded to 188 I/O points, which provides the ideal solution for material handling, HVAC, pump control, irrigation, lighting, energy management, industrial control, and home automation. The easyE4 nano programmable logic controller excels in traditional applications where multiple relays, timers and pushbuttons are used.

 

For the purpose of ordering the roadtest units, a question arose about the input voltage while discussing the roadtest with Eaton. The two types I am considering is 24VDC or 110-220VAC. While both versions are available, and I could get both, I just wanted to get a sense what would be a roadtester's preference. This is more a logistics question than a tech question. Both versions have the same functionality.

 

Here's the 24VDC version

 

**Image is updated***

 

easyE4 Nano Programmable Logic Controllers 24vdc

**** Datasheet is updated**** Datasheet EASY-E4-UC-12RC1

 

 

Here's the 110-220VAC version

 

easyE4 Nano Programmable Logic Controllers 110-220VAc

Datasheet

 

Poll question: Which version do you prefer AC or DC?

  • scasny
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 6 years ago +6
    I will ask about the EasySoft7 software. But it seems there is a desire for both AC and DC. I will ask for both. I'll ask for these two models: Easy-E4-UC-12RC1 and Easy-E4-AC-12RC1 Randall --element1…
  • michaelkellett
    michaelkellett over 6 years ago +5
    Definitely DC, kind of places you use these devices often have limited access and very frequently need live commissioning and/or debugging. A 24V DC based solution may cost a little more (needs more 24V…
  • cghaba
    cghaba over 6 years ago in reply to hugohu +5
    When you talk about programming PLCs you talk about programmming in Ladder Diagrams, Instruction List, Structrued Text, Function Blocks languages. For this PLC it is used the Ladder Diagram language.
  • hugohu
    hugohu over 6 years ago in reply to rscasny

    I am probably interested but I'm on page 80 of the manual and still trying to figure out exactly what this thing does.

     

    So, it's basically a bunch of programmable relays with HMI?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to gpolder

    Interesting indeed.

     

    I'd tend to say that hobbyists have access to bench power supplies, so 24V is no biggie, but if its commercial Unless if you want a 24V AC-DC cable?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gpolder
    gpolder over 6 years ago in reply to hugohu

    I'm thinking completely opposite, 24V for industrial applications, AC for hobbyists and Roadtesting.

     

    No idea how many cents my opinion counts for.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to Gough Lui

    EasySoft7 is probably (97% chance) NOT included. It mentions that the demo is a limited version of the actual paid version. Yes, I'm combing through the 800 page manual.

     

    Since you have experience with EasySoft what programming language does it use? C/C++? Python? ST?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to Gough Lui

    I'm starting to think that 24V is better for hobbyists and Roadtesting, but for commercial applications it is more to buy a power supply and a 24V version, so in those cases AC is used.

     

    Just my two cents.

     

    If that's what two cents means.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago in reply to cghaba

    Indeed it can - I didn't think about that ... although with the matrix LCD, it won't be comfortable if you've got a lot of rungs ... definitely something I'd like to try as well.

     

    I previously had a play with the Eaton SmartWire DT as part of a "grab bag" RoadTest - no LCD on that one, so everything was done using easySoft-Pro 6 which was quite an experience in itself, having never really used a PLC before. The problem I ran into was the SmartWire-DT system being pretty much "orphaned" without much in the way of compatible wiring or peripherals available locally to extend on the provided bits which consisted of two 3ph contactors and two push-buttons. I liked the experience ... and I think it'll definitely be interesting to devise something using an "all in one" unit with connectivity for expansion.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cghaba
    cghaba over 6 years ago in reply to rscasny

    Maybe you can ask 3 pieces of DC type and 3 of AC type. Then, we could have the roadtest experience from the two worlds.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cghaba
    cghaba over 6 years ago in reply to Gough Lui

    This type of PLCs can be programmed using only the HMI (LCD and buttons). Of course, using easySoft is much more easy to program it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago in reply to rscasny

    I'm definitely interested - just wondering, will it come bundled with a license for easySoft 7 which is needed to program it or is it going to be just the unit?

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 6 years ago

    AC or DC is totally depends on final application.

    Normally PLC is largely applied in factory and stores, such as brand Siemenz or Omron.Then 24V DC is only choice. 24V DC is not simply stacked by batteries but from UPS with battery banks.

    But this Eaton version is different and creative. It is compact in size and reasonable in price, I guess, in compare with Siemenz PLCs. It can replace more non-standard application  and even for home-automation, of which complex DC power supply system can be removed at the cost of lower power source reliablility.

    I suggest several110-220V PLC be tested as well, according to the vendor's target market.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>