I am trying to create a through hole part( a simple SPST tactile switch) and when I go to device and try and connect the symbol to the package I see the yellow ! and when I double click on it I get no pins just pads. So why do I not see pins? I have the…
I basically want to receive a arbitrary string of approximately 80 characters through usart of microcontroller, but I could not succeed accordingly.Pseudo code for my project is as below #include<avr/io.h> #include<util/delay.h> unsigned char USART_receive…
I'm making a two layer board for the first time, and have come across a question regarding component placement. Say for example I have a through hole DC-DC converter. This converter has four pins and will be placed on the top of the board, therefore the…
IEC Gerätestecker mit Netzschalter Die Energieeffizienz wird beim Design elektronischer Geräte immer wichtiger. Aus diesem Grund gibt es viele Bestrebungen zur Reduktion des Standby-Verbrauchs. Die konsequente Realisierung zeigt sich in der sicheren Netztrennung…
NASA has created augmented reality goggles which could soon be available to airline pilots and help them 'see' through fog. The goggles can track a pilot's head-movements and overlay runways, towers and potentially other airplanes over their view - an…
How do I get this to display messages, text, etc; through GPIO? I have seen others do it before but they never state or tell how they do it. I want to know if this is possible to do and how difficult it is to get the software for it. This is my screen…
Hi Thanks in Advance Am using Rapsberry Pi2 with Raspbian Debian Wheezy OS, configured the network as static with my LAN Connection and accessing pi2 by Putty. I tried to ping google.com, am getting the following response pi@raspberrypi ~ $ ping google…