3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Recommendation for a kit to build my first 3d printer.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 346 subscribers
  • Views 2101 views
  • Users 0 members are here
Related

Recommendation for a kit to build my first 3d printer.

majorkuso
majorkuso over 11 years ago

I would like some recommendations on a kit so I can build a 3d printer. would it be possible to build one with similar resolution as the robox? I was looking into the reprap prusa i3 models.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Workshopshed +3
    Or even much more complex objects like this Most of the parts for the Thorn gun from the game Destiny and as you say, it sucks when it fails part through
  • bobthechemist
    bobthechemist over 11 years ago +2
    Hi, Looks like I'm late to the party, but I thought I'd chime in. I purchased a makerfarm i3v 8" model at the beginning of the summer. I went with a kit primarily for the opportunity to build something…
  • Workshopshed
    Workshopshed over 11 years ago +1
    Hi James, I don't have any specific recommendations but some thoughts on the factors to consider. I think there are 4 key reasons to want to build a kit you enjoy building stuff you can learn more about…
Parents
  • majorkuso
    majorkuso over 11 years ago

    I appreciate the feedback, i am looking into a good sized build area any idea about this printer? or one of these two one, two? the printrbot seems rather small, is 4x4x5 sufficient? I realize that depends on my project but does anyone know the average size of objects printed? if I choose a larger build area can I print multiple objects in sequence on the larger platform, object a gets done thenthe head moves to other side then prints b, c etc  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • majorkuso
    majorkuso over 11 years ago

    I appreciate the feedback, i am looking into a good sized build area any idea about this printer? or one of these two one, two? the printrbot seems rather small, is 4x4x5 sufficient? I realize that depends on my project but does anyone know the average size of objects printed? if I choose a larger build area can I print multiple objects in sequence on the larger platform, object a gets done thenthe head moves to other side then prints b, c etc  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • celrobox
    celrobox over 11 years ago in reply to majorkuso

    Hi James,

     

    When considering build volume, its worth noting that the larger you go with your parts, the more prone they are to failure, and the larger the part, the more material is lost if a print fails. The Designer of the CEL Robox Chris Elseworthy has written a blog on Size and 3D printing you can find it here; http://www.cel-robox.com/bigger-really-better/

     

    Now of course I am going to be bias towards the Robox, but I have to ask, what is your reasoning for looking at kit printers rather than a pre built unit? Is it because you wish to have the experience of building it, which is probably the best (and in my opinion the only) reason to build from a kit, or to save money? I have built several kit printers myself and found the process very enjoyable, but I am now very glad to have an easy to maintain Robox by my side.

     

    Cheers,

    Simon

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to majorkuso

    >if I choose a larger build area can I print multiple objects in sequence on the larger platform

    No, you can't as the print head would likely knock the other items off the bed.

     

    However, you can print several things in parallel and potentially save time. However if you have to abandon the print because of an issue then you could loose the lot. Here's an example where I printed a batch of thumbwheels at the same time.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Workshopshed

    Or even much more complex objects like this

    image

    Most of the parts for the Thorn gun from the game Destiny and as you say, it sucks when it fails part through

    • Cancel
    • Vote Up +3 Vote Down