3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Building a 3D printer out of Hp G85 Office jet printers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 341 subscribers
  • Views 2878 views
  • Users 0 members are here
Related

Building a 3D printer out of Hp G85 Office jet printers

e14 Contributor
e14 Contributor over 12 years ago

Hello there my friends... so i saw these 3D printer things... and i thought it would be cool to try to make one... now i have no background with Arduino at all... but i do have a little bit of knowlege when it comes to CNC's... see my father purchased 6 of these Hp G85 office jets this was a loooong time ago at least 12 years ago recently the last of them died and was replaced with a newer inkjet...

and so with the permission of my father i started disassembling one of these printers to see if they could be of use...

 

parts of notable significance

 

steppers 2 steppers per printer... both have encoders not sure if they are useful to me though

rails there are 2 rails per printer aswell

belts two belts per printer and gears/ sprockets to go with the belts...

cold cathode light (from the scanner) useful for other projects and possibly for built in lighting on the 3d printer...

Glass plate from the scanner

various springs and stuff

 

that seems to be it

 

so my question is could i use 2-3 of these printers to build a 3d printer

will the steppers be adequate?

if not what steppers are recommended?

where can i find a mc-mega dev board and a RAMPS Sheild?

 

my goal design is to build one similar to the portable one ben heck built... although mine wont be portable...

 

any information you have to share with me would be greatly appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    That sounds like a Cartesian-format layout (take a look at the Mendel or Prusa i3) and definitely the Arduino MEGA + RAMPS is a good way to go. Most of the other common boards (RAMBO, etc) are just combined…
Parents
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago

    Springs could be used on the bed for tension, the steppers can be used to drive the axis' and the belt could be used in conjunction to move them.

    Very nice idea on the subject of recycling electronics, good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to hawkeyethehacker

    thats what i was thinking with the steppers... although one is larger than the other as one was use to move the print head and ink carts... while the other was only used to move the scan bar....im not sure about using springs on the bed because im going to have the bed move along the x axis and let the hot end take care of y and z

     

    Thanks for the reply Josh i appreciate the advice!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to hawkeyethehacker

    thats what i was thinking with the steppers... although one is larger than the other as one was use to move the print head and ink carts... while the other was only used to move the scan bar....im not sure about using springs on the bed because im going to have the bed move along the x axis and let the hot end take care of y and z

     

    Thanks for the reply Josh i appreciate the advice!