3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Prusa Mendel Iteration 2 Stepper Motor Z Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 342 subscribers
  • Views 2770 views
  • Users 0 members are here
  • mendel
  • printer
  • 3d
  • issue
  • issues
  • 2
  • iteration
  • stepper
  • prusa
  • motor
  • z
Related

Prusa Mendel Iteration 2 Stepper Motor Z Issues

e14 Contributor
e14 Contributor over 12 years ago

     So I bought all the components I need to make a PMI2 and put it all together, being sure to measure multiple times so it can be accurate as possible. The only issues Ive had are the electronics, mainly the stepper motors. They're have some slight binding issues which are really apparent on the Z axis. I check all the angles that have to do with it and they are really accurate. I also have the rods lubricated and adjusted the power output to max for the stepper motors. The thing is I don't think that the Z motors are receiving enough power, considering that they are connected together. I've had it sitting for a few months now and I have yet to print anything.

 

     If anyone has a PMI2 or know how I can fix the issue that would be a lot of help. Thanks for taking your time to read this. image

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 12 years ago

    Running two motors in parallel is going to double your power requirements and stored energy.  What are the ratings of your drivers and motors, including coil resistance?  Do you have an oscilloscope?  Does it record?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 12 years ago

    Running two motors in parallel is going to double your power requirements and stored energy.  What are the ratings of your drivers and motors, including coil resistance?  Do you have an oscilloscope?  Does it record?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey

    Here's the stepper motors i have currently

     

    Displaying 20140617_122822.jpg

     

    and the specs with it 

                                          

    Shaft: 5mm diameter with flat
    Current Per Phase: 1.5A
    Holding Torque: 5.5Kg.cm (76 oz-in)
    Rated Voltage: 4.2V
    NO.of Phase: 2
    Step Angle: 1.8° ± 5%
    Resistance Per Phase: 2.8Ω± 10%
    Inductance Per Phase: 4.8mH± 20%
    Insulation Class: Class B
    Dielectric Strength: 100Mohm
    Operation Temp Range: -20 ~ +40° C
    Lead Wire: 22AWG / 750mm with connector to stepper motor driver

     

    As for the drivers i want to say its a ramps 1.4 for an arduino mega, here's a picture

    Found the kit i bought: SainSmart MEGA2560 A4988 Ramps 1 4 3D Printer Kit for Arduino RepRap | eBay

    image

    I'm also changing the couplers from the 3d printed to the metal ones and changing my stop switches to mechanical ones

    I don't have an oscilloscope but I do have a multimeter

    Also here's my power supply ratings