3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Prusa Mendel Iteration 2 Stepper Motor Z Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 342 subscribers
  • Views 2782 views
  • Users 0 members are here
  • mendel
  • printer
  • 3d
  • issue
  • issues
  • 2
  • iteration
  • stepper
  • prusa
  • motor
  • z
Related

Prusa Mendel Iteration 2 Stepper Motor Z Issues

e14 Contributor
e14 Contributor over 12 years ago

     So I bought all the components I need to make a PMI2 and put it all together, being sure to measure multiple times so it can be accurate as possible. The only issues Ive had are the electronics, mainly the stepper motors. They're have some slight binding issues which are really apparent on the Z axis. I check all the angles that have to do with it and they are really accurate. I also have the rods lubricated and adjusted the power output to max for the stepper motors. The thing is I don't think that the Z motors are receiving enough power, considering that they are connected together. I've had it sitting for a few months now and I have yet to print anything.

 

     If anyone has a PMI2 or know how I can fix the issue that would be a lot of help. Thanks for taking your time to read this. image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I would check to make sure the steppers are wired the same way (even in batches from the same manufacturer, you can find occasional variations), then try applying power to one motor and then its mate - watch for rotational phase or micro-stepping conflicts between each. Binding can definitely be an issue if overly constrained (both ends, etc) when using metal bushings or thrust bearings. You can test by loosening the bearing and allowing it to float while testing the motor. You can also apply small heat sinks to the A4988 chips to help dissipate heat if it starts to work and then stops - thermal failure can be tricky to identify sometimes.

     

    Kirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    I would check to make sure the steppers are wired the same way (even in batches from the same manufacturer, you can find occasional variations), then try applying power to one motor and then its mate - watch for rotational phase or micro-stepping conflicts between each. Binding can definitely be an issue if overly constrained (both ends, etc) when using metal bushings or thrust bearings. You can test by loosening the bearing and allowing it to float while testing the motor. You can also apply small heat sinks to the A4988 chips to help dissipate heat if it starts to work and then stops - thermal failure can be tricky to identify sometimes.

     

    Kirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    So it turns out it was the settings that the software comes with. I have it set to this

    image

    It seems off but it was working.

    the only issue right now is this

    image

    and the temperature was reading something like 375 but I think it was a wiring short. I'll just have to reorder the parts and insulate it better