3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Prusa Mendel Iteration 2 Stepper Motor Z Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 342 subscribers
  • Views 2782 views
  • Users 0 members are here
  • mendel
  • printer
  • 3d
  • issue
  • issues
  • 2
  • iteration
  • stepper
  • prusa
  • motor
  • z
Related

Prusa Mendel Iteration 2 Stepper Motor Z Issues

e14 Contributor
e14 Contributor over 12 years ago

     So I bought all the components I need to make a PMI2 and put it all together, being sure to measure multiple times so it can be accurate as possible. The only issues Ive had are the electronics, mainly the stepper motors. They're have some slight binding issues which are really apparent on the Z axis. I check all the angles that have to do with it and they are really accurate. I also have the rods lubricated and adjusted the power output to max for the stepper motors. The thing is I don't think that the Z motors are receiving enough power, considering that they are connected together. I've had it sitting for a few months now and I have yet to print anything.

 

     If anyone has a PMI2 or know how I can fix the issue that would be a lot of help. Thanks for taking your time to read this. image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    You seem to have covered the basics as far as drive current.

     

    You need to make sure that your Z axis moves smoothly. Both the smooth rod AND the threaded rod should be lubricated.  If you have a design that has a spring loaded pair of nuts on the Z drive, make sure the spring isn't overloaded, it should only have a few ounces of pressure.

     

    Also, on the motors, you should be using coils with no more than 3.6 ohms of resistance per winding.  1.8 ohm windings are better.  I once got some steppers with 8 or 10 ohm windings for a printer build and the motors were weak as kittens, I had to toss them.

     

    Oh, also, make sure you're not trying to step too fast.  Turn it down to 1mm per second max speed as a trial.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    You seem to have covered the basics as far as drive current.

     

    You need to make sure that your Z axis moves smoothly. Both the smooth rod AND the threaded rod should be lubricated.  If you have a design that has a spring loaded pair of nuts on the Z drive, make sure the spring isn't overloaded, it should only have a few ounces of pressure.

     

    Also, on the motors, you should be using coils with no more than 3.6 ohms of resistance per winding.  1.8 ohm windings are better.  I once got some steppers with 8 or 10 ohm windings for a printer build and the motors were weak as kittens, I had to toss them.

     

    Oh, also, make sure you're not trying to step too fast.  Turn it down to 1mm per second max speed as a trial.