3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum PrintrBot Simple Maker's Edition (Help)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 341 subscribers
  • Views 804 views
  • Users 0 members are here
  • help
  • printrbot
Related

PrintrBot Simple Maker's Edition (Help)

e14 Contributor
e14 Contributor over 11 years ago

I have had the PrintrBot Simple for two months now.

 

I started out printing small cubes and little models like a tardis. I have had trouble aligning the z-axis and have set the probe height several times. I have had little difficulty so far.

 

Last weekend when I tried to print a model, the z-probe started acting strange. I go to home the z-axis and the z motor raises the hotend and keeps raising the hotend again and stops. This puts the hotend about an inch off the bed and it thinks this is level.

 

I cannot lower the hotend manually and the z-home keeps getting higher and higher. HELP!

 

I have already tried flashing the board with the new firmware about 3 times. I already tried cleaning the z-probe and unplugging it. The only thing I can think of when it started is when I tried to print a model with a different computer. I cannot print anything.

 

What should I do next?

  • Sign in to reply
  • Cancel
  • bradnorwood
    bradnorwood over 11 years ago

    Did you build yours or was it assembled? The reason I ask is that you may need to reverse the motor in repetier it can be done or manually by the wire.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bradnorwood
    bradnorwood over 11 years ago in reply to bradnorwood

    Are you in the states? I might can help over the phone, I'm in NC, USA. I have had a simple kit over 2 years, I'm good at printing with it and maybe able to give you support. Brad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bradnorwood

    I assembled it. The motor worked fine for a month and a half. I made sure to put the plug back in the right orientation. When I use manual control I can make the z-axis raise up normally.

     

    I am from the states. I live in TN.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bradnorwood
    bradnorwood over 11 years ago in reply to e14 Contributor

    My cell is 704-999-8277. That's crazy, cause I've seen my software glitchy but not that off. Are you using repetier? and slic3r? I've had to reboot my pc, uplug and re plug to clear out glitches before. I actually hand turn z axis to get my desired starting point, I use a sheet of paper folded over as the thickness gauge, slic3r lets you play with the height also -1mm to + 2mm, I can look up the section name if you can't find it.