3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Hi Im having a misalignment in the x-axis on my makerbot replicator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 342 subscribers
  • Views 2955 views
  • Users 0 members are here
  • 3d-printings
  • 3D Printing
  • 3d_printer
Related

Hi Im having a misalignment in the x-axis on my makerbot replicator

e14 Contributor
e14 Contributor over 10 years ago

Hi I'm having some troubles with the alignment in the x-axis

i tried:

swamping axis motors -Same result

checked the heat bed level -Same result

Reset factory settings -Same result

 

and also checked axis belt and it looks fine with good tension (but I never changed and I have my printer for almost 2 years)

(and Im just ordered a new belt)

 

do you have any thoughts on the problem?

Also I attached some pictures of the model and the result

 

thanks for the help

Attachments:
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Nate1616 +1
    Hi there I just made and change the motor cable and it worked very fine thanks for the help
  • michaelwylie
    0 michaelwylie over 10 years ago

    One of the 3D printers where I use to work had this problem. It turned out to be a combination of a loose belt and a bad cable going to one of the motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 10 years ago

    Michael has some great points.  I would also check your acceleration.  To fast will also cause misalignment.  It seems like the shift is consistent in one direction which would make me think there is some printer alignment issue.   Check to see that all the axis are square and that the grub screws on the pulleys are tight.  Do all the axis move freely and without a bind point.  When you swapped the motors did the shift go in the opposite direction?  Did this start to occur after a software or firmware update?  Does the electronics get hot?

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Nate1616

    Hi Thanks for helping me
    I just change the x axis belt and the thing keeps doing the same

    being honest I didn't remember when it started to fail

     

    i remember that it has problems with the limit switch in the x-axis that causes a loud cranking sound when the belt hops the pulley (so I change the cable) but i didnt notice an alignment issue in small prints (1in x 1in)
    and also at first y was using replicator G and then moved to maker ware

     

    the electronics have proper heat sink so them dont heat excessively

     

    and even if the model is rotated the alignment issue stays in the x-axis (at first I was thinking that it seems as an accumulative error because there is no gaps)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 10 years ago in reply to e14 Contributor

    Since you know there was an issue with the x-axis switch have you checked to see if its triggered or never triggered at all?  This would cause issues with prints.  I see you said you swapped the motors did you also swap the stepper drivers?  Have you tried adjusting the current on the steppers?  Like i said since it seems to not follow anything at this time we can conclude its the x-axis components causing the issue.  You dont see it in small prints just for the fact the error isnt high enough to show up.  I would assume if a larger object is printed the misalignment would be greater.  Have you checked to make sure the x-axis moves freely?

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    @zion_taron

    Maybe this can help: http://download.makerbot.com/replicator2x/MakerBot_Replicator_2X_Troubleshooting___Maintenance.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    thanks for the advice image

    but that's the first thing I did when the problem happens

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Nate1616

    I see you said you swapped the motors did you also swap the stepper drivers?

    Yes - and the misalignment keeps in X axis

     

    Have you tried adjusting the current on the steppers?

    I don't know how to check it, but I presume that is in default setting

     

    Have you checked to make sure the x-axis moves freely?

    Yes - the cart can jog all the way through X axis

     

    I just change the belt with no good result

     

    the next thing you want to try is to change the motor cable, even though the cable has continuity can be broken filaments, which can cause current problems

     

    do you know what are the part number for the connectors?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 10 years ago in reply to e14 Contributor

    Aaron-

    Did you every get things worked out on the axis issues?

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 10 years ago in reply to e14 Contributor

    Here is a link to replace the Cable.  Replicator 2/2X Jumper Cable - X Endstop - RobotShop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Nate1616

    I'm afraid that this link is for the Sensor swich cable not for the Motor cable

     

    I'm locking for a brand new makerbot replicator Motor cable or to find parts to make one or

     

    as last resource refurbish my "faulty" cable 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>