3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Brittle PLA
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 17 answers
  • Subscribers 348 subscribers
  • Views 6455 views
  • Users 0 members are here
  • pla
  • white_pla
  • 3D Printing
  • robox
  • cel_robox
Related

Brittle PLA

danielw
danielw over 10 years ago

Has anybody had any issues with PLA going brittle?  At work we have a CEL Robox and I've noticed that some white PLA filament that was on the end of a spool and lying around for several months has gone brittle and snaps easily. New filament is much more bendy.

 

We have a windowless office so it has only seen fluorescent light, so I guess that it's to do with moisture in the air.  We keep current filament in ziplock bags with silica gel packs.

 

I know that PLA is supposed to be bio degradable so maybe it's just degrading?  I'm wondering if the same will happen to finished parts?  I'm planning to print out some test strips and test them over time, but wondered if anybody has any good info on this and point to a good online resource.  I'll also be having a look on the CEL site for info.

 

I suppose this is possibly another reason for using ABS on my REP RAP bodge-o-matic printer at home!  I thought I'd get away with PLA if it wasn't too hot.

 

Dan.

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago +5 suggested
    Hello Daniel, The problem is not specifically related to PLA, but - in a different measure - it occurs also with ABS. Anyway PLA filament is subject to degrading almost easily than ABS. This is the reason…
  • gregoryfenton
    gregoryfenton over 10 years ago +5 suggested
    I regularly change the colours of the materials I use meaning that I have lots of partly used rolls. The simple technique I use is to put each roll in a bag, pierce a small hole for the filament to pull…
  • dougw
    dougw over 10 years ago +4 suggested
    My experience is that the tendency to become brittle is much more likely in the section of PLA that is in the printer, perhaps because of exposure to heat. Maybe the pigment material starts annealing into…
Parents
  • brucekline
    0 brucekline over 7 years ago

    I have experience with optical fiber and it has the same problem! Water can make glass fiber brittle if there is stress. But it takes both. Water attacks the micro-cracks on the surface of a stressed fiber. No stress, the water can't get into the glass. No water, the micro-cracks do not grow. Most optical fiber has a moisture barrier plus a clearly stated minimum bend radius to avoid stress.

     

    My experience with PLA shows very similar behavior. Only the filament under stress (the straitened portion in this case) is susceptible to humidity. The fiber that is still coiled on the reel without stress is not absorbing moisture (at least not fast enough to matter). The timer starts when the filament is unreeled, straightened, and put under stress. The heating and printing process relaxes the stress making the printed object immune to the effects of moisture. The cooling object does shrink a bit which might cause stress but I have not experienced nor heard of any problems with spontaneous fracture.

     

    Here's an experiment I think I'll try: Unwind enough filament while on the printer to relieve the stress; let it coil to a more stress free state. I'm hoping that the filament within the printhead has been warmed enough for stress relief. Someone else should try this too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • brucekline
    0 brucekline over 7 years ago

    I have experience with optical fiber and it has the same problem! Water can make glass fiber brittle if there is stress. But it takes both. Water attacks the micro-cracks on the surface of a stressed fiber. No stress, the water can't get into the glass. No water, the micro-cracks do not grow. Most optical fiber has a moisture barrier plus a clearly stated minimum bend radius to avoid stress.

     

    My experience with PLA shows very similar behavior. Only the filament under stress (the straitened portion in this case) is susceptible to humidity. The fiber that is still coiled on the reel without stress is not absorbing moisture (at least not fast enough to matter). The timer starts when the filament is unreeled, straightened, and put under stress. The heating and printing process relaxes the stress making the printed object immune to the effects of moisture. The cooling object does shrink a bit which might cause stress but I have not experienced nor heard of any problems with spontaneous fracture.

     

    Here's an experiment I think I'll try: Unwind enough filament while on the printer to relieve the stress; let it coil to a more stress free state. I'm hoping that the filament within the printhead has been warmed enough for stress relief. Someone else should try this too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • danielw
    0 danielw over 6 years ago in reply to brucekline

    Hi Bruce, 

    That makes some sense,  I had tried printing some parts and kept one in a sealed bag with desiccant, and another in water,  After 2 to 3 months I would say they behaved similarly.  Unfortunately the company went into administration. I left and the test pieces will have been thrown away in the clear out.  I wonder if the results would have been different if I'd stressed the parts.

     

    I knew about the minimum bend radius and had thought that it was just a factor of the cracks scattering the light.  I didn't know about moisture effects, you learn something new every day!

     

    Dan.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer