3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum how to my A8 3D printer to print
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 342 subscribers
  • Views 1522 views
  • Users 0 members are here
  • 3d printer
Related

how to my A8 3D printer to print

fatguyl0l
fatguyl0l over 8 years ago

Hi I just got a new A8 3D printer for the Holidays. I finished setting it up checked all the motors every thing moves as it should. Then when I go to load gcode into the printer it will say it's printing but will not move any advise. Here is what I am working with.

Attachments:
imageA8 3D Printer Installation Instructions.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +2 suggested
    When it starts, the nozzle needs to heat up to about 190 degrees or more which can take a few minutes. Also if it has a heated bed the bed can take quite a while to heat up. Nothing moves until the correct…
  • fatguyl0l
    fatguyl0l over 8 years ago +2
    Yup bad sd card works great thank you so much for all your help it's nice to bounce ideas back and forth between some one thank you.
  • fatguyl0l
    fatguyl0l over 8 years ago in reply to dougw +1
    everything is at temp before I run it from what I've seen so far it's something with the gcode it's not reading a code that it needs and after I try to run it will remove all the code on the file and leave…
Parents
  • fatguyl0l
    0 fatguyl0l over 8 years ago

    Nope still just shows that print on the lcd won't move and then deletes the gcode that I try to run. well I'm at a dead end I've even scrolled through the gcode on the sd card that came with it to see if there was something not being added in and no differences between the two just xyz if nothing else going to see if maybe it's the sd card that's all I can think that might cause the problem.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fatguyl0l
    0 fatguyl0l over 8 years ago

    Nope still just shows that print on the lcd won't move and then deletes the gcode that I try to run. well I'm at a dead end I've even scrolled through the gcode on the sd card that came with it to see if there was something not being added in and no differences between the two just xyz if nothing else going to see if maybe it's the sd card that's all I can think that might cause the problem.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer