3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum ROBOX New Head Calibration
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 341 subscribers
  • Views 1826 views
  • Users 0 members are here
Related

ROBOX New Head Calibration

danielw
danielw over 8 years ago

Hi, Those with Robox printers might find this useful.

 

I've recently had a new head for the CEL ROBOX printer after the last head burst its seals and splurged plastic all over itself, out of warranty of course.

After putting the head on and purging to Polar White PLA, I had issues with poor extrusion, feeder slipping and so on.  I ran the nozzle opening calibration and (touch wood,) the printer is now working normally.

The head is a Quick fill V2

 

Before calibration my B values were 0.8 and -0.8

After calibration the values are 1.55 and -1.6

 

That seems like a fairly big difference and explains the under extrusion issues.

Has anyone else seen this.  I was under the impression that the heads came pre-calibrated.

 

Dan.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to dougw +3 suggested
    I recently had to also buy a new head (200$... ouch), the change was pretty easy, just ran the standard calibration routines and that was it. Be warned that a new head comes with very little warranty,…
  • dougw
    dougw over 8 years ago +1 suggested
    I have done a lot of printing with my Cel Robox and have blown the seals twice. The first time it was fixed under warranty. I have not replaced it yet after it blew a second seal because it is also cogging…
Parents
  • danielw
    0 danielw over 8 years ago

    Glad to see it's not just me.

    The Robox is a good machine with simple software and ideal for in work as it looks the part.

    But,  The first head lasted over 500 hours and it's seals went above the fine nozzle after running some higher temperature filament through it. The second head lasted a month and blew it's seal above the fine nozzle and was replaced under warranty.

    Third head blew its seal, again above the fine nozzle after about 7 months.  It has been quiet mechanically so it hadn't got anywhere near 500 hours. (Less than 200H I think)

    Other than that It has had a replacement filament detection switch. (The plastic on the original one wears away.)  I temporarily repaired it by packing it out.  The replacement part has a metal surface to the filament to run against.

     

    As Peter quite rightly said, you can build one.  Which I did do, and since I built it (and it's mine,) I'm a lot less hesitant to dive in and fix / improve it if I see a problem.  It's got an E3D hotend and I've chucked all sorts of different filaments through it. And It's quick to change filaments.  Some of the guys at work have seen it and think it's terrible (it is a bit of a franken-printer) but quality is up there with the ROBOX.  I will admit it's not quite as plug and play though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • danielw
    0 danielw over 8 years ago

    Glad to see it's not just me.

    The Robox is a good machine with simple software and ideal for in work as it looks the part.

    But,  The first head lasted over 500 hours and it's seals went above the fine nozzle after running some higher temperature filament through it. The second head lasted a month and blew it's seal above the fine nozzle and was replaced under warranty.

    Third head blew its seal, again above the fine nozzle after about 7 months.  It has been quiet mechanically so it hadn't got anywhere near 500 hours. (Less than 200H I think)

    Other than that It has had a replacement filament detection switch. (The plastic on the original one wears away.)  I temporarily repaired it by packing it out.  The replacement part has a metal surface to the filament to run against.

     

    As Peter quite rightly said, you can build one.  Which I did do, and since I built it (and it's mine,) I'm a lot less hesitant to dive in and fix / improve it if I see a problem.  It's got an E3D hotend and I've chucked all sorts of different filaments through it. And It's quick to change filaments.  Some of the guys at work have seen it and think it's terrible (it is a bit of a franken-printer) but quality is up there with the ROBOX.  I will admit it's not quite as plug and play though.