3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Ack! My trusty Monoprice Maker Select Plus is broken.  Any sugestions on a suitable replacement/upgrade?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 5 answers
  • Subscribers 340 subscribers
  • Views 4465 views
  • Users 0 members are here
Related

Ack! My trusty Monoprice Maker Select Plus is broken.  Any sugestions on a suitable replacement/upgrade?

genebren
genebren over 5 years ago

About 6 hours into a 8 1/2 hour job, I finally took notice that my job was still a few layers above the raft.  Even though the head was moving, no filament was being extruded.  I am not sure of the order of events, but the filament was jammed.  Did the hot end cool too much to melt the filament? Did the filament actually jam entering the heater?  After a quick disassembly, I found a distorted filament (partially ground away) in the extruder drive housing.  After I reheated and cleared the tip, I extracted the remaining chuck of filament (very difficult as I could neither pull or push it with a hot tip).  I then fed new filament into the extruder and attempted to drive it into the heater.  Oh no, there was no filament movement (funny but after detecting the failure, I attempted to drive the extruder and thought that I had heard it driving???).  Moving the extruder motor into place on another driver it seemed to work.  I am now into a full disassembly to see if I can repair this unit.  Only time will tell.  I am also thinking about the possibility of buying a new printer to take the place as primary while I refurbish the existing one as a backup (or secondary) printer.

 

I am leading heavily into getting a new printer.  But now I face a dilemma, what kind of printer do I get?  I have not been looking around to see what else might be available and I still am a relative newbie to the world of 3D printers as this was my first printer, so I find myself not too well equipped to pick a replacement. Any suggestions as to designs, models or vendors would be a great help.  What features should I be considering at this point (auto leveling, upgraded hot ends, etc.)?

 

Thanks in advance,

Gene

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +8 suggested
    I have an Anycubic I3 Mega and prints are done using PLA so nothing exotic. I don’t level it frequently and haven’t added any upgrades. It has been reliable so I would say it has been good for a basic…
  • milosrasic98
    milosrasic98 over 5 years ago +7 verified
    Hi Gene! If you're looking for another printer, could you maybe tell us a bit what you're looking for in the printer, by that I mean, just some general stuff like, size of prints, are you planning on printing…
  • hlipka
    hlipka over 5 years ago in reply to milosrasic98 +7 suggested
    I can second the Prusa. Half a year ago I exchanged my K8200 for a Prusa MK3S, and I have not looked back (and in the 6 months I have printed more stuff than in the 5 years I owned the K8200). It really…
Parents
  • milosrasic98
    0 milosrasic98 over 5 years ago

    Hi Gene!

     

    If you're looking for another printer, could you maybe tell us a bit what you're looking for in the printer, by that I mean, just some general stuff like, size of prints, are you planning on printing just PLA, or printing flexibles, ABS, Nylon, your budget for a main/secondary machine? I took a look at the model of your 3D printer and it looks like a really good machine with rods and linear bearings for all axis which I love. A machine that comes to mind is a Prusa i3 or a Prusa Mini. I haven't worked with them directly, but I've heard really great things about both machines and know people who have an i3, though they are a bit more pricey. There is also the Prusa slicer which comes with really fine tuned presets for these machines.

     

    I have a Creality Ender3 Pro, which I have used for the last 9 or 10 months and considering it's under 250$ it performs amazing. I didn't have any major problems with it, a few clogs with some specific filament, but besides that, it worked flawlessly. I haven't tried any materials but PLA on it. It has an okay build volume of 220x220x250mm and instead of rods and linear bearings, it uses v-slot extrusions and rollers. It would be a downgrade on that aspect from your machine, but if you're looking just for something to work while you fix your printer, this can be a good option considering  the price. There is also an Ender3 V2 out which has an automatic bed leveling sensor, I haven't used it, but I've read pretty good stuff about it. The best thing I can say about the Ender3 Pro is that it's a great machine for tinkering around with it and upgrading with a lot of mods available, for example, it's a bowden extruder machine, so it won't really work with flexibles as it is, but there are a lot of mods to convert it to a direct drive so it can print flexible materials and so on.

     

    Hope you get your machine fixed fast!

     

    Milos

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hlipka
    0 hlipka over 5 years ago in reply to milosrasic98

    I can second the Prusa. Half a year ago I exchanged my K8200 for a Prusa MK3S, and I have not looked back (and in the 6 months I have printed more stuff than in the 5 years I owned the K8200). It really is a work horse, and you can expect to unpack it and start printing (having done quite a lot of PLA and PETG and a bit of ABS so far).

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 5 years ago in reply to hlipka

    Thanks hlipka .  When I first decided to get a 3D printer, a lot of people had suggested Prusa printers.  This is definitely on my list to consider.  It is good to hear that you are happy with yours!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • genebren
    0 genebren over 5 years ago in reply to hlipka

    Thanks hlipka .  When I first decided to get a 3D printer, a lot of people had suggested Prusa printers.  This is definitely on my list to consider.  It is good to hear that you are happy with yours!

    • Cancel
    • Vote Up +3 Vote Down