3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Having a hard time starting out [Prusa i3] e3D v6 hotend, pla clogging all the time
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 341 subscribers
  • Views 2283 views
  • Users 0 members are here
  • i3
  • 3d-printing
  • 3d_printer
  • prusa
Related

Having a hard time starting out [Prusa i3] e3D v6 hotend, pla clogging all the time

e14 Contributor
e14 Contributor over 11 years ago

So I've assembled my first 3D printer out of mostly spare parts and bits..

Got everything setup, at first i used a all metal hotend from china, E3D v6 replica's for 10$

 

image

The beginning of the test cube, 3 different attempts, learning about the settings..

In each case, i stopped the printer early because it was not moving high enough Z axis,

meaning it ended up, grinding around inside the previous layer.

 

Unfortunally it constantly failed, sometimes in the beginning, sometimes mid print. It failed by clogging up,

I thought i'd better get a "decent" hotend, so I puchased a E3D V6 hotend 0.4mm nozzle. and set it all as a bowden setup.

Still fails.

 

image

This is how my printer looks most of the time, me cleaning out clogging. image

 

My main issues

 

1) Hotend clogging up, "way up in the cold part"  as if it's retracting melted plastic upwards.

Result,  nozzle + entire insides of the hotend is clogged up, I'm fairly quick now to remove the clogging, but it does not really help me out.

 

 

2) Z-axis is not raising enough. It' appears 1st layer is printet "into" the glass, meaning 1st layer is invisible, then second layer is barely visible.

My Z-axis is connected via 5mm rods, (M5) to 2x nema 17, 1.8(200) steppers. and used the prusa calculator via google and set the step to 75..

not sure about the 0.8/0.8*1 in the firmware so i left it..

 

 

 

Things I tryed allready,

- Calibrating PID temperature for the hotend.

- Calibrating / leveling the bed to the hotend, allowing only 1 single sheet of paper to fit under it at anylocation at Z-home

- Printing pla with to high temperatures, not a good idea image what a mess.

 

I'm not sure weither it's my Marlin setup, my G-code or whats up, but I'm kinda frustrated right now image

 

This is my typical slic3r settings(hope you can see, not sure about the resolution on the webpage)

image

 

And promterface.. (havent really done anything here, except when i was calibrating the hotend temp for marlin.)

image

 

 

Attached files

 

- Marlin for Ramps 1.4

- 20mmx20mmx20mm test cube

 

 

Any help would be appriciated... 

Attachments:
Marlin.zip
20mm_cube.g.zip
  • Sign in to reply
  • Cancel
Parents
  • bwelsby
    0 bwelsby over 11 years ago

    Hi Martin,  First things first lets try and sort the Z axis, the E3D clogging may be partly due to the Z axis not lifting enough causing too much back pressure on the extruder.

     

    How you got 75 is confusing so lets start from scratch.

    Your stepper motor requires 200 full steps for one rotation, however it is usual to have your stepper drivers configured for micro stepping and it is common to have this set to 16 times.  Check what your stepper drivers are and what links have you on your RAMPS  for this.

     

    So lets assume that this is the case, the stepper motor will require 200 x 16 micro steps for one full revolution thats 3200

    A standard M5 rod has a pitch of 0.8 mm  so 3200 steps will move the z axis by 0.8mm

    Therefore to move the z axis by 1mm you require 3200/0.8 * 1 steps  = 4000

    What I see in your firmware is:

    #define DEFAULT_AXIS_STEPS_PER_UNIT   {100, 100, (75.0*8/0.8)*1, 800}

    (75.0 *8 / 0.8) * 1 = 750

     

    Try this

    #define DEFAULT_AXIS_STEPS_PER_UNIT   {100, 100, 4000, 800}

    Use pronterface to raise the z axis by say 10mm and measure to confirm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bwelsby

    Very nice..

     

    That Z-axis is moving a lot faster now, i will try to make a test print with the new setting, even though it seems fine with promterface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Update

     

    Clearly the Z axis is much much better now, and it both sounds and feels "as I expect it should"

    I raised the Z axis around 20mm and tryed extruding via pronterface also working, extruded quite a bit, and it was ok. (i did not retract at all)

     

    I rechecked my endstops @ home also 1 paper height from the glass plate in all 4 corners.

    Eiger to try, i started the printer on the cube again,

     

    However, even the 1st layer came out blank, and i could see the extruder wheel feeding filament into the hotend.

    yet nothing came out, i stopped the printer, raised the Z-axis again, tryed manual extruding, nothing came out.

     

    Turn off heating, removed the bowden tupe, pulled carefulle the filament out of the hotend,

    there was probably 150mm inside, curled up. like a screw.

     

    image

    The filament i pulled out of the hotend "topside" is right there.

     

    Just to be safe i disassembled the hotend and it was clear, seems i was able to pull it all out, before it completely cooled.

    It was around 150 degress during disassembly.

     

    Is there a way to calibrate the extruder ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Update

     

    Clearly the Z axis is much much better now, and it both sounds and feels "as I expect it should"

    I raised the Z axis around 20mm and tryed extruding via pronterface also working, extruded quite a bit, and it was ok. (i did not retract at all)

     

    I rechecked my endstops @ home also 1 paper height from the glass plate in all 4 corners.

    Eiger to try, i started the printer on the cube again,

     

    However, even the 1st layer came out blank, and i could see the extruder wheel feeding filament into the hotend.

    yet nothing came out, i stopped the printer, raised the Z-axis again, tryed manual extruding, nothing came out.

     

    Turn off heating, removed the bowden tupe, pulled carefulle the filament out of the hotend,

    there was probably 150mm inside, curled up. like a screw.

     

    image

    The filament i pulled out of the hotend "topside" is right there.

     

    Just to be safe i disassembled the hotend and it was clear, seems i was able to pull it all out, before it completely cooled.

    It was around 150 degress during disassembly.

     

    Is there a way to calibrate the extruder ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bwelsby
    0 bwelsby over 11 years ago in reply to e14 Contributor

    If you are using 1.75mm filament the bowden tube should fit into the hot end as far as it can up to the heat break there shouldn't be any room for the filament to curl up. See E3D instructions E3D-v6 Assembly - E3D-Online

     

    Calibrating the extruder steps per mm:

    Disconnect the bowden from the drive end and mark a point on the filament at the drive exit.

    Tell extruder to extrude 100mm and mark at same exit point.

    measure length between the two points, it should be 100mm.

    Adjust the extruder steps per mm to correct.   New value = (100 / measured length) * old value

    In your config you have it currently set to 800

    new value would therefore be      (100 / measured length )  * 800

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer