3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum 3D Printer Power Supply Amperage
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 341 subscribers
  • Views 2316 views
  • Users 0 members are here
  • 3d_printer
  • power_supply
Related

3D Printer Power Supply Amperage

neildonn
neildonn over 11 years ago

HI folks,

 

I noticed today (as look may have it) my 3D printer was smoking. image On closer inspection I noticed the power terminal on the RAMPS board was melting and smoking. Don't worry, at this point I quickly unplug from the mains.

 

The power supply is 220v (I live in the UK) with a 12v and 20A ouput. I'm wondering if the power supply is faulty or the cable from the power supply cannot handle the power/amps.

 

Any ideas? I have a spare PC power supply will that do if needed?

 

Cheers,

Neil.

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 11 years ago in reply to neildonn +2
    Yes 25A is fine as long as it isn't too big to fit into the terminals.
  • bwelsby
    bwelsby over 11 years ago +1 suggested
    Hi Neil, To me this sounds like it could be a bad connection on the RAMPS board power terminal as that what was getting hot. It's important for these high current connections are clean and tight. If you…
  • bwelsby
    bwelsby over 11 years ago in reply to neildonn +1
    That's great. Personally I would leave it soldered, it's not something I would really need to disconnect. Brian
Parents
  • Nate1616
    0 Nate1616 over 11 years ago

    Neil-

    Sorry I'm a bit late but Brian stated it pretty well.  One thing I have also ran into with 3d printing electronic boards is a lot of the cheaper Chinese made ones have at times burned and smoked as you stated.  Just lower quality parts used.  The typical power supplied for the RAMPS should be 12V >16A (20A optimal) if running a heated bed.  Soldering to the board should not be a problem just wont be easy if have to change something.

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Nate1616
    0 Nate1616 over 11 years ago

    Neil-

    Sorry I'm a bit late but Brian stated it pretty well.  One thing I have also ran into with 3d printing electronic boards is a lot of the cheaper Chinese made ones have at times burned and smoked as you stated.  Just lower quality parts used.  The typical power supplied for the RAMPS should be 12V >16A (20A optimal) if running a heated bed.  Soldering to the board should not be a problem just wont be easy if have to change something.

    Nate