3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Which is better ABS or PLA filament?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 343 subscribers
  • Views 1559 views
  • Users 0 members are here
  • 3d_printing
Related

Which is better ABS or PLA filament?

bkoehlercq
bkoehlercq over 11 years ago

Hello,

 

I am very much a beginner, and am just learning more about 3D printing. I do 3D modeling as a hobby, and I have a pretty basic question. I would like to save up for my first 3D printer and would like to know which is better PLA or ABS filament?

 

Also would like some suggestions on a good starter printer.

 

Thank you in advance

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    I will just add the Clem's response. Another good thing about ABS is you can give it an acetone bath and make the print look as though it was cast using molds. ABS needs to be used on any part that will…
  • clem57
    clem57 over 11 years ago +2 suggested
    Simplifying the myriad of factors that influence the use of one material over the other, broad strokes draw this comparison. ABS - Its strength, flexibility, machinability, and higher temperature resistance…
Parents
  • clem57
    0 clem57 over 11 years ago

    Simplifying the myriad of factors that influence the use of one material over the other, broad strokes draw this comparison.

    ABS - Its strength, flexibility, machinability, and higher temperature resistance make it often a preferred plastic for engineers, and professional applications. The hot plastic smell deter some as does the plastics petroleum based origin. The additional requirement of a heated print bed means there are some printers simply incapable of printing ABS with any reliability.

    PLA - The wide range of available colors and translucencies and glossy feel often attract those who print for display or small household uses. Many appreciate the plant based origins and prefer the semi-sweet smell over ABS. When properly cooled, PLA seems to have higher maximum printing speeds, lower layer heights, and sharper printed corners. Combining this with low warping on parts make it a popular plastic for home printers, hobbyists, and schools.

     

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bkoehlercq
    0 bkoehlercq over 11 years ago in reply to clem57

    Thank you Clem, I really appreciate the information

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bkoehlercq
    0 bkoehlercq over 11 years ago in reply to clem57

    Thank you Clem, I really appreciate the information