3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Which is better ABS or PLA filament?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 343 subscribers
  • Views 1557 views
  • Users 0 members are here
  • 3d_printing
Related

Which is better ABS or PLA filament?

bkoehlercq
bkoehlercq over 11 years ago

Hello,

 

I am very much a beginner, and am just learning more about 3D printing. I do 3D modeling as a hobby, and I have a pretty basic question. I would like to save up for my first 3D printer and would like to know which is better PLA or ABS filament?

 

Also would like some suggestions on a good starter printer.

 

Thank you in advance

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    I will just add the Clem's response. Another good thing about ABS is you can give it an acetone bath and make the print look as though it was cast using molds. ABS needs to be used on any part that will…
  • clem57
    clem57 over 11 years ago +2 suggested
    Simplifying the myriad of factors that influence the use of one material over the other, broad strokes draw this comparison. ABS - Its strength, flexibility, machinability, and higher temperature resistance…
Parents
  • dougw
    0 dougw over 11 years ago

    My printer (Cel Robox) can do both PLA and ABS and I have both types of reel, but I only use PLA - it is stronger than I expected and I can operate the printer anywhere without objectionable smells. I print lots of things that need to be "structural". I find it is more or less comparable to the average low cost plastic consumer product. One advantage of PLA is you can get "clear" PLA which is great if you want LEDs to shine through or diffuse through the material.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    My printer (Cel Robox) can do both PLA and ABS and I have both types of reel, but I only use PLA - it is stronger than I expected and I can operate the printer anywhere without objectionable smells. I print lots of things that need to be "structural". I find it is more or less comparable to the average low cost plastic consumer product. One advantage of PLA is you can get "clear" PLA which is great if you want LEDs to shine through or diffuse through the material.