3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum What Type of 3D Printing Filament Material Do You Use?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 341 subscribers
  • Views 6794 views
  • Users 0 members are here
  • 3D printing filament
Related

What Type of 3D Printing Filament Material Do You Use?

rscasny
rscasny over 2 years ago

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 2 years ago +3
    About a year ago, I switched from PLA to PETG. Strong prints, less warping, and it isn't excessively expensive compared to PLA. I also have several bright colors in ColorFABB's nGEN. That's probably…
  • strb
    strb over 2 years ago +1
    To me it really depends on the application I will use the 3D printed object. PLA is the "go to" material for general purpose stuff without particular requirements, probably 80% of what I print PETG if…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to dougw +1
    "print a hole" is meta!
Parents
  • strb
    strb over 2 years ago

    To me it really depends on the application I will use the 3D printed object.
    PLA is the "go to" material for general purpose stuff without particular requirements, probably 80% of what I print
    PETG if I need a little bit more heat resistance or ABS if I need heat resistance and ease of post proceessing (it can be easily glued,can be machined beautifully and it's easy to smooth)
    TPU for compliant or "soft" objects
    PA+CF because it's cool, almost never used except for some small part on my RC car where high mechanical properties are essentials

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • strb
    strb over 2 years ago

    To me it really depends on the application I will use the 3D printed object.
    PLA is the "go to" material for general purpose stuff without particular requirements, probably 80% of what I print
    PETG if I need a little bit more heat resistance or ABS if I need heat resistance and ease of post proceessing (it can be easily glued,can be machined beautifully and it's easy to smooth)
    TPU for compliant or "soft" objects
    PA+CF because it's cool, almost never used except for some small part on my RC car where high mechanical properties are essentials