555 Timers
  • Technologies
  • More
555 Timers
Blog 555s Used as Monostables
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 10 May 2022 11:47 AM Date Created
  • Views 1796 views
  • Likes 11 likes
  • Comments 3 comments
  • monostable
  • ne555
Related
Recommended

555s Used as Monostables

jc2048
jc2048
10 May 2022

I've never used a 555 timer as a monostable, so I thought I'd give it a go. This should be easy,
shouldn't it.

Here's the circuit as it's given on an old ST datasheet.

image

As they describe it, a falling edge at the trigger input sets the output and releases the capacitor
to start charging. When it gets to the internal threshold voltage, the output is reset and the
capacitor is discharged ready for another go. I've wired one up on a breadboard with a 10uF and 22k
for the timing capacitor and resistor. According to the timing formula (t=1.1*C*R) that should give
me an output pulse width of something like 240ms, though using an electrolytic means it won't be
all that accurate.

To give the falling edge, I've also wired up another 555 (no expense spared when it comes to e14
blogging) as an astable. That way I can see how the monostable behaves when repetitively triggered.
The astable period is around 1.5 seconds.

What I expected was a nice neat positive-going pulse at every falling edge of the astable waveform.
What I got was this

image

The yellow trace is the trigger input to the monostable and the blue is the output. The pulse
period is ok, but after that it can't seem to make up its mind what it wants to do. Evidently,
there's more to this than the ST datasheet would lead me to believe.

Looking at the capacitor voltage, I see this

image

The capacitor does charge, but then just sits there without the reset happening. The reset doesn't
happen until the input goes high again, so it looks like the trigger needs to be not only a
negative-going edge but also short enough that it doesn't block the reset of the monostable.

The old National datasheet for the NE555 explains this better and, in a suggested circuit for a
chain of monostables, shows the use of a coupling capacitor and a pull-up resistor (1nF and 33k) as
a differentiator for the trigger as a way to to get the necessary short pulse width. (There's no
sign of a diode, to catch the positive-going edge that will ascend from the rail voltage, so
presumably they're confident that the anti-static protection diode can cope.)

image

So, here it is with the extra capacitor and resistor added

image

That's better. Just for interest, here's the differentiator output as the trigger input sees it.

That gives a pulse width that's around 10us at the trigger input.

image

Finally, for fun, I've wired a chain of five monostables in a row, with the outputs driving LEDs.
Here they are pulsing in sequence every time that the astable triggers them:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In case it's not obvious, the astable is on the right and the chain of monostables run from right to left. Why I did it like that I don't know, but I'm not going to change it now.

If you found this interesting and would like to see more blogs I've written, a list can be found
here: /members-area/b/blog/posts/jc2048-blog-index-new-version

References
[1] https://www.st.com/en/clocks-and-timers/ne555.html
[2] https://www.ti.com/lit/ds/symlink/ne555.pdf

  • Sign in to reply
  • shabaz
    shabaz over 4 years ago

    Neat demo!

    I've not used monostable mode much either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    Here is a secret.......this arduino ray gun project  https://www.youtube.com/watch?v=t-4IWkrXu9E

    has 2 555s in it.

    One is used as the debouncer on the trigger.

    The other 555 is the clock that sequences the LED rotation  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 4 years ago

    Yes, the 555 can be the source of endless fun and circuit variations.