555 Timers
  • Technologies
  • More
555 Timers
Forum Feedback on 555 timer Schmidt Trigger design
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 2 answers
  • Subscribers 49 subscribers
  • Views 6420 views
  • Users 0 members are here
  • input conditioning
  • photo resistor
  • schmidt-trigger
Related

Feedback on 555 timer Schmidt Trigger design

colporteur
colporteur over 3 years ago

image

Can I get members insight into using a 555 timer as a schmidt-trigger design that I pulled from the Internet?

I found this schmidt-trigger design using a 555 timer. I would like to use it to condition the output of a photo-resistor. The 555 timer output will feed the input to a Arduino Mega. I'm in the process of bench testing the setup to finalize component values. While testing I figured I would throw it out to some more enlightened minds than mine for feedback.

I'm using the 555 only because I have a stock of them. I don't have any readily available smidth-trigger IC's so I figured I would go with what I have and build from scratch. Building from scratch especially using Internet designs comes with risk. I was hoping to mitigate the risk by getting community feedback.

If inquiring minds suggest you don't want to do this, that is a good thing.

  • Sign in to reply
  • Cancel

Top Replies

  • AE7HD
    AE7HD over 3 years ago in reply to colporteur +1
    I have a fair amount of experience with 555 timers, IR sensing, break beam circuits, etc. I'd like to help. But I need to know what you are trying to do. What is the ultimate goal?
  • colporteur
    colporteur over 3 years ago in reply to AE7HD +1
    Is this the sensor placement you are suggesting?
  • colporteur
    colporteur over 3 years ago in reply to Jan Cumps +1
    Sorry JC I have a reluctance to invest anymore effort in the IR solution. Modification of the train cars is something that frowned upon. This applied to even putting a magnet for another solution. I…
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi Sean,

    There are known working circuits here: https://www.talkingelectronics.com/projects/50%20-%20555%20Circuits/50%20-%20555%20Circuits.html

    (press Ctrl-F and search for "light", since that's a very long page.

    There are light detectors using an LDR, and some with phototransistor.

    Otherwise I think you'd have to either try that for real, or simulate it, since that circuit could have come from anywhere, and it's not one of the two normal topologies seen regularly with a 555. That doesn't mean it won't work, it just means it's perhaps a lot less common. Definitely worth simulating or trying for real especially if it's for the train use-case.

    What's the actual requirement incidentally? Is it for train detection, or some other purpose? 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to shabaz

    Detector for KY-008 laser light. I'm using what consumables I have on hand. Photo resistors and 55 timers. This circuit might have some merit. I will checkout the resources. Thanks for the insight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to colporteur

    Hi Sean,

    I see! Is it a break-beam kind of thing with no modulation? If so, then there is an easier way that may work better than the 555 circuit:

    Since the laser is powerful, the LDR resistance will change significantly. You could experiment with connecting just the LDR and a resistor (i.e. potential divider circuit) directly to the analog input of the Arduino. It could even have an automatic calibration on start-up, or if a button is pressed, whereby it reads the analog level when a train is present or when a train is not present, and the code then uses its own threshold. 

    But probably there may be no need for calibration, since the difference with the laser blocked and unblocked may be significant (if it is well aligned).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to shabaz

    But really this should be a stopgap solution, since it is worth experimenting with the modulation method mentioned in the earlier discussion, it is cheaper and less need for precise alignment, unlike with an unmodulated laser. With modulation you get great sensitivity in your detection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to shabaz

    I agree there is a more simpler solution. I just don't have it! My ideal was to buy rather than build. That failed miserably with the IR sensors (well I learned a lot). I haven't found a reliable IR solution so I am on to plan B. 

    The IR solution was a disappointment. The noise reduced their performance. I'm rolling around the idea of further bench testing the IR sensor. Discuss their operation. Explore some of the problems and look at some solutions. I discovered (wasn't aware of this) that not all the IR sensors have the same circuit. I found four different schematics all for the same IR sensor image. They all may look the same in the pic but the circuits are different. My schedule doesn't afford me the time to park what I am doing and take the tangent learning opportunity. 

    I've been experimenting with the KY-008 laser and the photo resistors. I have had good success detecting the beam on the bench setup. I haven't incorporated the schmidt-trigger design yet. I got distracted by another project to help an Arduino code developer. I'm hoping to get back at the sensor this week. My thinking is using the simple trigger is a quantitative transition feeding the Mega would improve performance. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to colporteur

    A few years ago I did something similar with reed switches, something very simple.

    (+) VenTTracker #06 -  Window Sensor Prototype - element14 Community
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
  • colporteur
    0 colporteur over 3 years ago in reply to javagoza

    Nice design and layout. What is the sensor the magnet on the upper small square block triggering. A read switch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to colporteur

    They are two Plastic Magnetic Reed Switches. Reed Contact Normally Open (N/O)

    https://www.amazon.es/Gebildet-Interruptor-Magn%C3%A9tico-Inducci%C3%B3n-Normalmente/dp/B07Z4RR4QV

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • javagoza
    0 javagoza over 3 years ago in reply to colporteur

    They are two Plastic Magnetic Reed Switches. Reed Contact Normally Open (N/O)

    https://www.amazon.es/Gebildet-Interruptor-Magn%C3%A9tico-Inducci%C3%B3n-Normalmente/dp/B07Z4RR4QV