Products
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
Artificial Intelligence and Machine Learning
  • Technologies
  • More
Artificial Intelligence and Machine Learning
Forum Does anyone know about K210 Dual-core RISC-V 64bit Boards ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Artificial Intelligence and Machine Learning to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 96 subscribers
  • Views 5883 views
  • Users 0 members are here
  • kpu
  • k210
  • cnn
  • ai module
  • ml
  • audio accelerator
  • cnn accelerator
  • risc-v
  • ai
  • apu
Related

Does anyone know about K210 Dual-core RISC-V 64bit Boards ?

gsgill112
gsgill112 over 7 years ago

I was surfing the web and stumbled upon K210 Dual-core RISC-V 64bit Boards ...

another one Here and they pretty cheep for about 800 INR for the Module with Wifi ...

 

And these claim to have KPU(Neural Network Processor) inside,  64 KPU which is 576bit width, support convolution kernels, any form of activation function. It offers 0.25TOPS@0.3W,400MHz, and when you overclock to 800MHz, it offers 0.5TOPS. It means you can do object recognition 60fps@VGA.

 

Isn't that Coollll.....

 

Ref:-

https://www.indiegogo.com/projects/sipeed-maix-the-world-first-risc-v-64-ai-module#/

 

and even BananaPi has then in their dev boards ..

BPI-K210 RISC-V AIoT board - Banana Pi Wiki

 

Few details from the vendor:(Aliexpress)-

 

MAIX development board compared with OPENMV V4 development board
MAIX series development boardOPENMV V4
Master chipK210STM32H743
Chip coreDual-core RISC-V 64bit IMAFDCARM Cortex-M7 32bit
Main frequencyNominal 400M, can exceed 600MNominal 400M
RAM6MB general purpose memory + 2MB AI memory1MB
Flash16MB2MB
Mpy supportSupport, MaixPy open source projectSupport, openmv open source project
Conventional vision algorithmSupported, compatible with most openmv algorithmsOpenmv algorithm
Conventional visual algorithm speed2~3 times in openmv v4\
Neural network algorithmSupport, encapsulates the nnn class of mpySupport, encapsulates the nnn class of mpy
Neural network algorithm speedHundreds of GOPS (thousands of times STM32)Hundreds of MOPS
Face detection speed (QVGA, RGB image)Conventional algorithm 6 frames,
AI acceleration can reach more than 60 frames
About 2 frames
Price (RMB)69~199499
Is it commercially available?Commercial stamp hole moduleno

 

image

image

image

image

Awesome Features for a fraction of the cost ....

Anyone has used it ?

 

Regards,

GS Gill

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 7 years ago

    The comparison with an STM32H743 is simply ridiculous - the two chips are quite different and aimed at different markets.

    The STM32H743 does not cost $70.

     

    The problem with RISC-V modules from China is getting decent documentation and tools - both are free and easily available from multiple sources for ARM processors.

     

    I suspect that RISC-V is a coming thing - there is a momentum behind it, pushed by the Chinese corporate state (and others) so it may become a rival to ARM.

     

    A dual 64 bit core core RISC-V processor is not  really in the same class as Cortex M devices. If you are interested in further study it's worth reading :

    https://en.wikipedia.org/wiki/RISC-V

     

    and to get an idea of the money going in:

     

    https://www.sifive.com/risc-v-core-ip

     

    @Gurinder

     

    Have you used this thing or looked beyond the page you posted ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 7 years ago

    The comparison with an STM32H743 is simply ridiculous - the two chips are quite different and aimed at different markets.

    The STM32H743 does not cost $70.

     

    The problem with RISC-V modules from China is getting decent documentation and tools - both are free and easily available from multiple sources for ARM processors.

     

    I suspect that RISC-V is a coming thing - there is a momentum behind it, pushed by the Chinese corporate state (and others) so it may become a rival to ARM.

     

    A dual 64 bit core core RISC-V processor is not  really in the same class as Cortex M devices. If you are interested in further study it's worth reading :

    https://en.wikipedia.org/wiki/RISC-V

     

    and to get an idea of the money going in:

     

    https://www.sifive.com/risc-v-core-ip

     

    @Gurinder

     

    Have you used this thing or looked beyond the page you posted ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gsgill112
    gsgill112 over 7 years ago in reply to michaelkellett

    @michaelkellett

    Nup I was intrigued by the Cost point of the module and the claimed performance but did Not order YET due to the cost image Although the Module itself is Cheep (850 INR) The usable Module Board costs about 2500 INR which given it comes with a LCD and Camera Module is slightly higher for me to try out.

     

    I even found a Chinese FPGA Dev board that is like 1500 INR and boasts a ton of features, but al the docs is in Chinese and the Manufacture of the FPGA won't let me download the VDI file without a Chinese mobile no registration image .  

     

    Doing some digging, I found that the product page is Non Existing but couple of links to GitHub Repos can be found

     

    https://github.com/sipeed/MaixPy_Doc_Us_En_Backup

     

    https://github.com/sipeed/MaixPy

     

    It seams to be based on Python.. ..

     

    Will update if I find anything else.

     

    Regards,

    GS Gill