Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Documents
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Document Actions
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Related
Recommended
  • Audi Reveals Electric Bi-Turbo V6 Diesel Engine

    In the quest to get engines to perform better, while using less fuel, Audi have announced that they are working on a version of their V6 TDI engine which uses an electric...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Rolls-Royce delivers first rim-mounted permanent magnet tunnel thruster

    Rolls-Royce has delivered the first of its newly-developed permanent magnet tunnel thrusters (TT-PM) to Norwegian company Olympic Shipping, which will operate the thruster...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Toyota and DENSO develop of device enabling real-time vehicle data collection and transmission

    Toyota Motor Corporation (TMC) and DENSO Corporation (DENSO) jointly have developed an onboard communications network device, CAN-Gateway ECU (Controller Area Network...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Michelin demonstrates how low rolling resistance tires work

    Tires get overlooked in the headlines about fuel economy and CAFE standards, which is a little odd. After all, a car's tires are the only contact it has with the road...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • New Cadillac models offer a new advanced safety system that can avoid crashes

    Three new Cadillac models, including the ATS sport sedan, offer a new advanced safety system that can automatically stop the vehicle in low-speed conditions to help avoid...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Engineers putting wasted engine heat to good use: improving fuel economy

    Gasoline-powered, internal combustion engines are notoriously inefficient. Some estimates say as much as 70 percent of the fuel's energy is lost to friction and heat...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Nissan Concept Car Uses a Tablet as the Dashboard

    Nissan is using a tablet as an instrumental panel inside its new Terra SUV concept car, which it will showcase at the Paris Motor Show later this month. The innovative...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Gesture recognition coming to a car near you

    Imagine being able to operate your car radio, telephone or climate control settings just by making simple hand gestures. Consumer electronics experts believe it is the...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • 2013 Porsche Cayenne Diesel Rated by EPA, Bests Hybrid Sibling on Highway

    EPA fuel-economy data for the new-for-2013 Porsche Cayenne diesel is out, and the twist-happy sport-ute is good for 19 mpg in the city and 29 on the highway. Those figures...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Pilot Plans Record-Setting Flight With Diesel Made From Plastic

    A British pilot is hoping to set a world record for long-distance flight when he attempts to fly from Sydney to London in a small single-engine plane. But Jeremy Roswell...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Integrated wind-powered electric vehicle charging station

    Urban Green Energy (UGE) and GE unveiled the first integrated wind-powered electric vehicle charging station. The Sanya Skypump pairs UGE’s 4 kW vertical wind turbine...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • Apple iPhone 5: Five things for motorists to expect

    The Apple iPhone 5 is expected to be unveiled on 12 September. But with iPod integration fitted as standard in many cars (and as an option in many more), what does it...
    • Revision #1
    • on 8 Oct 2021 5:12 AM
  • S12ZVHY: S12 MagniV Mixed-Signal MCU for Automotive Instrument Cluster Applications*

    The S12ZVHY platform , part of the S12 MagniV mixed-signal MCU family , is an automotive instrument cluster solution with high integration in a single chip. It integrates...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • Low cost CAN 8/16/32 bits microcontrollers : more than 100 products to chose from

    Looking for low cost CAN microcontrollers ? Microchip offers more than 100 microcontrollers with 1 or 2 CAN interfaces and multiples LIN interfaces. These products can...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • MOST : un réseau à 25/50/150 Mbits pour l'automobile

    community.element14.com/.../contentimage_5F00_19286.html Destiné aux réseaux multimedia dans les véhicules, le bus MOST (haut débit) fonctionne sur des bus physiques...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • XKT564L: Evaluation system supporting MPC564xL 32-bit microcontrollers*

    The XKT564L EVB is an evaluation system supporting our MPC564xL microcontrollers . The complete system consists of an XPC56xxMB2 motherboard and an XDC564L daughter-card...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • MPC564xL: Qorivva 32-bit MCU for Chassis and Safety Applications*

    The Qorivva MPC564xL family of 32-bit Power Architecture MCUs is d esigned to specifically address the requirements of the safety standards IEC61508 (SIL3) and ISO26262...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • Single-Chip, Low-End Instrument Cluster based on Freescale S12 MagniV Mixed-Signal MCU*

    Get details on the S12ZVH MagniV microcontroller and associated production software package in a low-cost, single-chip instrument cluster solution. www.youtube.com/watch...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • MPC564xL Steer-by-Wire Lite Demo*

    Freescale puts the focus on steering with this dual motor control solution, featuring 32-bit Power Architecture. www.youtube.com/watch Visit Freescale.com/motorcontr...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
  • S12ZVH: S12 MagniV Mixed-Signal MCU for Instrument Cluster Applications*

    The S12ZVH platform , part of the S12 MagniV mixed-signal microcontroller family, is the first automotive instrument cluster solution with the most integration in a single...
    • Revision #1
    • on 8 Oct 2021 5:11 AM
<>