Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog Creating a new product - Research
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 21 Oct 2014 9:57 AM Date Created
  • Views 1487 views
  • Likes 1 like
  • Comments 4 comments
  • entrepreneur
  • business
Related
Recommended

Creating a new product - Research

Workshopshed
Workshopshed
21 Oct 2014

Following the RoadTest of the CapSense MBR3 Evaluation kit, I thought about creating a simple cursor board with 4 direction buttons and a select button with an I2C interface to a microcontroller host.

image

Before embarking on any venture, I like to do a bit of research to determine if the project is feasible.

 

  • Are there other products on the market?
  • What components will be needed?
  • What skills will be needed?
  • What tools will be needed?
  • Costs

 

Other products

The purpose of looking at other products to two fold. Firstly to see if there is an identical product already available or if you fit into a gap or can sufficiently differentiate your offering. The second is to see if there is a demand for your product. If you have something completely new then it's looking at more generic products to give yourself an idea.

I'd already looked into mechanical buttons as part of the roadtest so we can discount these from further analysis.

For the capacitive switches there do seem to be some comparative products. At the bottom end of the market there are breakout boards and single click buttons. At the top end there are complete touch solutions with inbuilt microcontrollers.

So there does seem to be a position for my board and the other products also suggest that the price point around $10 to $15 if I chose to sell them.

 

ProductSupplierPrice
Breakout board for the Freescale’s MPR121QR2Sparkfun$9.95
Breakout board for AT42QT1070Adafruit$7.50
Single touch sensor board with AT42QT1012Adafruit$5.95
Touch PotentiometerTindie$24.95
Makey MakeyMakey Makey$49.95
Bare Conductive Touch BoardBare Conductive£55.00
HoverboardTindie$39.00

 

Components

As I've already a bit of experience with the MBR3 chips I decided that I'd stick with those. There are several in the series but the CY8CMBR3110CY8CMBR3110 with it's 10 channels will be able to handle the 5 buttons, host interupt and shield sensor. I took advantage of the Cypress offer and order myself a small batch. As this is a surface mount device it made sense to also use surface mount components for the discrete components needed.  I quizzed the Element14 community on the most suitable smd sizes and will use these to design my board.

 

Skills

There are three key skills for this project. Desgining PCBs, SMD soldering and configuring the MBR3 device. I've created PCBs before, firstly by hand in the 1980s using etch resistant tape, then in the 1990s with photo resist using a plugin for AutoCAD to design the layout. The capacitive sensors need a bit of care designing but there's a good design guide for CapSense switches that explains best practice for designing sensors and laying out the board so I'm reading and re-reading that. I've started learning how to use Eagle and created some basic layouts. I should be able to build the board and learn as I go. I've also had some exposure to hand soldering SMD components although I've not tried with a solder paste and a reflow oven.

It should be possible to avoid the need for etching by outsoucing the creating of the PCB. There cheapest option seems to be Dirty Cheap PCBs but there is quite a long lead time for them and any boards they make are Open Source Hardware so they are not for everyone. Another option is Ragworm who are based in the UK so can turn around boards more quickly.

 

Tools

Here's one area where I might need to make some purchases. I'm using the freeware version of Eagle which meets my technical requirements but if I want to make my project commercial then there would be a €62 cost to move to the correct license.

Also my soldering equipment is limited to an accient Antex iron with no temperature control, I have done other surface mount work with that but I also managed to melt one chip so a better iron would be a good idea if I am to hand solder the boards. Related to this some form of magnification would be a good idea. I have also thought about building or buying a reflow oven to assemble the boards, if I plan to make a lot of boards this would definately be a good investment. Again I've quizzed the community for recommended tools for The specified item was not found..

For configuring the MBR3 these can be programmed by sending a block of data from a microcontroller. However, I worked out that I could remove the jumpers on the evaluation board and use that and the E-ZClick tools to hook up my new board. The advantage of doing that is that I can tweek the settings and analyse the performance of the switches more easily. So apart from making an adapter this aspect is covered.

 

Costs

Leading on from the components, skills and tools this brings us to costs. My bill of materials is pretty small, the circuit I'm planning is just 12 components costing approx £2 for small quantities.

I've done a very rough estimate below, my low end reflow oven estimate of £50 is a self build solution with the top of the range being an off the shelf model. The soldering iron costs I've just picked a couple of tempoerature controlled models. My costing model is also quite simple in that it assumes that I need to recoup all of the one off costs imediately even though some of the tools/software might have longer term value. Another simplification of the model is that I've not scalled the BOM and PCB costs based on quantity so there could be more savings to be made. However these costs don't include any marketting or logistic/shipping costs so there could be additional costs on top of these.

 

ItemHand soldered (min)Hand soldered (max)Reflow (min)Reflow (max)Outsourced Assembly
Eagle License €62£50£50£50£50£50
Reflow Oven£50£1,722
Temperature controlled Iron£40£200
Jigs, wires etc£10£10£10£10
Build of Materials (BOM)£2£2£2£2£2
PCBs, outsourced in all cases£5£5£5£5£5
Consumables such as solder, cleaner (estimate)£1£1£1£1
Assembly Cost£20
Total investment based on 10 boards£180£340£190£1,862£120
Total per board for 10 boards£18£34£19£186£32
Total per board for 20 boards£11£19£12£95£30
Total per board for 50 boards£10£13£10£44£28
Total per board for 100 boards£9£11£9£26£28

 

There's some really useful points from Anna Lowe in the following video.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Summary

As a project this does seem viable, there are other products in this area but not one that's directly competing.

The components are readily available and the skills needed to assemble are within my capability.

The costs for the parts is also good but I need to be aware of the one off costs for equipment I'd need to put these together. I'm likely to start with minimal investiment and ramp up as I need.

 

What next

I've already been learning to use the PCB tools and reading up on the capacitive switch design requirements. My plan is to draw up the designs for the board and get one made up to test before buying a bigger batch. This will initially be more expensive but will mean I won't end up with a load of unusable boards. I've also been creating Eagle Libraries for the MBR3 chips and hope to release those via the CadSoft website CadSoft EAGLE PCB Design Software - EAGLE part libraries

  • Sign in to reply
Parents
  • shabaz
    shabaz over 11 years ago

    Hey Andy,

     

    Good stuff. I'd been looking at the Freescale and Atmel options a while back.

     

    I think it's true that a business case could be made for such a project. I guess you're aiming for the hobbyist market?

    Most keypads are for industrial use, with a corresponding price : (

    I've been forced to create my own keypad for a couple of projects (with switches, not capacitive) due to lack of options.

     

    I'd love to try out your board when it's released : )

     

    Also, not necessarily for the first release (better to get something out that meets initial needs first), but perhaps as future

    roadmap items, what might be interesting is space on the board for an LED (either for status or for backlight in the center

    of the buttons, and as another idea the I2C and supply rails brought out to an edge, for those who want to connect up

    an I2C LCD display alongside the board, or for connecting up any boards in your future product portfolio : )


    But in general it does sound like a useful product.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to shabaz

    Hi Shabaz,

    thanks for the feedback. Yes I will likely want some beta testers, or even roadtesters. I'm thinking of the B2M (Business to Maker) market.

    The intial board will likely be a bare minimum but there are spare pins on the chip that could be used for additional sensors or output e.g. led or haptic. Running an I2C LCD in parallel was exactly the kind of use case I envisaged. The wiring I planned a 5 pin header, I probably won't include a "thru" connector as that could also be done in the cabling.

    Watch this space....

    Cheers.

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to shabaz

    Hi Shabaz,

    thanks for the feedback. Yes I will likely want some beta testers, or even roadtesters. I'm thinking of the B2M (Business to Maker) market.

    The intial board will likely be a bare minimum but there are spare pins on the chip that could be used for additional sensors or output e.g. led or haptic. Running an I2C LCD in parallel was exactly the kind of use case I envisaged. The wiring I planned a 5 pin header, I probably won't include a "thru" connector as that could also be done in the cabling.

    Watch this space....

    Cheers.

    Andy