Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Why is this transistor required
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 71 subscribers
  • Views 2827 views
  • Users 0 members are here
  • relay
Related

Why is this transistor required

rishi2628
rishi2628 over 10 years ago

Why is the transistor Q3 required in this circuit of a optocoupler and a relay. Can't I directly attach the power pin of the relay to the opto coupler pin 3 and ground the other pin of the relay. I tried it and it works. Just want to know why is it not implemented and why is the transistor required.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 10 years ago in reply to rishi2628 +1
    Ah yes, I see what you mean. Possibly the switching current for the relay coil is higher than the optocoupler can safely provide, so the transistor is there to do the job instead.
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    There should be some notion of design margin.  Even if, say, the optocoupler Q is rated at 30mA and the relay coil is rated at 30 mA, the buffer Q should still be employed.  There is such a thing as specsmanship.  There is such a thing as design (process) variation.  There is such a thing as not being a stunod.  For every 10 degree K more heat (temperature rise, heat is not measured in Kelvins) you put into a device you halve its lifetime.

     

    We don't have to race to the bottom of being cheap if our applications are valid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    There should be some notion of design margin.  Even if, say, the optocoupler Q is rated at 30mA and the relay coil is rated at 30 mA, the buffer Q should still be employed.  There is such a thing as specsmanship.  There is such a thing as design (process) variation.  There is such a thing as not being a stunod.  For every 10 degree K more heat (temperature rise, heat is not measured in Kelvins) you put into a device you halve its lifetime.

     

    We don't have to race to the bottom of being cheap if our applications are valid.