Code Exchange
  • Technologies
  • More
Code Exchange
Blog C++ moving and returning objects part 1: object as return value (embedded friendly C++)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 Jul 2025 11:02 AM Date Created
  • Views 1158 views
  • Likes 6 likes
  • Comments 3 comments
  • Modern C++
  • c++26
  • c++23
  • c++
  • c++20
Related
Recommended

C++ moving and returning objects part 1: object as return value (embedded friendly C++)

Jan Cumps
Jan Cumps
19 Jul 2025

You may read guidelines that say: "never use an object as return value of a function. Because of performance reasons". Because the object is copied into the receiving variable when returning from the function call. That was true in C++98. In modern C++, this is no longer true.

Initially (the old days):

  • the return object was locally constructed in your function
  • it was copied (via copy constructor) into the receiving variable
  • the function-local original object was destructed

Now (since 10 years):

  • the return object is directly constructed, on location, in the receiving variable

This behaviour (copy elision) is not optional, or an optimiser choice. C++ compilers have to do that for C++ standard 17 and later (i.e.: from GCC 7.x on).

Example code:

#include <iostream>

using std::cout;
using std::endl;

struct T {
    int value;
    T(int value); // ctor
    ~T();         // dtor
};

T::T(int value) : value(value) { cout << "ctor" << endl; }
T::~T() { cout << "dtor" << endl; }

inline T work() {
    // this object is constructed in place in the variable that's receiving this value (modern c++)
    // it is not created as a function-local variable, then copied and discarded (old days)
    return T(1);
}

int main() {
    T t = work();
    return 0;
}

You 'll notice that the object is constructed once. It's constructed by function work() directly on location in the memory area of variable t.
No copying, or destroying. It's just one object that's available to the caller after the function returns.

It will be destroyed when variable t goes out of scope: when main() exits.

In essence, the code above is using the same assembler as:

int main() {
    T t (1);
    return 0;
}

Run both versions of main(), and check in the output how many times the constructor and destructor are called. Is one more expensive than the other?

Next post: how to efficiently move objects in a program, while avoiding copying large data members.
hint: you can "move" members from one object to the other, instead of "copy, then destroy source"

Thank you for reading.

 C++ moving and returning objects part 1: object as return value (embedded friendly C++) 

 C++ moving and returning objects part 2: move and copy (embedded friendly C++) 

  • Sign in to reply
  • kmikemoo
    kmikemoo over 1 year ago

    Good information. Thumbsup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 1 year ago

    Nice post Jan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    I'm using this technique sparsely in a GPS parser lib I wrote. Several developers that  wanted to use it, challenged performance because I sometimes return an object. This post can help put some context to that question.

    What I learned while writing C++ libraries, is that not a lot of people challenge the functionality. Virtual any comment is about the use of C++, STL, ... As if we were in 1998.
    While there is a lot to gain for embedded designs. Embedded firmware is close to hardware. It's an excellent candidate for object based designs.
    And OO designs come cheap this days. For memory and clock ticks. A lot of times the execution cost is 0 bytes, 0 ticks. But it's expensive for the designer community brain flex ...