Code Exchange
  • Technologies
  • More
Code Exchange
Blog C++ write your own stream class - part 1: output stream initial design (embedded friendly C++)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 11 Nov 2025 7:09 PM Date Created
  • Views 530 views
  • Likes 4 likes
  • Comments 6 comments
  • Modern C++
  • c++
Related
Recommended

C++ write your own stream class - part 1: output stream initial design (embedded friendly C++)

Jan Cumps
Jan Cumps
11 Nov 2025

In C++ it's common to stream data. You write to a file using the << operator.

example: 

cout << "hello, world! << endl;

In this blog I'm making my own minimal output stream class. Just enough code to show that it works. This could become an object that allows you to write to a UART, SPI, CAN, ... . In this post, I called my class uartostream, although it doesn't do anything UART. Just to give it an embedded sounding name, and to show how this could look like in firmware.

I put embedded friendly in the title because this is a resource-friendly exercise. Can be used on the smallest controllers.

output stream class

You can stream c-type strings to this class, and std::string objects. 

class uartostream {
public:
    uartostream() {}    
    
    uartostream& operator << (const char* msg) {
      // write to UART
      return *this;
    }
    
    uartostream& operator << (const std::string& msg) {
      // write to UART
      return *this;
    }
};

Notice that the class doesn't do anything with them. In this first post I want to check if the code compiles. And I use a debugger to see if the strings arrive in their handlers. If I put a breakpoint in the handler methods, and the msg parameter contains the string we've streamed to it, the mechanism works.

using the class

In the example code, I'll stream a std::string and a classic c-style char string. 

#include <string>

class uartostream{ // see previous section for class definition
};

uartostream u;

int main() {
  u << std::string("5") << "5" ;
}

test

I put a breakpoint in both operator << members. The code should first halt in the one that takes a std::string reference. Then the one that takes the c string.

image

The screen capture above shows the state while streaming the first part. If you want to see what happens when the "5" is streamed: try it in your favourite C++ IDE.

Here's a little breakout post that checks if this kind of C++ abstraction creates any runtime overhead: C++ write your own stream class - part 1a: the cost of objects can be zero (embedded friendly C++) 

Thank you for reading. To be continued.

  • Sign in to reply
Parents
  • DAB
    DAB 10 months ago

    Nice post Jan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB 10 months ago

    Nice post Jan.