Code Exchange
  • Technologies
  • More
Code Exchange
Blog modern C++: initialise a static array inside a class
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2025 4:58 PM Date Created
  • Views 1555 views
  • Likes 6 likes
  • Comments 10 comments
  • c++17
  • Modern C++
  • c++
Related
Recommended

modern C++: initialise a static array inside a class

Jan Cumps
Jan Cumps
24 Nov 2025

Pre C++17

In traditional C++, if you have a class that has a static array as data member, you have to initialise that array outside of the class. 

class myclass {
protected:
    static uint myarray[4];
};

uint myclass::myarray[4];

You will typically have the declaration in your header file, and the definition (initialisation) in a cpp file.

Since C++17

With modern C++, you can do all in the above in the class declaration, with inline:

class myclass {
private:
    inline static uint myarray[4] = {};
};

The generated code is the same.

Thank you for reading.

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps 5 months ago

    I'm making a few changes to the nmea lib API and code: let the library return objects, instead of passing them via output parameters

    image

    Since C++17, the compiler can directly use the object that receives the return value. So no constructors or copies are called in this mechanism.

    Old version:

    void nmea::time(const std::string_view& sv, time_t& t) {
    	std::string s(sv);
    	t = time_t{
    		std::chrono::hours(std::stoi(s.substr(0,  2))) +
    		std::chrono::minutes(std::stoi(s.substr(2,  2))) +
    	    std::chrono::seconds(std::stoi(s.substr(4,  2))) +
    		std::chrono::milliseconds(std::stoi(s.substr(7)))
    	};
    }

    New version (uses exactly same amount of resources):

    time_t nmea::time(const std::string_view& sv) {
    	std::string s(sv);
    	return time_t{
    		std::chrono::hours(std::stoi(s.substr(0,  2))) +
    		std::chrono::minutes(std::stoi(s.substr(2,  2))) +
    	    std::chrono::seconds(std::stoi(s.substr(4,  2))) +
    		std::chrono::milliseconds(std::stoi(s.substr(7)))
    	};
    }

    All API functions that use an output parameter have been adapted. I'm running tests to see if any regression happened...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vmate
    vmate 5 months ago in reply to Jan Cumps

    It's almost always better to do it the new way, and actually the time_t example doesn't apply here at all, since it's a fundamental type, so there is no ctor/dtor or any performance penalty. 

    For small objects, even a full constructor call is probably just as fast if not faster than passing in by reference and having the code mess with pointers and stuff.

    Also, Return Value Optimization has been part of the spec (although optional) for like 30 years at this point if I recall correctly, so C++17's guaranteed copy elision is not even needed for small and relatively simple types.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 5 months ago in reply to vmate

    > Also, Return Value Optimization has been part of the spec (although optional) for like 30 years at this point if I recall correctly,
    > so C++17's guaranteed copy elision is not even needed for small and relatively simple types.

    Yes, it exists since c++11. Enforced by compiler (regardless of what command line switches are passed during build) since c++17.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 5 months ago in reply to vmate

    the time_t example doesn't apply here at all, since it's a fundamental type, so there is no ctor/dtor or any performance penalty. 

    Not obvious from the snippet I posted, but it's a class (with a constructor) in this case:

    using time_t = std::chrono::hh_mm_ss<std::chrono::duration<long long, std::ratio<1, 1000>>>;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps 5 months ago in reply to vmate

    the time_t example doesn't apply here at all, since it's a fundamental type, so there is no ctor/dtor or any performance penalty. 

    Not obvious from the snippet I posted, but it's a class (with a constructor) in this case:

    using time_t = std::chrono::hh_mm_ss<std::chrono::duration<long long, std::ratio<1, 1000>>>;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps 5 months ago in reply to Jan Cumps

    ... that sits in the nmea namespace:

    namespace nmea {
    
    using time_t = std::chrono::hh_mm_ss<std::chrono::duration<long long, std::ratio<1, 1000>>>;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vmate
    vmate 5 months ago in reply to Jan Cumps

    Ah, sorry then, all the times I've encountered time_t, it has been just a typedef to a 32/64bit int.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 5 months ago in reply to vmate

    giving it a same name as a built-in type wasn't my brightest moment Slight smile