Code Exchange
  • Technologies
  • More
Code Exchange
Blog modern C++: initialise a static array inside a class
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2025 4:58 PM Date Created
  • Views 1561 views
  • Likes 6 likes
  • Comments 10 comments
  • c++17
  • Modern C++
  • c++
Related
Recommended

modern C++: initialise a static array inside a class

Jan Cumps
Jan Cumps
24 Nov 2025

Pre C++17

In traditional C++, if you have a class that has a static array as data member, you have to initialise that array outside of the class. 

class myclass {
protected:
    static uint myarray[4];
};

uint myclass::myarray[4];

You will typically have the declaration in your header file, and the definition (initialisation) in a cpp file.

Since C++17

With modern C++, you can do all in the above in the class declaration, with inline:

class myclass {
private:
    inline static uint myarray[4] = {};
};

The generated code is the same.

Thank you for reading.

  • Sign in to reply
Parents
  • vmate
    vmate 9 months ago

    A notable exception is that with constexpr arrays, this can be done pre-c++17:

    class myclass {
    public:
        static constexpr uint32_t myarray[4] = {1, 2, 3, 4};
    };


    Also, in recent versions of C++, std::array should probably be used instead of 'regular' arrays:
    class myclass {
    private:
        inline static std::array<uint32_t, 4> myarray = {0};
    }

    Instead of myarray becoming a uint32_t pointer, and then the programmer is responsible for doing everything correctly with it, std::array actually behaves as a proper object, it knows its own size, can be assigned properly to another array, etc. It has a bunch of convenience features like .begin() and .end() too, and it is zero cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vmate
    vmate 9 months ago

    A notable exception is that with constexpr arrays, this can be done pre-c++17:

    class myclass {
    public:
        static constexpr uint32_t myarray[4] = {1, 2, 3, 4};
    };


    Also, in recent versions of C++, std::array should probably be used instead of 'regular' arrays:
    class myclass {
    private:
        inline static std::array<uint32_t, 4> myarray = {0};
    }

    Instead of myarray becoming a uint32_t pointer, and then the programmer is responsible for doing everything correctly with it, std::array actually behaves as a proper object, it knows its own size, can be assigned properly to another array, etc. It has a bunch of convenience features like .begin() and .end() too, and it is zero cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps 9 months ago in reply to vmate

    I did a few posts on std::array and standard lib algorithms for embedded:

     modern C++ on a Pico: use C++ Standard Library algorithms - embedded friendly 

     C++ parser library for NMEA GPS data - pt. 4: We have C++ objects and containers: So what? 

    For this post, I tried to keep it short and focused on the initialise functionality.